]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/libdrm.git/commitdiff
intel: Get intel_decode.c minimally building.
authorEric Anholt <eric@anholt.net>
Tue, 20 Dec 2011 21:06:16 +0000 (13:06 -0800)
committerEric Anholt <eric@anholt.net>
Fri, 30 Dec 2011 00:43:36 +0000 (16:43 -0800)
My plan is to use this drm_intel_dump_batchbuffer() interface for the
current GPU tools, and the current Mesa batch dumping usage, while
eventually building more interesting interfaces for other uses.

Warnings are currently suppressed by using a helper lib with CFLAGS
set manually, because the code is totally not ready for libdrm's warnings
setup.

Acked-by: Daniel Vetter <daniel.vetter@ffwll.ch>
Acked-by: Eugeni Dodonov <eugeni@dodonov.net>
intel/Makefile.am
intel/intel_bufmgr.h
intel/intel_decode.c

index 7a44aaf9aa71e6d659dfd8ae3eadae8e49086086..1af0187daaf969beec397d28858f91cb1226c050 100644 (file)
@@ -33,7 +33,20 @@ AM_CFLAGS = \
 libdrm_intel_la_LTLIBRARIES = libdrm_intel.la
 libdrm_intel_ladir = $(libdir)
 libdrm_intel_la_LDFLAGS = -version-number 1:0:0 -no-undefined
-libdrm_intel_la_LIBADD = ../libdrm.la @PTHREADSTUBS_LIBS@ @PCIACCESS_LIBS@ @CLOCK_LIB@
+libdrm_intel_la_LIBADD = ../libdrm.la \
+       @PTHREADSTUBS_LIBS@ \
+       @PCIACCESS_LIBS@ \
+       @CLOCK_LIB@ \
+       libintel_decode.la
+
+
+noinst_LTLIBRARIES = libintel_decode.la
+
+libintel_decode_la_SOURCES = intel_decode.c
+libintel_decode_la_CFLAGS = \
+       -I$(top_srcdir) \
+       -I$(top_srcdir)/intel \
+       -std=c99
 
 libdrm_intel_la_SOURCES = \
        intel_bufmgr.c \
@@ -44,6 +57,8 @@ libdrm_intel_la_SOURCES = \
        mm.c \
        mm.h
 
+intel_bufmgr_gem_o_CFLAGS = $(AM_CFLAGS) -c99
+
 libdrm_intelincludedir = ${includedir}/libdrm
 libdrm_intelinclude_HEADERS = intel_bufmgr.h \
                              intel_debug.h
index 808e5dfa4a6df397987ee4004c6b363268b0e18e..68017a5433452b09b2213e76c67b11d6a148251d 100644 (file)
@@ -190,6 +190,18 @@ void drm_intel_bo_fake_disable_backing_store(drm_intel_bo *bo,
 void drm_intel_bufmgr_fake_contended_lock_take(drm_intel_bufmgr *bufmgr);
 void drm_intel_bufmgr_fake_evict_all(drm_intel_bufmgr *bufmgr);
 
+struct drm_intel_decode *drm_intel_decode_context_alloc(uint32_t devid);
+void drm_intel_decode_context_free(struct drm_intel_decode *ctx);
+void drm_intel_decode_set_batch_pointer(struct drm_intel_decode *ctx,
+                                       void *data, uint32_t hw_offset,
+                                       int count);
+void drm_intel_decode_set_dump_past_end(struct drm_intel_decode *ctx,
+                                       int dump_past_end);
+void drm_intel_decode_set_head_tail(struct drm_intel_decode *ctx,
+                                   uint32_t head, uint32_t tail);
+void drm_intel_decode(struct drm_intel_decode *ctx);
+
+
 /** @{ Compatibility defines to keep old code building despite the symbol rename
  * from dri_* to drm_intel_*
  */
index e06142c14191c14894a281ff3502dd904a9d6b17..e61d5ed6269e3ad8473fad0ead8df34204886e9e 100644 (file)
  */
 
 #include <stdint.h>
+#include <stdlib.h>
 #include <stdio.h>
+#include <stdbool.h>
 #include <stdarg.h>
 #include <string.h>
 
 #include "intel_decode.h"
 #include "intel_chipset.h"
-#include "intel_gpu_tools.h"
+#include "intel_bufmgr.h"
+
+/* Struct for tracking drm_intel_decode state. */
+struct drm_intel_decode {
+       /** PCI device ID. */
+       uint32_t devid;
+
+       /** GPU address of the start of the batchbuffer data. */
+       uint32_t hw_offset;
+       /** CPU Virtual address of the start of the batchbuffer data. */
+       uint32_t *data;
+       /** Number of DWORDs of batchbuffer data. */
+       uint32_t count;
+
+       /** @{
+        * GPU head and tail pointers, which will be noted in the dump, or ~0.
+        */
+       uint32_t head, tail;
+       /** @} */
+
+       /**
+        * Whether to dump the dwords after MI_BATCHBUFFER_END.
+        *
+        * This sometimes provides clues in corrupted batchbuffers,
+        * and is used by the intel-gpu-tools.
+        */
+       bool dump_past_end;
+};
 
 static FILE *out;
 static uint32_t saved_s2 = 0, saved_s4 = 0;
@@ -3278,7 +3307,7 @@ decode_3d_965(uint32_t *data, int count, uint32_t hw_offset, uint32_t devid,
                return len;
 
        case 0x7a00:
-               if (intel_gen(devid) >= 6) {
+               if (IS_GEN6(devid) || IS_GEN7(devid)) {
                        int i;
                        len = (data[0] & 0xff) + 2;
                        if (len != 4 && len != 5)
@@ -3505,6 +3534,50 @@ decode_3d_i830(uint32_t *data, int count, uint32_t hw_offset, uint32_t devid,
        return 1;
 }
 
+struct drm_intel_decode *
+drm_intel_decode_context_alloc(uint32_t devid)
+{
+       struct drm_intel_decode *ctx;
+
+       ctx = calloc(1, sizeof(struct drm_intel_decode));
+       if (!ctx)
+               return NULL;
+
+       ctx->devid = devid;
+
+       return ctx;
+}
+
+void
+drm_intel_decode_context_free(struct drm_intel_decode *ctx)
+{
+       free(ctx);
+}
+
+void
+drm_intel_decode_set_dump_past_end(struct drm_intel_decode *ctx,
+                                  int dump_past_end)
+{
+       ctx->dump_past_end = !!dump_past_end;
+}
+
+void
+drm_intel_decode_set_batch_pointer(struct drm_intel_decode *ctx,
+                                  void *data, uint32_t hw_offset, int count)
+{
+       ctx->data = data;
+       ctx->hw_offset = hw_offset;
+       ctx->count = count;
+}
+
+void
+drm_intel_decode_set_head_tail(struct drm_intel_decode *ctx,
+                              uint32_t head, uint32_t tail)
+{
+       ctx->head = head;
+       ctx->tail = tail;
+}
+
 /**
  * Decodes an i830-i915 batch buffer, writing the output to stdout.
  *
@@ -3512,14 +3585,28 @@ decode_3d_i830(uint32_t *data, int count, uint32_t hw_offset, uint32_t devid,
  * \param count number of DWORDs to decode in the batch buffer
  * \param hw_offset hardware address for the buffer
  */
-int
-intel_decode(uint32_t *data, int count,
-            uint32_t hw_offset,
-            uint32_t devid, uint32_t ignore_end_of_batchbuffer)
+void
+drm_intel_decode(struct drm_intel_decode *ctx)
 {
        int ret;
        int index = 0;
        int failures = 0;
+       uint32_t *data;
+       uint32_t count, hw_offset;
+       uint32_t devid;
+
+       if (!ctx)
+               return;
+
+       data = ctx->data;
+       count = ctx->count;
+       hw_offset = ctx->hw_offset;
+       devid = ctx->devid;
+       head_offset = ctx->head;
+       tail_offset = ctx->tail;
+
+       saved_s2_set = 0;
+       saved_s4_set = 1;
 
        out = stdout;
 
@@ -3536,7 +3623,7 @@ intel_decode(uint32_t *data, int count,
                         * case.
                         */
                        if (ret == -1) {
-                               if (ignore_end_of_batchbuffer) {
+                               if (ctx->dump_past_end) {
                                        index++;
                                } else {
                                        for (index = index + 1; index < count;
@@ -3553,7 +3640,7 @@ intel_decode(uint32_t *data, int count,
                                           hw_offset + index * 4, &failures);
                        break;
                case 0x3:
-                       if (IS_965(devid)) {
+                       if (IS_9XX(devid) && !IS_GEN3(devid)) {
                                index +=
                                    decode_3d_965(data + index, count - index,
                                                  hw_offset + index * 4, devid,
@@ -3577,18 +3664,4 @@ intel_decode(uint32_t *data, int count,
                }
                fflush(out);
        }
-
-       return failures;
-}
-
-void intel_decode_context_reset(void)
-{
-       saved_s2_set = 0;
-       saved_s4_set = 1;
-}
-
-void intel_decode_context_set_head_tail(uint32_t head, uint32_t tail)
-{
-       head_offset = head;
-       tail_offset = tail;
 }