summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 0ef7644)
raw | patch | inline | side by side (parent: 0ef7644)
author | Paulo Zanoni <paulo.r.zanoni@intel.com> | |
Sat, 21 Apr 2012 20:51:53 +0000 (17:51 -0300) | ||
committer | Daniel Vetter <daniel.vetter@ffwll.ch> | |
Thu, 3 May 2012 11:32:02 +0000 (13:32 +0200) |
In the future we'll have more than just connector properties, so create
a dump_prop function that can handle any property (instead of the
current dump_props function that only handles connector properties).
Also, make this function print a lot more information about the existing
properties.
Also change the printed indentation of the modes to make the output more
readable.
The previous function dump_props also segfaulted when we didn't have
enought permissions. The new function does not segfault in this case (by
checking for the return value of drmModeGetProperty).
Reviewed-by: Eugeni Dodonov <eugeni.dodonov@intel.com>
Signed-off-by: Paulo Zanoni <paulo.r.zanoni@intel.com>
Signed-off-by: Daniel Vetter <daniel.vetter@ffwll.ch>
a dump_prop function that can handle any property (instead of the
current dump_props function that only handles connector properties).
Also, make this function print a lot more information about the existing
properties.
Also change the printed indentation of the modes to make the output more
readable.
The previous function dump_props also segfaulted when we didn't have
enought permissions. The new function does not segfault in this case (by
checking for the return value of drmModeGetProperty).
Reviewed-by: Eugeni Dodonov <eugeni.dodonov@intel.com>
Signed-off-by: Paulo Zanoni <paulo.r.zanoni@intel.com>
Signed-off-by: Daniel Vetter <daniel.vetter@ffwll.ch>
tests/modetest/modetest.c | patch | blob | history |
index 6deed69eaa45412655c4e2765cb9edfc7ddf5c4d..57846220f84910aeef1e94b942635894e289d4ae 100644 (file)
#include <stdio.h>
#include <stdlib.h>
#include <stdint.h>
+#include <inttypes.h>
#include <unistd.h>
#include <string.h>
#include <errno.h>
void dump_mode(drmModeModeInfo *mode)
{
- printf(" %s %d %d %d %d %d %d %d %d %d\n",
+ printf("\t%s %d %d %d %d %d %d %d %d %d\n",
mode->name,
mode->vrefresh,
mode->hdisplay,
}
static void
-dump_props(drmModeConnector *connector)
+dump_blob(uint32_t blob_id)
+{
+ uint32_t i;
+ unsigned char *blob_data;
+ drmModePropertyBlobPtr blob;
+
+ blob = drmModeGetPropertyBlob(fd, blob_id);
+ if (!blob)
+ return;
+
+ blob_data = blob->data;
+
+ for (i = 0; i < blob->length; i++) {
+ if (i % 16 == 0)
+ printf("\n\t\t\t");
+ printf("%.2hhx", blob_data[i]);
+ }
+ printf("\n");
+
+ drmModeFreePropertyBlob(blob);
+}
+
+static void
+dump_prop(uint32_t prop_id, uint64_t value)
{
- drmModePropertyPtr props;
int i;
+ drmModePropertyPtr prop;
+
+ prop = drmModeGetProperty(fd, prop_id);
+
+ printf("\t%d", prop_id);
+ if (!prop) {
+ printf("\n");
+ return;
+ }
+
+ printf(" %s:\n", prop->name);
+
+ printf("\t\tflags:");
+ if (prop->flags & DRM_MODE_PROP_PENDING)
+ printf(" pending");
+ if (prop->flags & DRM_MODE_PROP_RANGE)
+ printf(" range");
+ if (prop->flags & DRM_MODE_PROP_IMMUTABLE)
+ printf(" immutable");
+ if (prop->flags & DRM_MODE_PROP_ENUM)
+ printf(" enum");
+ if (prop->flags & DRM_MODE_PROP_BLOB)
+ printf(" blob");
+ printf("\n");
+
+ if (prop->flags & DRM_MODE_PROP_RANGE) {
+ printf("\t\tvalues:");
+ for (i = 0; i < prop->count_values; i++)
+ printf(" %"PRIu64, prop->values[i]);
+ printf("\n");
+ }
- for (i = 0; i < connector->count_props; i++) {
- props = drmModeGetProperty(fd, connector->props[i]);
- printf("\t%s, flags %d\n", props->name, props->flags);
- drmModeFreeProperty(props);
+ if (prop->flags & DRM_MODE_PROP_ENUM) {
+ printf("\t\tenums:");
+ for (i = 0; i < prop->count_enums; i++)
+ printf(" %s=%llu", prop->enums[i].name,
+ prop->enums[i].value);
+ printf("\n");
+ } else {
+ assert(prop->count_enums == 0);
}
+
+ if (prop->flags & DRM_MODE_PROP_BLOB) {
+ printf("\t\tblobs:\n");
+ for (i = 0; i < prop->count_blobs; i++)
+ dump_blob(prop->blob_ids[i]);
+ printf("\n");
+ } else {
+ assert(prop->count_blobs == 0);
+ }
+
+ printf("\t\tvalue:");
+ if (prop->flags & DRM_MODE_PROP_BLOB)
+ dump_blob(value);
+ else
+ printf(" %"PRIu64"\n", value);
+
+ drmModeFreeProperty(prop);
}
void dump_connectors(void)
if (connector->count_modes) {
printf(" modes:\n");
- printf(" name refresh (Hz) hdisp hss hse htot vdisp "
+ printf("\tname refresh (Hz) hdisp hss hse htot vdisp "
"vss vse vtot)\n");
for (j = 0; j < connector->count_modes; j++)
dump_mode(&connector->modes[j]);
printf(" props:\n");
- dump_props(connector);
+ for (j = 0; j < connector->count_props; j++)
+ dump_prop(connector->props[j],
+ connector->prop_values[j]);
}
drmModeFreeConnector(connector);