summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: cf7cc62)
raw | patch | inline | side by side (parent: cf7cc62)
author | Paul Berry <stereotype441@gmail.com> | |
Fri, 4 May 2012 19:41:00 +0000 (12:41 -0700) | ||
committer | Paul Berry <stereotype441@gmail.com> | |
Thu, 10 May 2012 18:32:39 +0000 (11:32 -0700) |
This patch adds a new function,
drm_intel_bufmgr_gem_set_aub_annotations(), which can be used to
annotate the type and subtype of data stored in various sections of
each buffer. This data is used to populate type and subtype fields
when generating the .aub file, which improves the ability of later
debugging tools to analyze the contents of the .aub file.
If drm_intel_bufmgr_gem_set_aub_annotations() is not called, then we
fall back to the old set of annotations (annotate the portion of the
batchbuffer that is executed as AUB_TRACE_TYPE_BATCH, and everything
else as AUB_TRACE_TYPE_NOTYPE).
Reviewed-by: Eric Anholt <eric@anholt.net>
drm_intel_bufmgr_gem_set_aub_annotations(), which can be used to
annotate the type and subtype of data stored in various sections of
each buffer. This data is used to populate type and subtype fields
when generating the .aub file, which improves the ability of later
debugging tools to analyze the contents of the .aub file.
If drm_intel_bufmgr_gem_set_aub_annotations() is not called, then we
fall back to the old set of annotations (annotate the portion of the
batchbuffer that is executed as AUB_TRACE_TYPE_BATCH, and everything
else as AUB_TRACE_TYPE_NOTYPE).
Reviewed-by: Eric Anholt <eric@anholt.net>
intel/intel_bufmgr.h | patch | blob | history | |
intel/intel_bufmgr_gem.c | patch | blob | history |
diff --git a/intel/intel_bufmgr.h b/intel/intel_bufmgr.h
index 45389e1e32167225fe311faa5751c63b83d11d55..c197abc62faa22072e15702e06f73365ec214ff8 100644 (file)
--- a/intel/intel_bufmgr.h
+++ b/intel/intel_bufmgr.h
AUB_DUMP_BMP_FORMAT_ARGB_8888 = 7,
};
+typedef struct _drm_intel_aub_annotation {
+ uint32_t type;
+ uint32_t subtype;
+ uint32_t ending_offset;
+} drm_intel_aub_annotation;
+
#define BO_ALLOC_FOR_RENDER (1<<0)
drm_intel_bo *drm_intel_bo_alloc(drm_intel_bufmgr *bufmgr, const char *name,
int x1, int y1, int width, int height,
enum aub_dump_bmp_format format,
int pitch, int offset);
+void
+drm_intel_bufmgr_gem_set_aub_annotations(drm_intel_bo *bo,
+ drm_intel_aub_annotation *annotations,
+ unsigned count);
int drm_intel_get_pipe_from_crtc_id(drm_intel_bufmgr *bufmgr, int crtc_id);
index 3c91090409900b125ae6fba8be4b213ce0e023b0..b776d2f755ef1f1950569696dd12487deb98066e 100644 (file)
--- a/intel/intel_bufmgr_gem.c
+++ b/intel/intel_bufmgr_gem.c
bool mapped_cpu_write;
uint32_t aub_offset;
+
+ drm_intel_aub_annotation *aub_annotations;
+ unsigned aub_annotation_count;
};
static unsigned int
bo_gem->used_as_reloc_target = false;
bo_gem->has_error = false;
bo_gem->reusable = true;
+ bo_gem->aub_annotations = NULL;
+ bo_gem->aub_annotation_count = 0;
drm_intel_bo_gem_set_in_aperture_size(bufmgr_gem, bo_gem);
DBG("DRM_IOCTL_GEM_CLOSE %d failed (%s): %s\n",
bo_gem->gem_handle, bo_gem->name, strerror(errno));
}
+ free(bo_gem->aub_annotations);
free(bo);
}
aub_write_bo_data(bo, offset, size);
}
+/**
+ * Break up large objects into multiple writes. Otherwise a 128kb VBO
+ * would overflow the 16 bits of size field in the packet header and
+ * everything goes badly after that.
+ */
static void
-aub_write_bo(drm_intel_bo *bo)
+aub_write_large_trace_block(drm_intel_bo *bo, uint32_t type, uint32_t subtype,
+ uint32_t offset, uint32_t size)
{
uint32_t block_size;
- uint32_t offset;
-
- aub_bo_get_address(bo);
+ uint32_t sub_offset;
- /* Break up large objects into multiple writes. Otherwise a
- * 128kb VBO would overflow the 16 bits of size field in the
- * packet header and everything goes badly after that.
- */
- for (offset = 0; offset < bo->size; offset += block_size) {
- block_size = bo->size - offset;
+ for (sub_offset = 0; sub_offset < size; sub_offset += block_size) {
+ block_size = size - sub_offset;
if (block_size > 8 * 4096)
block_size = 8 * 4096;
- aub_write_trace_block(bo, AUB_TRACE_TYPE_NOTYPE, 0,
- offset, block_size);
+ aub_write_trace_block(bo, type, subtype, offset + sub_offset,
+ block_size);
+ }
+}
+
+static void
+aub_write_bo(drm_intel_bo *bo)
+{
+ drm_intel_bo_gem *bo_gem = (drm_intel_bo_gem *) bo;
+ uint32_t offset = 0;
+ unsigned i;
+
+ aub_bo_get_address(bo);
+
+ /* Write out each annotated section separately. */
+ for (i = 0; i < bo_gem->aub_annotation_count; ++i) {
+ drm_intel_aub_annotation *annotation =
+ &bo_gem->aub_annotations[i];
+ uint32_t ending_offset = annotation->ending_offset;
+ if (ending_offset > bo->size)
+ ending_offset = bo->size;
+ if (ending_offset > offset) {
+ aub_write_large_trace_block(bo, annotation->type,
+ annotation->subtype,
+ offset,
+ ending_offset - offset);
+ offset = ending_offset;
+ }
+ }
+
+ /* Write out any remaining unannotated data */
+ if (offset < bo->size) {
+ aub_write_large_trace_block(bo, AUB_TRACE_TYPE_NOTYPE, 0,
+ offset, bo->size - offset);
}
}
drm_intel_bufmgr_gem *bufmgr_gem = (drm_intel_bufmgr_gem *) bo->bufmgr;
drm_intel_bo_gem *bo_gem = (drm_intel_bo_gem *) bo;
int i;
+ bool batch_buffer_needs_annotations;
if (!bufmgr_gem->aub_file)
return;
- /* Write out all but the batchbuffer to AUB memory */
- for (i = 0; i < bufmgr_gem->exec_count - 1; i++) {
- if (bufmgr_gem->exec_bos[i] != bo)
- aub_write_bo(bufmgr_gem->exec_bos[i]);
+ /* If batch buffer is not annotated, annotate it the best we
+ * can.
+ */
+ batch_buffer_needs_annotations = bo_gem->aub_annotation_count == 0;
+ if (batch_buffer_needs_annotations) {
+ drm_intel_aub_annotation annotations[2] = {
+ { AUB_TRACE_TYPE_BATCH, 0, used },
+ { AUB_TRACE_TYPE_NOTYPE, 0, bo->size }
+ };
+ drm_intel_bufmgr_gem_set_aub_annotations(bo, annotations, 2);
}
- aub_bo_get_address(bo);
+ /* Write out all buffers to AUB memory */
+ for (i = 0; i < bufmgr_gem->exec_count; i++) {
+ aub_write_bo(bufmgr_gem->exec_bos[i]);
+ }
- /* Dump the batchbuffer. */
- aub_write_trace_block(bo, AUB_TRACE_TYPE_BATCH, 0,
- 0, used);
- aub_write_trace_block(bo, AUB_TRACE_TYPE_NOTYPE, 0,
- used, bo->size - used);
+ /* Remove any annotations we added */
+ if (batch_buffer_needs_annotations)
+ drm_intel_bufmgr_gem_set_aub_annotations(bo, NULL, 0);
/* Dump ring buffer */
aub_build_dump_ringbuffer(bufmgr_gem, bo_gem->aub_offset, ring_flag);
}
}
+/**
+ * Annotate the given bo for use in aub dumping.
+ *
+ * \param annotations is an array of drm_intel_aub_annotation objects
+ * describing the type of data in various sections of the bo. Each
+ * element of the array specifies the type and subtype of a section of
+ * the bo, and the past-the-end offset of that section. The elements
+ * of \c annotations must be sorted so that ending_offset is
+ * increasing.
+ *
+ * \param count is the number of elements in the \c annotations array.
+ * If \c count is zero, then \c annotations will not be dereferenced.
+ *
+ * Annotations are copied into a private data structure, so caller may
+ * re-use the memory pointed to by \c annotations after the call
+ * returns.
+ *
+ * Annotations are stored for the lifetime of the bo; to reset to the
+ * default state (no annotations), call this function with a \c count
+ * of zero.
+ */
+void
+drm_intel_bufmgr_gem_set_aub_annotations(drm_intel_bo *bo,
+ drm_intel_aub_annotation *annotations,
+ unsigned count)
+{
+ drm_intel_bo_gem *bo_gem = (drm_intel_bo_gem *) bo;
+ unsigned size = sizeof(*annotations) * count;
+ drm_intel_aub_annotation *new_annotations =
+ count > 0 ? realloc(bo_gem->aub_annotations, size) : NULL;
+ if (new_annotations == NULL) {
+ free(bo_gem->aub_annotations);
+ bo_gem->aub_annotations = NULL;
+ bo_gem->aub_annotation_count = 0;
+ return;
+ }
+ memcpy(new_annotations, annotations, size);
+ bo_gem->aub_annotations = new_annotations;
+ bo_gem->aub_annotation_count = count;
+}
+
/**
* Initializes the GEM buffer manager, which uses the kernel to allocate, map,
* and manage map buffer objections.