]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/meta-arago-glsdk.git/shortlog
glsdk/meta-arago-glsdk.git
2013-01-30 Chase Maupinti-tisdk-setup: Pull in latest sources denzil 2013.01
2013-01-30 Denys Dmytriyenkobison: drop remove-gets.patch bbappend for native,...
2013-01-30 Franklin S... recipes: Remove unused recipe and bbappend
2013-01-30 Franklin S... meta-toolchain-arago: Remove remaining .la files
2013-01-30 Franklin S... bc: Fix segmentation fault when using -l option
2013-01-30 Franklin S... u-boot_2012.10.psp05.06.00.00 - Freeze PSP 05.06.00.00
2013-01-30 Jeff Lanceqt4-embedded: Add patch to fix QWSLOCK messages
2013-01-30 Franklin S... matrix-gui-apps-git.inc: Pull in latest power managemen...
2013-01-30 Franklin S... linux-am335x-3.2.0-psp05.06.00.00: Fix Suspend and...
2013-01-30 Franklin S... linux-am335x_3.2.0-psp05.06.00.00: Limit Smartreflex...
2013-01-30 Franklin S... oprofile-example: Use updated PACKAGE_STRIP syntax
2013-01-30 Franklin S... dosfstools: Increase FAT partition size and large file...
2013-01-30 Eyal Reizerti-compat-wireless: remove driver version print
2013-01-30 Franklin S... ti-wif-utils: Only run calibrate on startup
2013-01-30 Eyal Reizerbattleship: kill wpa_supplicant before launching
2013-01-30 Eyal Reizerwifi-direct-demo: kill the supplicant before starting
2013-01-30 Eyal Reizerwpa_supplicant: add a script for killing in case running
2013-01-30 Franklin S... wl1271-demo_git: Add obex-client to the runtime depende...
2013-01-30 Franklin S... task-arago-tisdk-connectivity: Add obex-client to the...
2013-01-30 Franklin S... ti-tisdk-setup: Update to include several bug fixes
2013-01-30 Franklin S... busybox: Add rtcwake
2013-01-30 Franklin S... matrix-gui-crypto-demos: Switch to C base crypto applic...
2013-01-30 Franklin S... matrix-gui-apps-git: Pull in latest Matrix Apps changes
2013-01-30 Franklin S... ti-crypto-examples: Install OpenSSL script
2013-01-30 Franklin S... task-arago-toolchain-tisdk-target: Add task-arago-tisdk...
2013-01-30 Franklin S... task-arago-tisdk-addons: Add canutils
2013-01-30 Franklin S... linux-am335x: Add patch to Update SPI flash layout
2013-01-30 Franklin S... linux-am335x: Remove dirty tag patch
2013-01-30 Franklin S... arago-amsdk-image: Remove additional GPLv3 components
2013-01-30 Franklin S... arago.conf: Use non GPLv3 version of gettext
2013-01-30 Franklin S... gnutls: Allow non GPLv3 version of gettext to work
2013-01-30 Franklin S... gettext: Mimic patch "Make gettext 0.16.1 extend native...
2013-01-30 Franklin S... tiff: Remove xz and lzma dependency
2013-01-30 Franklin S... tisdk-image.bbclass: Add additional GPLv3 tables
2013-01-27 Franklin S... bash: Remove reserved word
2013-01-27 Franklin S... arago-image.inc: Use bash as shell instead of busybox
2013-01-27 Franklin S... bash: Use non GPLv3 version of bash
2013-01-27 Franklin S... bash: Mimic patch "Make it possible to run bash 3.2...
2013-01-27 Franklin S... tisdk-image.bbclass: Update manifest text
2013-01-27 Franklin S... sourceipk.bbclass: Remove .git directory
2013-01-27 Franklin S... Revert "board-port-labs: Tweak recipe"
2013-01-27 Michael Tadyshakpinmux-utility: Pull in Pin Mux Utility v2.4.1.0
2013-01-27 Franklin S... gst-plugins-good: Remove gconf dependency
2013-01-27 Franklin S... arago.conf: Set PREFERRED_VERSION for readline-native
2013-01-27 Eyal Reizerwl1271-demo: add license file
2013-01-27 Eyal Reizerwifi-direct-demo: add license info
2013-01-27 Eyal Reizerbattleship: update license information
2013-01-26 Franklin S... linux-am335x: Update to latest am335x PSP kernel
2013-01-26 Franklin S... am33x-cm3: Update to latest firmware
2013-01-26 Franklin S... task-arago-standalone-sdk-target: Fix PREFERRED_PROVIDER
2013-01-26 Franklin S... ti-tisdk-setup: Add 12.04 as a supported OS
2013-01-26 Chase Maupinti-crypto-examples: update to latest sources and add...
2013-01-26 Chase Maupinmatrix-gui-apps-git: update to latest commit
2013-01-26 Chase Maupinti-tisdk-makefile: add ti-crypto-examples targets
2013-01-26 Chase Maupincrypto-tasks: Add ti-crypto-examples
2013-01-26 Chase Maupinti-crypto-examples: Add cryptography example C applications
2013-01-26 Eyal Reizerarago.conf: update preferred versions of wpa-supplicant...
2013-01-26 Eyal Reizerti-wifi-utils: update based on wlan r5_sp3 release
2013-01-26 Eyal Reizerwpa-supplicant: update based on wlan r5_sp3 release
2013-01-26 Eyal Reizerhostapd: update for wlan r5_sp3 release
2013-01-26 Eyal Reizerti-compat-bluetooth: update to use a different compat zip
2013-01-26 Eyal Reizerwl12xx-firmware: update for wlan r5_sp3 release
2013-01-26 Eyal Reizerti-compat-wireless-wl12xx: update for wlan r5_sp3 release
2013-01-26 Franklin S... bluez4: Re-enable hidd tool
2013-01-26 Eyal Reizerobexd: increase opp push timeout
2013-01-25 Franklin S... meta-toolchain-arago: Substitute dirname statement
2013-01-25 Dave GerlachMakefile_qml-playground: Renamed to Makefile_quick...
2013-01-25 Dave GerlachMakefile_am-benchmarks: Renamed to Makefile_arm-benchmarks
2013-01-25 Franklin S... matrix-gui-apps-git.inc: Update Matrix v2 applications
2013-01-25 Chase Maupinti-tisdk-setup: Pull latest sources for create-sdcard fix
2013-01-25 Franklin S... qt-tstat: Remove proxy settings
2013-01-25 Franklin S... busybox: Enable rev utility
2013-01-25 Franklin S... ti-tisdk-setup: Switch back filesystem file type
2013-01-25 Chase Maupintisdk-image: Fix missing header in SW manifest
2013-01-25 Franklin S... tisdk-rootfs-image: Build on top of arago-base-tisdk...
2013-01-25 Chase Maupintisdk-image: Package gz file systems by default
2013-01-25 Chase Maupinarago-amsdk-image: use gz compression instead of bz2
2013-01-25 Franklin S... arago.conf: Remove commercial license whitelisting
2013-01-25 Franklin S... gst-plugins-bad: Disable any feature based on mpeg2...
2013-01-25 Franklin S... libav: Disable any mp3 or mpeg2 related features
2013-01-25 Franklin S... task-arago-gst: Remove gst-plugins-ugly
2013-01-25 Franklin S... task-arago-tisdk-amsdk: Add mount-sdcard init script
2013-01-25 Franklin S... mount-sdcard: Add recipe that automounts SD Card partitions
2013-01-25 Franklin S... task-arago-qte-toolchain-target: Add additional packages
2013-01-25 Franklin S... task-arago-qte: Add additional packages
2013-01-25 Franklin S... task-arago-qte-sdk-target: Delete unused task
2013-01-25 dgerlachalsa-state: Creating empty asound.conf file
2013-01-25 Franklin S... arago-source-ipk: Create source ipk file for oe-layersetup
2013-01-25 Franklin S... oe-layersetup: Add oe-layersetup script
2013-01-25 Franklin S... task-arago-tisdk-matrix: Fix syntax for am180x-evm...
2013-01-25 Franklin S... task-arago-tisdk-matrix: Add back Bluetooth and WLAN...
2013-01-25 Franklin S... task-arago-tisdk-connectivity: Add back battleship...
2013-01-25 Franklin S... task-arago-tisdk-connectivity: Add back wlan and blueto...
2013-01-25 Franklin S... ti-compat-bluetooth: Port ti-compat-bluetooth recipe
2013-01-25 Franklin S... ti-compat-wireless: Port ti-compat-wireless recipe.
2013-01-23 Eyal Reizerbattleship: Fix build issue when upgrading qt4
2013-01-23 Eyal Reizerbluetooth-gui: Fix segmentation fault on exit
2013-01-23 Eyal Reizerwifi-direct-demo: fix segmentation error on exit
2013-01-23 Franklin S... arago.conf: Use bluez-hcidump version 2.2
2013-01-23 Franklin S... bluez-hcidump: Pull in bluez-hcidump from Arago
next