recipes-kernel: Add GLSDK specific kernel tree for omap-a15 * Machine compatible with only omap-a15 devices. * The TI Staging tree will not be used to maintain K3.8. Instead, this new tree is set up as a production tree. Pending features for 3.8 will be implemented on this tree. - Backported features from linux mainline - Backported bug-fixes from linux mainline and linux-stable. - Features implemented by the GLSDK team which maybe product specific. This is the tree on which GLSDK kernel releases will be made. * This recipe is based off the Core SDK 2013.04.02 released kernel recipe - recipes-kernel/linux/linux-ti-staging_3.8.bb Signed-off-by: Siddharth Heroor <heroor@ti.com> cc: Mrinmayee Hingolikar <mrinmayee@ti.com> Acked-by: Chase Maupin <chase.maupin@ti.com> Signed-off-by: Denys Dmytriyenko <denys@ti.com>
omap3-sgx-modules: remove unnecessary patches for x11, cleanup old patch Signed-off-by: Denys Dmytriyenko <denys@ti.com>
libgles-omap3-x11: add missing X11 version of the recipe, after it got split Signed-off-by: Denys Dmytriyenko <denys@ti.com>
libgles-omap3: don't RCONFLICT/RREPLACE no-x version with x11 as it breaks non-X distros * Enables building/installing both X11 and RAW libs/demos. Plus otherwise the build is broken for non-X distros, as it pulls in X11 deps due to RREPLACES... * Fix broken DEPENDS copy/paste typo. * Also, clean up after the previous changes - extra empty lines, indentation, etc. Signed-off-by: Denys Dmytriyenko <denys@ti.com>
omap3-sgx-modules-x11: Separate X11 SGX driver package into new recipe omap3-sgx-modules now contains only non-X11 drivers. The X11 driver is available in the omap3-sgx-modules-x11 package. Signed-off-by: Prabindh Sundareson <prabu at ti.com> Signed-off-by: Denys Dmytriyenko <denys@ti.com>
libgles-omap3-x11: Separate X11 SGX driver package into new recipe libgles-omap3 now contains only non-X11 drivers. The X11 driver is available in the libgles-omap3-x11 package. This package has dependency on specific kernel versions for DRM builds. Signed-off-by: Prabindh Sundareson <prabu at ti.com> Signed-off-by: Denys Dmytriyenko <denys@ti.com>
libgles-omap3: Package files with right permission This patch adds correct permissions for startup script pvr-init. This is part of a clean up of the Graphics recipe starting from 4.09.00.01 version of the Graphics SDK. Signed-off-by: Prabindh Sundareson <prabu at ti.com> Signed-off-by: Denys Dmytriyenko <denys@ti.com>
libgles-omap3: Add missing RPROVIDES RPROVIDES specifies the libraries that are dynamically loaded at runtime. This patch fixes "no package provides libGLESv2.so" and similar errors that occur when including packages like qtbase. Signed-off-by: Prabindh Sundareson <prabu at ti.com> Signed-off-by: Denys Dmytriyenko <denys@ti.com>
libgles-omap3: Remove copying of unused header files Current recipe copies lot of headers that are unused, including unsupported files for OpenVG. This patch removes copying of such files. Signed-off-by: Prabindh Sundareson <prabu at ti.com> Signed-off-by: Denys Dmytriyenko <denys@ti.com>
libgles-omap3: Remove OpenVG references OpenVG API is no longer supported in the SGX Graphics SDK. Customers are encouraged to move to OpenGL ES2.x. Signed-off-by: Prabindh Sundareson <prabu at ti.com> Signed-off-by: Denys Dmytriyenko <denys@ti.com>
libgles-omap3: Remove unsupported core build option ES2.0 ES2.0 build option for SGX user binaries is deprecated as the corresponding SOC is no longer in production Signed-off-by: Prabindh Sundareson <prabu at ti.com> Signed-off-by: Denys Dmytriyenko <denys@ti.com>
omap3-sgx-modules: Remove X11 related build and packaging SGX530 driver for X11 is only buildable and testable standalone with the pre-built X11 package provided with the Graphics SDK. This patch removes X11 build from the default kernel module recipe, to enable moving X11 build to a separate recipe. This is part of a clean up of the Graphics recipe starting from 4.09.00.01 version of the Graphics SDK. Signed-off-by: Prabindh Sundareson <prabu at ti.com> Signed-off-by: Denys Dmytriyenko <denys@ti.com>
libgles-omap3: Remove X11 related build and packaging SGX530 driver for X11 is only buildable and testable standalone with the pre-built X11 package provided with the Graphics SDK. This patch removes X11 build from the default recipe, to enable moving X11 build to a separate recipe. This is part of a clean up of the Graphics recipe starting from 4.09.00.01 version of the Graphics SDK. Signed-off-by: Prabindh Sundareson <prabu at ti.com> Signed-off-by: Denys Dmytriyenko <denys@ti.com>
u-boot-dra7xx: add latest u-boot from the integration branch While the code is being pulled from ti-u-boot integration tree, J6/DRA7xx bring up is being done from a separate branch that does not include all the commits made for am335x. Hence, until those branches are merged with the mainline and unified in a single recipe, a separate recipe just for DRA7xx makes more sense. This recipe should eventually go away and unified under u-boot-ti-staging one. Signed-off-by: Denys Dmytriyenko <denys@ti.com> Acked-by: Chase Maupin <chase.maupin@ti.com>