sdcard_image bbclass: make ext4 the default Signed-off-by: Koen Kooi <koen@dominion.thruhere.net> Signed-off-by: Denys Dmytriyenko <denys@ti.com>
sdcard_image: Add image version info to root fs Signed-off-by: Joel A Fernandes <joelagnel@ti.com> Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
sdcard_image bbclass: run genex2fs directly on the loop device Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
sdcard_image: add dependency on native ext2 utilities Signed-off-by: Peter A. Bigot <bigotp@acm.org> Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
sdcard_image bbclass: reinstate vfat copy of uImage Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
sdcard_image bbclass: switch to vfat layout Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
sdcard_image bbclass: add proper ext4 support, fix inode calculations, etc, etc Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
sdcard_image bbclass: add ext4 support note Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
sdcard_image bbclass: increas inode count again Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
sdcard_image bbclass: make payload errors non-fatal
sdcard_image bbclass: fix payload logic Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
sdcard_image bbclass: add support to copy over payload from rootfs to vfat Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
sdcard_image bbclass: add timestamp to image filename Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
sdimage_class: eliminate 2GB exception for BeagleBone Gerald has said his supply of 2GB SD cards for BeagleBone has gone away, so we are back to 4GB cards. No more need for this exeption: Signed-off-by: Jason Kridner <jdk@ti.com> Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
sdcard_image bbclass: raise number of inodes to avoid out of space errors Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Revert "sdcard_image: align partitions with flash pages" This has 2 problems: 1) | Warning: partition 1 does not end at a cylinder boundary | | sfdisk: I don't like these partitions - nothing changed. 2) CCCCCCCCC on the beaglebone, the ROM code doesn't accept it after fixing 1) with --force This reverts commit ed09701ebe89d4ce0802cf734aa25c29e94febe8.
sdcard_image: align partitions with flash pages * Align partitions for SD card performance/wear optimization. For more details, please see: http://sakoman.com/OMAP/a-script-for-partitioningformatting-a-bootable-sdmicrosd-card.html # Modifications to align partitioning by Steve Sakoman # based on work by Arnd Bergmann # Align partitions for SD card performance/wear optimization # FAT partition size is 131072 sectors (64MB) less: # MBR - 1 sector # padding to align to the page size of the underlying flash - 127 sectors # so we start the first partition at sector 128 and make it 131072 - 128 = 130944 sectors # second partition starts at 131072 and continues to fill the card Signed-off-by: Jason Kridner <jdk@ti.com> Signed-off-by: Denys Dmytriyenko <denys@ti.com>
sdcard_image bbclass: reinstate uEnv.txt copying Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
sdcard image bbclass: don't copy uEnv.txt for the time being Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
sdcard_image bblass: set beaglebone VFAT label to 'BEAGLE_BONE'