u-boot-dra7xx: add latest u-boot from the integration branch While the code is being pulled from ti-u-boot integration tree, J6/DRA7xx bring up is being done from a separate branch that does not include all the commits made for am335x. Hence, until those branches are merged with the mainline and unified in a single recipe, a separate recipe just for DRA7xx makes more sense. This recipe should eventually go away and unified under u-boot-ti-staging one. Signed-off-by: Denys Dmytriyenko <denys@ti.com> Acked-by: Chase Maupin <chase.maupin@ti.com>
omap5-evm: update U-Boot machine to omap5 uevm * The U-Boot config to be used in the latest code has been updated to use omap5_uevm instead of omap5_evm. * Update to the latest code to pickup this change and modify the machine file as well. Signed-off-by: Chase Maupin <Chase.Maupin@ti.com> Signed-off-by: Denys Dmytriyenko <denys@ti.com>
linux-ti-staging: Add panda dts file as supported DTS * Add the omap5-panda.dts file as a supported DTS to be built. This file is for use on the panda and uEVM boards. Signed-off-by: Chase Maupin <Chase.Maupin@ti.com> Signed-off-by: Denys Dmytriyenko <denys@ti.com>
omap5-evm: Add OMAP5 EVM configuration * Add the machine configuration for the OMAP5 EVM device. * Create the omap-a15.inc file to be shared with all OMAP Cortex-A15 derivative devices. Signed-off-by: Chase Maupin <Chase.Maupin@ti.com> Signed-off-by: Denys Dmytriyenko <denys@ti.com>
beagleboard: switch default u-boot preference to machine-specific tree SDKs or other users of meta-ti can still use one of the other recipes for stability or featureset, by setting PREFERRED_PROVIDER in their config. Signed-off-by: Denys Dmytriyenko <denys@ti.com>
am180x: switch default u-boot preference to machine-specific tree SDKs or other users of meta-ti can still use one of the other recipes for stability or featureset, by setting PREFERRED_PROVIDER in their config. Signed-off-by: Denys Dmytriyenko <denys@ti.com>
keystone: switch default u-boot preference to machine-specific tree SDKs or other users of meta-ti can still use one of the other recipes for stability or featureset, by setting PREFERRED_PROVIDER in their config. Signed-off-by: Denys Dmytriyenko <denys@ti.com>
ti33x: switch default preference to ti-staging tree SDKs or other users of meta-ti can still use one of the older 3.2 recipes for stability or featureset, by setting PREFERRED_PROVIDER in distro or local config. Signed-off-by: Denys Dmytriyenko <denys@ti.com> Acked-by: Chase Maupin <chase.maupin@ti.com>