u-boot-am33x: modify am33x specific version to use new namespace feature Signed-off-by: Denys Dmytriyenko <denys@ti.com>
u-boot_2011.09[.10rc]: Always use gnu ld for LD - Pull in gnu ld patch for 2011.10rc recipe - Bump PR Signed-off-by: Roger Monk <r-monk@ti.com> Signed-off-by: Denys Dmytriyenko <denys@ti.com>
u-boot 2011.09+git: update to latest version of Tom Rini's tree Signed-off-by: Koen Kooi <koen@dominion.thruhere.net> Signed-off-by: Denys Dmytriyenko <denys@ti.com>
u-boot 2011.09+git: update to latest version of Tom Rini's tree All patches have been rediffed and boot tested Signed-off-by: Koen Kooi <koen@dominion.thruhere.net> Signed-off-by: Denys Dmytriyenko <denys@ti.com>
u-boot 2011.10rc: fix loading from /boot by adding ext4 support This patchset was pulled from u-boot patchwork and aren't final, but testing on beaglebone shows it to work. Signed-off-by: Koen Kooi <koen@dominion.thruhere.net> Acked-by: Tom Rini <trini@ti.com> Signed-off-by: Denys Dmytriyenko <denys@ti.com>
u-boot 2011.09: add patch to support 'cold' AM335x silicon Signed-off-by: Koen Kooi <koen@dominion.thruhere.net> Signed-off-by: Denys Dmytriyenko <denys@ti.com>
u-boot: cleanup Set compatible machine in all recipes, remove deprecated versions for some machines Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
u-boot 2011.10rc: enable i2c2 for beaglebone Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
u-boot: enhance deploy symlinking logic It will now deploy: u-boot-<machine>-<version>.suffix u-boot-<machine>.suffix (symlink) u-boot.suffix (symlink) And additionally for SPL builds: MLO-<machine>-<version> MLO-<machine> (symlink) MLO (symlink) Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
u-boot 2011.10rc: fatload does not set loadaddr, so be explicit Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
u-boot 2011.10rc: uboot extX loading is 20 times slower than vfat loading :( Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
u-boot 2011.10rc: turn on dcache for beaglebone Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
u-boot 2011.10rc: move beaglebone to ext4 Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
U-boot 2011.10rc: Refresh PMIC patch with Rev A1 fixes Signed-off-by: Joel A Fernandes <joelagnel@ti.com> Acked-by: Tom Rini <trini@ti.com> Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
u-boot 2011.10rc: Fix pmic shut down over USB power These are some fixes suggested by Jason Kridner to fix the PMIC instabilities we've been seeing over USB power. Signed-off-by: Joel A Fernandes <joelagnel@ti.com> Cc: Jason Kridner <jdk@ti.com> Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
u-boot 2011.10rc: tweak loadaddress for faster boot Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
u-boot 2011.10rc: update SRCREV and rediff patches Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
u-boot 2011.10rc: Read EEPROM header correctly for BeagleBone board detection This patch fixes the case where the EEPROM is programmed but we still use the fall back case to detect the bone board. Now that EEPROMs are programmed, we should correctly detect the bone board instead of relying on fall back to bone mode. PR bumped Signed-off-by: Joel A Fernandes <joelagnel@ti.com> Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
u-boot 2011.10rc: remove beaglebone machine ID patch Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
u-boot 2011.10rc: update to the latest revision Updated to latest version to pick up the following changes: * 9158d7f am335x: Really correct NAND partiton layout * 4723773 am335x: Wrap spl_board_init in a CONFIG_SPL_BOARD_INIT check * 40c310c Change CPU to 720MHz and bump VDD1 to 1.26V * 9c154ee Add missing i2c0 pin mux configuration in spl_board_init Signed-off-by: Denys Dmytriyenko <denys@ti.com> Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>