recipes-kernel: Add GLSDK specific kernel tree for omap-a15 * Machine compatible with only omap-a15 devices. * The TI Staging tree will not be used to maintain K3.8. Instead, this new tree is set up as a production tree. Pending features for 3.8 will be implemented on this tree. - Backported features from linux mainline - Backported bug-fixes from linux mainline and linux-stable. - Features implemented by the GLSDK team which maybe product specific. This is the tree on which GLSDK kernel releases will be made. * This recipe is based off the Core SDK 2013.04.02 released kernel recipe - recipes-kernel/linux/linux-ti-staging_3.8.bb Signed-off-by: Siddharth Heroor <heroor@ti.com> cc: Mrinmayee Hingolikar <mrinmayee@ti.com> Acked-by: Chase Maupin <chase.maupin@ti.com> Signed-off-by: Denys Dmytriyenko <denys@ti.com>
linux-ti-staging: Add dra7xx-evm support * Add the DTB entries for the dra7xx-evm machine type * Update to the latest git sources which have dra7xx-evm support. * Update the PV to match the latest source version Signed-off-by: Chase Maupin <Chase.Maupin@ti.com> Signed-off-by: Denys Dmytriyenko <denys@ti.com>
am33x-cm3: Split init script into its own package * 3.8+ kernels use an init script to load the cm3 firmware. * 3.2 kernel require the cm3 firmware during compile time therefore no init script is needed. * Separate the init script from the main package and place it in its own package. Signed-off-by: Denys Dmytriyenko <denys@ti.com>
linux-am335x: Update to latest 3.2 kernel release * Update to the latest PSP release (version 04.06.00.10) of the 3.2 kernel. * Rename recipe to match meta-ti kernel recipe naming convention. * Use in tree defconfig instead of providing a separate defconfig. These defconfigs were the same anyway. * Add additional crypto patches that were needed to fix suspend and resume issues. Signed-off-by: Franklin S. Cooper Jr <fcooper@ti.com> Signed-off-by: Denys Dmytriyenko <denys@ti.com>
linux-ti-staging: make cm3 firmware a run-time dependency * Make the am33x-cm3 firmware a run-time dependency instead of build time since it is no longer required at build time. Signed-off-by: Chase Maupin <Chase.Maupin@ti.com> Signed-off-by: Denys Dmytriyenko <denys@ti.com>
setup-defconfig: allow using KERNEL_LOCALVERSION * Add capability to use KERNEL_LOCALVERSION to set an extra version string in the kernel. This mimics functionality submitted to the kernel.bbclass but since this overwrites the do_configure it must be added here as well. Signed-off-by: Chase Maupin <Chase.Maupin@ti.com> Signed-off-by: Denys Dmytriyenko <denys@ti.com>
linux: Use setup-defconfig in kernel recipes * Now that the setup-defconfig.inc file has been moved to the meta-ti layer the kernel recipes should include this file. * This makes way to clear this inclusion from the bbappend files in meta-arago Signed-off-by: Chase Maupin <Chase.Maupin@ti.com> Signed-off-by: Denys Dmytriyenko <denys@ti.com>
linux-ti-staging: rename to have version in name, update to latest * Update to the latest kernel sources. This also requires changing the dtb file names since the omap5 devices have changed to use uevm instead of panda and sevm instead of evm. Signed-off-by: Denys Dmytriyenko <denys@ti.com> Signed-off-by: Chase Maupin <Chase.Maupin@ti.com>
linux-ti-staging: Add panda dts file as supported DTS * Add the omap5-panda.dts file as a supported DTS to be built. This file is for use on the panda and uEVM boards. Signed-off-by: Chase Maupin <Chase.Maupin@ti.com> Signed-off-by: Denys Dmytriyenko <denys@ti.com>
linux-ti-staging: Add OMAP5 support * Add the KERNEL_DEVICETREE definitions for omap5-evm * Add the omap-a15 SOC_FAMILY to the list of COMPATIBLE_MACHINEs Signed-off-by: Chase Maupin <Chase.Maupin@ti.com> Signed-off-by: Denys Dmytriyenko <denys@ti.com>