linux-ti33x-psp 3.2: switch ADC to 16x averaging, disable 275MHz, add 4.3" LCD support
[glsdk/meta-ti-glsdk.git] / README
1 The official OpenEmbedded/Yocto BSP layer for Texas Instruments platforms.
3 It is hosted on http://git.yoctoproject.org/cgit/cgit.cgi/meta-ti/ with the
4 source repository at git://git.yoctoproject.org/meta-ti
7 This layer depends on:
9 URI: git://git.openembedded.org/openembedded-core
10 layers: meta
11 branch: master
14 When not depending on meta-openembedded and not using systemd, you may need to
15 mask few miscellaneous recipes requiring systemd, by adding this to local.conf:
17 BBMASK = "meta-ti/recipes-misc"
20 The base BSP part of meta-ti should work with different OpenEmbedded/Yocto
21 distributions and layer stacks, such as:
22 distro-less (only with OE-Core), with Yocto/Poky, with Angstrom or Arago.
24 Please follow the recommended setup procedures of your OE distribution.
27 Send pull requests, patches, comments or questions to meta-ti@yoctoproject.org
29 Maintainers: Denys Dmytriyenko <denys@ti.com>
30              Koen Kooi <koen@dominion.thruhere.net>