bonescript: update to latest git
[glsdk/meta-ti-glsdk.git] / README
1 This layer hard depends on:
3 URI: git://git.openembedded.org/openembedded-core
4 branch: master
5 revision: HEAD
7 URI: git://git.openembedded.org/meta-openembedded
8 branch: master
9 revision: HEAD
11 And optionally depends on:
13 URI: git://git.angstrom-distribution.org/meta-angstrom
14 branch: master
15 revision: HEAD
17 Currently meta-ti only works with the Angstrom distribution and hence
18 requires the meta-angstrom layer. There are known issues when using
19 gcc-4.6 based toolchain from OpenEmbedded-Core, thus gcc-4.5 toolchain,
20 provided by meta-openembedded, is needed. It is planned to fix these
21 shortcomings in the near future and allow building the base BSP part
22 of meta-ti with different distributions and layer stacks, such as:
23 distro-less (only with OE-Core), with Yocto/Poky, with Angstrom or
24 Arago.
26 Due to the above, it is now recommended to follow the instructions at
27 http://www.angstrom-distribution.org/building-angstrom
29 This will set it up for the OpenEmbedded-core ('yocto') layout instead
30 of the old "Classic" OpenEmbedded-dev layout. You can optionally tweak
31 sources/layers.txt and conf/bblayers.conf to (de)select BSP layers.
33 Send pull requests to meta-ti@yoctoproject.org
35 Main layer maintainers: Denys Dmytriyenko <denys@ti.com>
36                         Koen Kooi <k-kooi@ti.com>