README: refer to toolchain-layer in meta-openembedded
[glsdk/meta-ti-glsdk.git] / classes / sdcard_image.bbclass
1 inherit image
3 # Add the fstypes we need
4 IMAGE_FSTYPES_append = " tar.bz2 sdimg"
6 # Ensure required utilities are present
7 IMAGE_DEPENDS_sdimg = "genext2fs-native e2fsprogs-native"
9 # Change this to match your host distro
10 LOSETUP ?= "/sbin/losetup"
12 # Since these need to go in /etc/fstab we can hardcode them
13 # Since the vars are weakly assigned, you can override them from your local.conf
14 LOOPDEV ?= "/dev/loop1"
15 LOOPDEV_BOOT ?= "/dev/loop2"
16 LOOPDEV_FS ?= "/dev/loop3"
18 # Default to 4GiB images
19 SDIMG_SIZE ?= "444" 
21 # FS type for rootfs
22 ROOTFSTYPE ?= "ext3"
24 BOOTPARTNAME_beaglebone = "BEAGLE_BONE"
25 BOOTPARTNAME ?= "${MACHINE}"
27 IMAGEDATESTAMP = "${@time.strftime('%Y.%m.%d',time.gmtime())}"
29 # Files and/or directories to be copied into the vfat partition
30 FATPAYLOAD ?= ""
32 IMAGE_CMD_sdimg () {
33         SDIMG=${WORKDIR}/sd.img
35         # sanity check fstab entry for boot partition mounting
36         if [ "x$(cat /etc/fstab | grep ${LOOPDEV_BOOT} | grep ${WORKDIR}/tmp-mnt-boot | grep user || true)" = "x" ]; then
37                 echo "/etc/fstab entries need to be created with the user flag for the loop devices like:"
38                 echo "${LOOPDEV_BOOT} ${WORKDIR}/tmp-mnt-boot vfat user 0 0"
39         false
40         fi
42         # cleanup loops
43         for loop in ${LOOPDEV} ${LOOPDEV_BOOT} ${LOOPDEV_FS} ; do
44                 ${LOSETUP} -d $loop || true
45         done
47         # If an SD image is already present, reuse and reformat it
48         if [ ! -e ${SDIMG} ] ; then
49                 dd if=/dev/zero of=${SDIMG} bs=$(echo '255 * 63 * 512' | bc) count=${SDIMG_SIZE}
50         fi
52         ${LOSETUP} ${LOOPDEV} ${SDIMG}
54         # Create partition table
55         dd if=/dev/zero of=${LOOPDEV} bs=1024 count=1024
56         SIZE=$(/sbin/fdisk -l ${LOOPDEV} | grep Disk | grep bytes | awk '{print $5}')
57         CYLINDERS=$(echo $SIZE/255/63/512 | bc)
58         {
59         echo ,9,0x0C,*
60         echo ,,,-
61         } | /sbin/sfdisk -D -H 255 -S 63 -C ${CYLINDERS} ${LOOPDEV}
63         # Prepare loop devices for boot and filesystem partitions
64         BOOT_OFFSET=32256
65         FS_OFFSET_SECT=$(/sbin/fdisk -l -u ${LOOPDEV} 2>&1 | grep Linux | perl -p -i -e "s/\s+/ /"|cut -d " " -f 2)
66         FS_OFFSET=$(echo "$FS_OFFSET_SECT * 512" | bc)
67         FS_SIZE_BLOCKS=$(/sbin/fdisk -l -u ${LOOPDEV} 2>&1 | grep Linux | perl -p -i -e "s/\s+/ /g" \ 
68         |cut -d " " -f 4 | cut -d "+" -f 1)
69  
70         LOOPDEV_BLOCKS=$(/sbin/fdisk -l -u ${LOOPDEV} 2>&1 | grep FAT | perl -p -i -e "s/\s+/ /g"|cut -d " " -f 5)
71         LOOPDEV_BYTES=$(echo "$LOOPDEV_BLOCKS * 1024" | bc)
73         ${LOSETUP} -d ${LOOPDEV}
75         ${LOSETUP} ${LOOPDEV_BOOT} ${SDIMG} -o ${BOOT_OFFSET} 
77         /sbin/mkfs.vfat ${LOOPDEV_BOOT} -n ${BOOTPARTNAME} $LOOPDEV_BLOCKS
79         # Prepare filesystem partition
80         # Copy ubi used by flashing scripts
81         if [ -e  ${DEPLOY_DIR_IMAGE}/${IMAGE_NAME}.rootfs.ubi ] ; then
82                 echo "Copying UBIFS image to file system"
83                 cp ${DEPLOY_DIR_IMAGE}/${IMAGE_NAME}.rootfs.ubi ${IMAGE_ROOTFS}/boot/fs.ubi
84         fi
86         # Prepare boot partion. First mount the boot partition, and copy the boot loader and supporting files
87         # from the root filesystem
89         mkdir -p ${WORKDIR}/tmp-mnt-boot
90         mount $LOOPDEV_BOOT ${WORKDIR}/tmp-mnt-boot
92         echo "Copying bootloaders into the boot partition"
93         if [ -e ${IMAGE_ROOTFS}/boot/MLO ] ; then
94                 cp -v ${IMAGE_ROOTFS}/boot/MLO ${WORKDIR}/tmp-mnt-boot 
95         else
96                 cp -v ${DEPLOY_DIR_IMAGE}/MLO ${WORKDIR}/tmp-mnt-boot
97         fi
99         # Check for u-boot SPL
100         if [ -e ${DEPLOY_DIR_IMAGE}/u-boot-${MACHINE}.img ] ; then
101                 suffix=img
102         else
103                 suffix=bin
104         fi
106         cp -v ${IMAGE_ROOTFS}/boot/uEnv.txt ${WORKDIR}/tmp-mnt-boot || true
107         cp -v ${IMAGE_ROOTFS}/boot/user.txt ${WORKDIR}/tmp-mnt-boot || true
108         cp -v ${IMAGE_ROOTFS}/boot/uImage ${WORKDIR}/tmp-mnt-boot || true
110         if [ -e ${IMAGE_ROOTFS}/boot/u-boot.$suffix ] ; then
111                 cp -v ${IMAGE_ROOTFS}/boot/{u-boot.$suffix} ${WORKDIR}/tmp-mnt-boot || true
112         else
113                 cp -v ${DEPLOY_DIR_IMAGE}/u-boot-${MACHINE}.$suffix ${WORKDIR}/tmp-mnt-boot/u-boot.$suffix 
114         fi
116         if [ -n ${FATPAYLOAD} ] ; then
117                 echo "Copying payload into VFAT"
118                 for entry in ${FATPAYLOAD} ; do
119                                 # add the || true to stop aborting on vfat issues like not supporting .~lock files
120                                 cp -av ${IMAGE_ROOTFS}$entry ${WORKDIR}/tmp-mnt-boot || true
121                 done
122         fi
124         echo "${IMAGE_NAME}-${IMAGEDATESTAMP}" > ${IMAGE_ROOTFS}/etc/image-version-info
126         # Cleanup VFAT mount
127         echo "Cleaning up VFAT mount"
128         umount ${WORKDIR}/tmp-mnt-boot
129         ${LOSETUP} -d ${LOOPDEV_BOOT} || true
131         # Prepare rootfs parition
132         echo "Creating rootfs loopback"
133         ${LOSETUP} ${LOOPDEV_FS} ${SDIMG} -o ${FS_OFFSET}
135         FS_NUM_INODES=$(echo $FS_SIZE_BLOCKS / 4 | bc)
137         case "${ROOTFSTYPE}" in
138                 ext3)
139                                 genext2fs -z -N $FS_NUM_INODES -b $FS_SIZE_BLOCKS -d ${IMAGE_ROOTFS} ${LOOPDEV_FS}
140                                 tune2fs -L ${IMAGE_NAME} -j ${LOOPDEV_FS}
141                                 ;;
142                 ext4)
143                                 genext2fs -z -N $FS_NUM_INODES -b $FS_SIZE_BLOCKS -d ${IMAGE_ROOTFS} ${LOOPDEV_FS}
144                                 tune2fs -L ${IMAGE_NAME} -j -O extents,uninit_bg,dir_index ${LOOPDEV_FS}
145                                 ;;
146                 *)
147                                 echo "Please set ROOTFSTYPE to something supported"
148                                 exit 1
149                                 ;;
150         esac
152         ${LOSETUP} -d ${LOOPDEV_FS} || true
154         gzip -c ${WORKDIR}/sd.img > ${DEPLOY_DIR_IMAGE}/${IMAGE_NAME}-${IMAGEDATESTAMP}.img.gz
155         rm -f ${WORKDIR}/sd.img