linux-omap 2.6.37: sync with OE .dev
[glsdk/meta-ti-glsdk.git] / recipes-bsp / linux / linux-omap / media / 0010-media-Entities-pads-and-links.patch
1 From b4697e5a8ad1e564ea378d435c2ce190318c1027 Mon Sep 17 00:00:00 2001
2 From: Laurent Pinchart <laurent.pinchart@ideasonboard.com>
3 Date: Wed, 9 Dec 2009 12:40:00 +0100
4 Subject: [PATCH 10/43] media: Entities, pads and links
6 As video hardware pipelines become increasingly complex and
7 configurable, the current hardware description through v4l2 subdevices
8 reaches its limits. In addition to enumerating and configuring
9 subdevices, video camera drivers need a way to discover and modify at
10 runtime how those subdevices are connected. This is done through new
11 elements called entities, pads and links.
13 An entity is a basic media hardware building block. It can correspond to
14 a large variety of logical blocks such as physical hardware devices
15 (CMOS sensor for instance), logical hardware devices (a building block
16 in a System-on-Chip image processing pipeline), DMA channels or physical
17 connectors.
19 A pad is a connection endpoint through which an entity can interact with
20 other entities. Data (not restricted to video) produced by an entity
21 flows from the entity's output to one or more entity inputs. Pads should
22 not be confused with physical pins at chip boundaries.
24 A link is a point-to-point oriented connection between two pads, either
25 on the same entity or on different entities. Data flows from a source
26 pad to a sink pad.
28 Links are stored in the source entity. To make backwards graph walk
29 faster, a copy of all links is also stored in the sink entity. The copy
30 is known as a backlink and is only used to help graph traversal.
32 The entity API is made of three functions:
34 - media_entity_init() initializes an entity. The caller must provide an
35 array of pads as well as an estimated number of links. The links array
36 is allocated dynamically and will be reallocated if it grows beyond the
37 initial estimate.
39 - media_entity_cleanup() frees resources allocated for an entity. It
40 must be called during the cleanup phase after unregistering the entity
41 and before freeing it.
43 - media_entity_create_link() creates a link between two entities. An
44 entry in the link array of each entity is allocated and stores pointers
45 to source and sink pads.
47 When a media device is unregistered, all its entities are unregistered
48 automatically.
50 The code is based on Hans Verkuil <hverkuil@xs4all.nl> initial work.
52 Signed-off-by: Laurent Pinchart <laurent.pinchart@ideasonboard.com>
53 Signed-off-by: Sakari Ailus <sakari.ailus@maxwell.research.nokia.com>
54 ---
55  Documentation/DocBook/v4l/media-controller.xml |   20 +++
56  Documentation/media-framework.txt              |  151 ++++++++++++++++++++++++
57  drivers/media/Makefile                         |    2 +-
58  drivers/media/media-device.c                   |   56 +++++++++
59  drivers/media/media-entity.c                   |  147 +++++++++++++++++++++++
60  include/media/media-device.h                   |   19 +++
61  include/media/media-entity.h                   |  122 +++++++++++++++++++
62  7 files changed, 516 insertions(+), 1 deletions(-)
63  create mode 100644 drivers/media/media-entity.c
64  create mode 100644 include/media/media-entity.h
66 diff --git a/Documentation/DocBook/v4l/media-controller.xml b/Documentation/DocBook/v4l/media-controller.xml
67 index 253ddb4..f89228d 100644
68 --- a/Documentation/DocBook/v4l/media-controller.xml
69 +++ b/Documentation/DocBook/v4l/media-controller.xml
70 @@ -53,4 +53,24 @@
71      implementing policies that belong to userspace.</para>
72      <para>The media controller API aims at solving those problems.</para>
73    </section>
74 +
75 +  <section id="media-controller-model">
76 +    <title>Media device model</title>
77 +    <para>Discovering a device internal topology, and configuring it at runtime,
78 +    is one of the goals of the media controller API. To achieve this, hardware
79 +    devices are modelled as an oriented graph of building blocks called entities
80 +    connected through pads.</para>
81 +    <para>An entity is a basic media hardware or software building block. It can
82 +    correspond to a large variety of logical blocks such as physical hardware
83 +    devices (CMOS sensor for instance), logical hardware devices (a building
84 +    block in a System-on-Chip image processing pipeline), DMA channels or
85 +    physical connectors.</para>
86 +    <para>A pad is a connection endpoint through which an entity can interact
87 +    with other entities. Data (not restricted to video) produced by an entity
88 +    flows from the entity's output to one or more entity inputs. Pads should not
89 +    be confused with physical pins at chip boundaries.</para>
90 +    <para>A link is a point-to-point oriented connection between two pads,
91 +    either on the same entity or on different entities. Data flows from a source
92 +    pad to a sink pad.</para>
93 +  </section>
94  </chapter>
95 diff --git a/Documentation/media-framework.txt b/Documentation/media-framework.txt
96 index 1844c3f..b252cf9 100644
97 --- a/Documentation/media-framework.txt
98 +++ b/Documentation/media-framework.txt
99 @@ -13,6 +13,30 @@ Documentation/DocBook/v4l/media-controller.xml. This document will focus on
100  the kernel-side implementation of the media framework.
101  
102  
103 +Abstract media device model
104 +---------------------------
106 +Discovering a device internal topology, and configuring it at runtime, is one
107 +of the goals of the media framework. To achieve this, hardware devices are
108 +modeled as an oriented graph of building blocks called entities connected
109 +through pads.
111 +An entity is a basic media hardware building block. It can correspond to
112 +a large variety of logical blocks such as physical hardware devices
113 +(CMOS sensor for instance), logical hardware devices (a building block
114 +in a System-on-Chip image processing pipeline), DMA channels or physical
115 +connectors.
117 +A pad is a connection endpoint through which an entity can interact with
118 +other entities. Data (not restricted to video) produced by an entity
119 +flows from the entity's output to one or more entity inputs. Pads should
120 +not be confused with physical pins at chip boundaries.
122 +A link is a point-to-point oriented connection between two pads, either
123 +on the same entity or on different entities. Data flows from a source
124 +pad to a sink pad.
127  Media device
128  ------------
129  
130 @@ -65,3 +89,130 @@ Drivers unregister media device instances by calling
131         media_device_unregister(struct media_device *mdev);
132  
133  Unregistering a media device that hasn't been registered is *NOT* safe.
136 +Entities, pads and links
137 +------------------------
139 +- Entities
141 +Entities are represented by a struct media_entity instance, defined in
142 +include/media/media-entity.h. The structure is usually embedded into a
143 +higher-level structure, such as a v4l2_subdev or video_device instance,
144 +although drivers can allocate entities directly.
146 +Drivers initialize entities by calling
148 +       media_entity_init(struct media_entity *entity, u16 num_pads,
149 +                         struct media_pad *pads, u16 extra_links);
151 +The media_entity name, type, flags, revision and group_id fields can be
152 +initialized before or after calling media_entity_init. Entities embedded in
153 +higher-level standard structures can have some of those fields set by the
154 +higher-level framework.
156 +As the number of pads is known in advance, the pads array is not allocated
157 +dynamically but is managed by the entity driver. Most drivers will embed the
158 +pads array in a driver-specific structure, avoiding dynamic allocation.
160 +Drivers must set the direction of every pad in the pads array before calling
161 +media_entity_init. The function will initialize the other pads fields.
163 +Unlike the number of pads, the total number of links isn't always known in
164 +advance by the entity driver. As an initial estimate, media_entity_init
165 +pre-allocates a number of links equal to the number of pads plus an optional
166 +number of extra links. The links array will be reallocated if it grows beyond
167 +the initial estimate.
169 +Drivers register entities with a media device by calling
171 +       media_device_register_entity(struct media_device *mdev,
172 +                                    struct media_entity *entity);
174 +Entities are identified by a unique positive integer ID. Drivers can provide an
175 +ID by filling the media_entity id field prior to registration, or request the
176 +media controller framework to assign an ID automatically. Drivers that provide
177 +IDs manually must ensure that all IDs are unique. IDs are not guaranteed to be
178 +contiguous even when they are all assigned automatically by the framework.
180 +Drivers unregister entities by calling
182 +       media_device_unregister_entity(struct media_entity *entity);
184 +Unregistering an entity will not change the IDs of the other entities, and the
185 +ID will never be reused for a newly registered entity.
187 +When a media device is unregistered, all its entities are unregistered
188 +automatically. No manual entities unregistration is then required.
190 +Drivers free resources associated with an entity by calling
192 +       media_entity_cleanup(struct media_entity *entity);
194 +This function must be called during the cleanup phase after unregistering the
195 +entity. Note that the media_entity instance itself must be freed explicitly by
196 +the driver if required.
198 +Entities have flags that describe the entity capabilities and state.
200 +       MEDIA_ENT_FL_DEFAULT indicates the default entity for a given type.
201 +       This can be used to report the default audio and video devices or the
202 +       default camera sensor.
204 +Logical entity groups can be defined by setting the group ID of all member
205 +entities to the same non-zero value. An entity group serves no purpose in the
206 +kernel, but is reported to userspace during entities enumeration. The group_id
207 +field belongs to the media device driver and must not by touched by entity
208 +drivers.
210 +Media device drivers should define groups if several entities are logically
211 +bound together. Example usages include reporting
213 +       - ALSA, VBI and video nodes that carry the same media stream
214 +       - lens and flash controllers associated with a sensor
216 +- Pads
218 +Pads are represented by a struct media_pad instance, defined in
219 +include/media/media-entity.h. Each entity stores its pads in a pads array
220 +managed by the entity driver. Drivers usually embed the array in a
221 +driver-specific structure.
223 +Pads are identified by their entity and their 0-based index in the pads array.
224 +Both information are stored in the media_pad structure, making the media_pad
225 +pointer the canonical way to store and pass link references.
227 +Pads have flags that describe the pad capabilities and state.
229 +       MEDIA_PAD_FL_INPUT indicates that the pad supports sinking data.
230 +       MEDIA_PAD_FL_OUTPUT indicates that the pad supports sourcing data.
232 +One and only one of MEDIA_PAD_FL_INPUT and MEDIA_PAD_FL_OUTPUT must be set for
233 +each pad.
235 +- Links
237 +Links are represented by a struct media_link instance, defined in
238 +include/media/media-entity.h. Each entity stores all links originating at or
239 +targetting any of its pads in a links array. A given link is thus stored
240 +twice, once in the source entity and once in the target entity. The array is
241 +pre-allocated and grows dynamically as needed.
243 +Drivers create links by calling
245 +       media_entity_create_link(struct media_entity *source, u16 source_pad,
246 +                                struct media_entity *sink,   u16 sink_pad,
247 +                                u32 flags);
249 +An entry in the link array of each entity is allocated and stores pointers
250 +to source and sink pads.
252 +Links have flags that describe the link capabilities and state.
254 +       MEDIA_LNK_FL_ENABLED indicates that the link is enabled and can be used
255 +       to transfer media data. When two or more links target a sink pad, only
256 +       one of them can be enabled at a time.
257 +       MEDIA_LNK_FL_IMMUTABLE indicates that the link enabled state can't be
258 +       modified at runtime. If MEDIA_LNK_FL_IMMUTABLE is set, then
259 +       MEDIA_LNK_FL_ENABLED must also be set since an immutable link is always
260 +       enabled.
261 diff --git a/drivers/media/Makefile b/drivers/media/Makefile
262 index 019d3e0..b890248 100644
263 --- a/drivers/media/Makefile
264 +++ b/drivers/media/Makefile
265 @@ -2,7 +2,7 @@
266  # Makefile for the kernel multimedia device drivers.
267  #
268  
269 -media-objs     := media-device.o media-devnode.o
270 +media-objs     := media-device.o media-devnode.o media-entity.o
271  
272  ifeq ($(CONFIG_MEDIA_CONTROLLER),y)
273    obj-$(CONFIG_MEDIA_SUPPORT) += media.o
274 diff --git a/drivers/media/media-device.c b/drivers/media/media-device.c
275 index 57a9c6b..b8a3ace 100644
276 --- a/drivers/media/media-device.c
277 +++ b/drivers/media/media-device.c
278 @@ -25,6 +25,7 @@
279  
280  #include <media/media-device.h>
281  #include <media/media-devnode.h>
282 +#include <media/media-entity.h>
283  
284  static const struct media_file_operations media_device_fops = {
285         .owner = THIS_MODULE,
286 @@ -69,6 +70,10 @@ int __must_check media_device_register(struct media_device *mdev)
287         if (WARN_ON(mdev->dev == NULL || mdev->model[0] == 0))
288                 return -EINVAL;
289  
290 +       mdev->entity_id = 1;
291 +       INIT_LIST_HEAD(&mdev->entities);
292 +       spin_lock_init(&mdev->lock);
294         /* Register the device node. */
295         mdev->devnode.fops = &media_device_fops;
296         mdev->devnode.parent = mdev->dev;
297 @@ -94,7 +99,58 @@ EXPORT_SYMBOL_GPL(media_device_register);
298   */
299  void media_device_unregister(struct media_device *mdev)
300  {
301 +       struct media_entity *entity;
302 +       struct media_entity *next;
304 +       list_for_each_entry_safe(entity, next, &mdev->entities, list)
305 +               media_device_unregister_entity(entity);
307         device_remove_file(&mdev->devnode.dev, &dev_attr_model);
308         media_devnode_unregister(&mdev->devnode);
309  }
310  EXPORT_SYMBOL_GPL(media_device_unregister);
312 +/**
313 + * media_device_register_entity - Register an entity with a media device
314 + * @mdev:      The media device
315 + * @entity:    The entity
316 + */
317 +int __must_check media_device_register_entity(struct media_device *mdev,
318 +                                             struct media_entity *entity)
319 +{
320 +       /* Warn if we apparently re-register an entity */
321 +       WARN_ON(entity->parent != NULL);
322 +       entity->parent = mdev;
324 +       spin_lock(&mdev->lock);
325 +       if (entity->id == 0)
326 +               entity->id = mdev->entity_id++;
327 +       else
328 +               mdev->entity_id = max(entity->id + 1, mdev->entity_id);
329 +       list_add_tail(&entity->list, &mdev->entities);
330 +       spin_unlock(&mdev->lock);
332 +       return 0;
333 +}
334 +EXPORT_SYMBOL_GPL(media_device_register_entity);
336 +/**
337 + * media_device_unregister_entity - Unregister an entity
338 + * @entity:    The entity
339 + *
340 + * If the entity has never been registered this function will return
341 + * immediately.
342 + */
343 +void media_device_unregister_entity(struct media_entity *entity)
344 +{
345 +       struct media_device *mdev = entity->parent;
347 +       if (mdev == NULL)
348 +               return;
350 +       spin_lock(&mdev->lock);
351 +       list_del(&entity->list);
352 +       spin_unlock(&mdev->lock);
353 +       entity->parent = NULL;
354 +}
355 +EXPORT_SYMBOL_GPL(media_device_unregister_entity);
356 diff --git a/drivers/media/media-entity.c b/drivers/media/media-entity.c
357 new file mode 100644
358 index 0000000..e4ba2bc
359 --- /dev/null
360 +++ b/drivers/media/media-entity.c
361 @@ -0,0 +1,147 @@
362 +/*
363 + * Media entity
364 + *
365 + * Copyright (C) 2010 Nokia Corporation
366 + *
367 + * Contacts: Laurent Pinchart <laurent.pinchart@ideasonboard.com>
368 + *          Sakari Ailus <sakari.ailus@maxwell.research.nokia.com>
369 + *
370 + * This program is free software; you can redistribute it and/or modify
371 + * it under the terms of the GNU General Public License version 2 as
372 + * published by the Free Software Foundation.
373 + *
374 + * This program is distributed in the hope that it will be useful,
375 + * but WITHOUT ANY WARRANTY; without even the implied warranty of
376 + * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the
377 + * GNU General Public License for more details.
378 + *
379 + * You should have received a copy of the GNU General Public License
380 + * along with this program; if not, write to the Free Software
381 + * Foundation, Inc., 59 Temple Place, Suite 330, Boston, MA  02111-1307  USA
382 + */
384 +#include <linux/module.h>
385 +#include <linux/slab.h>
386 +#include <media/media-entity.h>
388 +/**
389 + * media_entity_init - Initialize a media entity
390 + *
391 + * @num_pads: Total number of input and output pads.
392 + * @extra_links: Initial estimate of the number of extra links.
393 + * @pads: Array of 'num_pads' pads.
394 + *
395 + * The total number of pads is an intrinsic property of entities known by the
396 + * entity driver, while the total number of links depends on hardware design
397 + * and is an extrinsic property unknown to the entity driver. However, in most
398 + * use cases the entity driver can guess the number of links which can safely
399 + * be assumed to be equal to or larger than the number of pads.
400 + *
401 + * For those reasons the links array can be preallocated based on the entity
402 + * driver guess and will be reallocated later if extra links need to be
403 + * created.
404 + *
405 + * This function allocates a links array with enough space to hold at least
406 + * 'num_pads' + 'extra_links' elements. The media_entity::max_links field will
407 + * be set to the number of allocated elements.
408 + *
409 + * The pads array is managed by the entity driver and passed to
410 + * media_entity_init() where its pointer will be stored in the entity structure.
411 + */
412 +int
413 +media_entity_init(struct media_entity *entity, u16 num_pads,
414 +                 struct media_pad *pads, u16 extra_links)
415 +{
416 +       struct media_link *links;
417 +       unsigned int max_links = num_pads + extra_links;
418 +       unsigned int i;
420 +       links = kzalloc(max_links * sizeof(links[0]), GFP_KERNEL);
421 +       if (links == NULL)
422 +               return -ENOMEM;
424 +       entity->group_id = 0;
425 +       entity->max_links = max_links;
426 +       entity->num_links = 0;
427 +       entity->num_backlinks = 0;
428 +       entity->num_pads = num_pads;
429 +       entity->pads = pads;
430 +       entity->links = links;
432 +       for (i = 0; i < num_pads; i++) {
433 +               pads[i].entity = entity;
434 +               pads[i].index = i;
435 +       }
437 +       return 0;
438 +}
439 +EXPORT_SYMBOL_GPL(media_entity_init);
441 +void
442 +media_entity_cleanup(struct media_entity *entity)
443 +{
444 +       kfree(entity->links);
445 +}
446 +EXPORT_SYMBOL_GPL(media_entity_cleanup);
448 +static struct media_link *media_entity_add_link(struct media_entity *entity)
449 +{
450 +       if (entity->num_links >= entity->max_links) {
451 +               struct media_link *links = entity->links;
452 +               unsigned int max_links = entity->max_links + 2;
453 +               unsigned int i;
455 +               links = krealloc(links, max_links * sizeof(*links), GFP_KERNEL);
456 +               if (links == NULL)
457 +                       return NULL;
459 +               for (i = 0; i < entity->num_links; i++)
460 +                       links[i].reverse->reverse = &links[i];
462 +               entity->max_links = max_links;
463 +               entity->links = links;
464 +       }
466 +       return &entity->links[entity->num_links++];
467 +}
469 +int
470 +media_entity_create_link(struct media_entity *source, u16 source_pad,
471 +                        struct media_entity *sink, u16 sink_pad, u32 flags)
472 +{
473 +       struct media_link *link;
474 +       struct media_link *backlink;
476 +       BUG_ON(source == NULL || sink == NULL);
477 +       BUG_ON(source_pad >= source->num_pads);
478 +       BUG_ON(sink_pad >= sink->num_pads);
480 +       link = media_entity_add_link(source);
481 +       if (link == NULL)
482 +               return -ENOMEM;
484 +       link->source = &source->pads[source_pad];
485 +       link->sink = &sink->pads[sink_pad];
486 +       link->flags = flags;
488 +       /* Create the backlink. Backlinks are used to help graph traversal and
489 +        * are not reported to userspace.
490 +        */
491 +       backlink = media_entity_add_link(sink);
492 +       if (backlink == NULL) {
493 +               source->num_links--;
494 +               return -ENOMEM;
495 +       }
497 +       backlink->source = &source->pads[source_pad];
498 +       backlink->sink = &sink->pads[sink_pad];
499 +       backlink->flags = flags;
501 +       link->reverse = backlink;
502 +       backlink->reverse = link;
504 +       sink->num_backlinks++;
506 +       return 0;
507 +}
508 +EXPORT_SYMBOL_GPL(media_entity_create_link);
509 diff --git a/include/media/media-device.h b/include/media/media-device.h
510 index e11f01a..0b1ecf5 100644
511 --- a/include/media/media-device.h
512 +++ b/include/media/media-device.h
513 @@ -25,8 +25,10 @@
514  
515  #include <linux/device.h>
516  #include <linux/list.h>
517 +#include <linux/spinlock.h>
518  
519  #include <media/media-devnode.h>
520 +#include <media/media-entity.h>
521  
522  /**
523   * struct media_device - Media device
524 @@ -37,6 +39,9 @@
525   * @bus_info:  Unique and stable device location identifier
526   * @hw_revision: Hardware device revision
527   * @driver_version: Device driver version
528 + * @entity_id: ID of the next entity to be registered
529 + * @entities:  List of registered entities
530 + * @lock:      Entities list lock
531   *
532   * This structure represents an abstract high-level media device. It allows easy
533   * access to entities and provides basic media device-level support. The
534 @@ -58,6 +63,12 @@ struct media_device {
535         char bus_info[32];
536         u32 hw_revision;
537         u32 driver_version;
539 +       u32 entity_id;
540 +       struct list_head entities;
542 +       /* Protects the entities list */
543 +       spinlock_t lock;
544  };
545  
546  /* media_devnode to media_device */
547 @@ -66,4 +77,12 @@ struct media_device {
548  int __must_check media_device_register(struct media_device *mdev);
549  void media_device_unregister(struct media_device *mdev);
550  
551 +int __must_check media_device_register_entity(struct media_device *mdev,
552 +                                             struct media_entity *entity);
553 +void media_device_unregister_entity(struct media_entity *entity);
555 +/* Iterate over all entities. */
556 +#define media_device_for_each_entity(entity, mdev)                     \
557 +       list_for_each_entry(entity, &(mdev)->entities, list)
559  #endif
560 diff --git a/include/media/media-entity.h b/include/media/media-entity.h
561 new file mode 100644
562 index 0000000..7cf9135
563 --- /dev/null
564 +++ b/include/media/media-entity.h
565 @@ -0,0 +1,122 @@
566 +/*
567 + * Media entity
568 + *
569 + * Copyright (C) 2010 Nokia Corporation
570 + *
571 + * Contacts: Laurent Pinchart <laurent.pinchart@ideasonboard.com>
572 + *          Sakari Ailus <sakari.ailus@maxwell.research.nokia.com>
573 + *
574 + * This program is free software; you can redistribute it and/or modify
575 + * it under the terms of the GNU General Public License version 2 as
576 + * published by the Free Software Foundation.
577 + *
578 + * This program is distributed in the hope that it will be useful,
579 + * but WITHOUT ANY WARRANTY; without even the implied warranty of
580 + * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the
581 + * GNU General Public License for more details.
582 + *
583 + * You should have received a copy of the GNU General Public License
584 + * along with this program; if not, write to the Free Software
585 + * Foundation, Inc., 59 Temple Place, Suite 330, Boston, MA  02111-1307  USA
586 + */
588 +#ifndef _MEDIA_ENTITY_H
589 +#define _MEDIA_ENTITY_H
591 +#include <linux/list.h>
593 +#define MEDIA_ENT_TYPE_SHIFT           16
594 +#define MEDIA_ENT_TYPE_MASK            0x00ff0000
595 +#define MEDIA_ENT_SUBTYPE_MASK         0x0000ffff
597 +#define MEDIA_ENT_T_DEVNODE            (1 << MEDIA_ENTITY_TYPE_SHIFT)
598 +#define MEDIA_ENT_T_DEVNODE_V4L                (MEDIA_ENTITY_T_DEVNODE + 1)
599 +#define MEDIA_ENT_T_DEVNODE_FB         (MEDIA_ENTITY_T_DEVNODE + 2)
600 +#define MEDIA_ENT_T_DEVNODE_ALSA       (MEDIA_ENTITY_T_DEVNODE + 3)
601 +#define MEDIA_ENT_T_DEVNODE_DVB                (MEDIA_ENTITY_T_DEVNODE + 4)
603 +#define MEDIA_ENT_T_V4L2_SUBDEV                (2 << MEDIA_ENTITY_TYPE_SHIFT)
604 +#define MEDIA_ENT_T_V4L2_SUBDEV_SENSOR (MEDIA_ENTITY_T_V4L2_SUBDEV + 1)
605 +#define MEDIA_ENT_T_V4L2_SUBDEV_FLASH  (MEDIA_ENTITY_T_V4L2_SUBDEV + 2)
606 +#define MEDIA_ENT_T_V4L2_SUBDEV_LENS   (MEDIA_ENTITY_T_V4L2_SUBDEV + 3)
608 +#define MEDIA_ENT_FL_DEFAULT           (1 << 0)
610 +#define MEDIA_LNK_FL_ENABLED           (1 << 0)
611 +#define MEDIA_LNK_FL_IMMUTABLE         (1 << 1)
613 +#define MEDIA_PAD_FL_INPUT             (1 << 0)
614 +#define MEDIA_PAD_FL_OUTPUT            (1 << 1)
616 +struct media_link {
617 +       struct media_pad *source;       /* Source pad */
618 +       struct media_pad *sink;         /* Sink pad  */
619 +       struct media_link *reverse;     /* Link in the reverse direction */
620 +       unsigned long flags;            /* Link flags (MEDIA_LNK_FL_*) */
621 +};
623 +struct media_pad {
624 +       struct media_entity *entity;    /* Entity this pad belongs to */
625 +       u16 index;                      /* Pad index in the entity pads array */
626 +       unsigned long flags;            /* Pad flags (MEDIA_PAD_FL_*) */
627 +};
629 +struct media_entity {
630 +       struct list_head list;
631 +       struct media_device *parent;    /* Media device this entity belongs to*/
632 +       u32 id;                         /* Entity ID, unique in the parent media
633 +                                        * device context */
634 +       const char *name;               /* Entity name */
635 +       u32 type;                       /* Entity type (MEDIA_ENT_T_*) */
636 +       u32 revision;                   /* Entity revision, driver specific */
637 +       unsigned long flags;            /* Entity flags (MEDIA_ENT_FL_*) */
638 +       u32 group_id;                   /* Entity group ID */
640 +       u16 num_pads;                   /* Number of input and output pads */
641 +       u16 num_links;                  /* Number of existing links, both
642 +                                        * enabled and disabled */
643 +       u16 num_backlinks;              /* Number of backlinks */
644 +       u16 max_links;                  /* Maximum number of links */
646 +       struct media_pad *pads;         /* Pads array (num_pads elements) */
647 +       struct media_link *links;       /* Links array (max_links elements)*/
649 +       union {
650 +               /* Node specifications */
651 +               struct {
652 +                       u32 major;
653 +                       u32 minor;
654 +               } v4l;
655 +               struct {
656 +                       u32 major;
657 +                       u32 minor;
658 +               } fb;
659 +               struct {
660 +                       u32 card;
661 +                       u32 device;
662 +                       u32 subdevice;
663 +               } alsa;
664 +               int dvb;
666 +               /* Sub-device specifications */
667 +               /* Nothing needed yet */
668 +       };
669 +};
671 +static inline u32 media_entity_type(struct media_entity *entity)
672 +{
673 +       return entity->type & MEDIA_ENT_TYPE_MASK;
674 +}
676 +static inline u32 media_entity_subtype(struct media_entity *entity)
677 +{
678 +       return entity->type & MEDIA_ENT_SUBTYPE_MASK;
679 +}
681 +int media_entity_init(struct media_entity *entity, u16 num_pads,
682 +               struct media_pad *pads, u16 extra_links);
683 +void media_entity_cleanup(struct media_entity *entity);
684 +int media_entity_create_link(struct media_entity *source, u16 source_pad,
685 +               struct media_entity *sink, u16 sink_pad, u32 flags);
687 +#endif
688 -- 
689 1.6.6.1