1 # This .inc file allows you to build and deploy multiple sets of kernel + modules with different defconfigs
2 #
3 # Note that this include will NOT stage anything nor create packages, since that is virtually impossible
4 # Userspace should be built against the 'regular' kernel
5 #
6 # The intended usecase is for machines that have mutually exclusive drivers due to e.g. pinmuxing issues.
7 # For example the LogicPD omap-l138 experimenter board can have multiple mutually exclusive expansion boards
8 # like lcd, ethernet, sound, 20x2 character LCD, etc. To be able to easily test all of those you can use this .inc
9 #
10 # To make it easier finding the original defconfig from a running kernel, this also forcefully turns on
11 # CONFIG_IKCONFIG_PROC so people can do 'zcat /proc/config.gz' on the target.
13 require linux.inc
15 SRC_URI_append = " \
16 file://configs/ "
18 MULTI_CONFIG_BASE_SUFFIX = "multi-config-"
20 # bitbake.conf only prepends PARALLEL make in tasks called do_compile, which isn't the case for multiconfig
21 # So explicitly enable it for compileconfigs in here
22 EXTRA_OEMAKE = "${PARALLEL_MAKE} "
24 do_compileconfigs () {
26 # Compile and Install additional kernel configs if found
27 if [ -e ${WORKDIR}/configs/.empty ] ; then
28 echo "No configs found in configs/ directory, skipping to regular build"
29 else
30 echo "Multiple configs found, building those first"
32 # Context Save the regular 'defconfig'
33 cp ${WORKDIR}/defconfig ${WORKDIR}/defconfig.save
35 for config in ${WORKDIR}/configs/* ; do
37 # Copy in alternative config
38 cd ${S}
39 cp $config ${WORKDIR}/defconfig
41 # Enable config to be viewed on the target
42 echo "CONFIG_IKCONFIG=y" >> ${WORKDIR}/defconfig
43 echo "CONFIG_IKCONFIG_PROC=y" >> ${WORKDIR}/defconfig
45 # Build and Install this alternative kernel
46 do_configure
47 kernel_do_compile
48 do_compile_kernelmodules
49 kernel_do_install
51 # Drop the resulting images in the deploy dir
52 install -d ${DEPLOY_DIR_IMAGE}
53 install -m 0644 ${KERNEL_OUTPUT} ${DEPLOY_DIR_IMAGE}/${KERNEL_IMAGE_BASE_NAME}.${MULTI_CONFIG_BASE_SUFFIX}$(basename $config).bin
55 if [ -d "${D}/lib" ]; then
56 fakeroot tar -cvzf ${DEPLOY_DIR_IMAGE}/${MODULES_IMAGE_BASE_NAME}.${MULTI_CONFIG_BASE_SUFFIX}$(basename $config).tgz -C ${D} lib
57 fi
59 # Install the final config alongside the images
60 cp .config ${DEPLOY_DIR_IMAGE}/config-${PV}-${PR}-${MACHINE}.${MULTI_CONFIG_BASE_SUFFIX}$(basename $config).config
62 # Create symlinks
63 cd ${DEPLOY_DIR_IMAGE}
64 rm -f ${KERNEL_IMAGE_SYMLINK_NAME}.${MULTI_CONFIG_BASE_SUFFIX}$(basename $config).bin
65 ln -sf ${KERNEL_IMAGE_BASE_NAME}.${MULTI_CONFIG_BASE_SUFFIX}$(basename $config).bin ${KERNEL_IMAGE_SYMLINK_NAME}.${MULTI_CONFIG_BASE_SUFFIX}$(basename $config).bin
66 rm -f modules-${MACHINE}.${MULTI_CONFIG_BASE_SUFFIX}$(basename $config).tgz
67 ln -sf ${MODULES_IMAGE_BASE_NAME}.${MULTI_CONFIG_BASE_SUFFIX}$(basename $config).tgz modules-${MACHINE}.${MULTI_CONFIG_BASE_SUFFIX}$(basename $config).tgz
68 rm -f config-${MACHINE}.${MULTI_CONFIG_BASE_SUFFIX}$(basename $config).config
69 ln -sf config-${PV}-${PR}-${MACHINE}.${MULTI_CONFIG_BASE_SUFFIX}$(basename $config).config config-${MACHINE}.${MULTI_CONFIG_BASE_SUFFIX}$(basename $config).config
71 done
73 # Restore the regular 'defconfig'
74 cp ${WORKDIR}/defconfig.save ${WORKDIR}/defconfig
75 fi
76 }
78 # For reference, copy .config to deploy image
79 do_deploy_append () {
81 # Drop the regular defconfig along side the others for consistency
82 cd ${S}
83 cp .config ${DEPLOY_DIR_IMAGE}/config-${PV}-${PR}-${MACHINE}.config
85 # add symlink
86 cd ${DEPLOY_DIR_IMAGE}
87 rm -f config-${MACHINE}.config
88 ln -s config-${PV}-${PR}-${MACHINE}.config config-${MACHINE}.config
90 rm -f modules-${MACHINE}.tgz
91 ln -sf ${MODULES_IMAGE_BASE_NAME}.tgz modules-${MACHINE}.tgz
93 }
95 do_compileconfigs[depends] += "u-boot-mkimage-native:do_populate_sysroot virtual/${TARGET_PREFIX}gcc:do_populate_sysroot virtual/${TARGET_PREFIX}gcc${KERNEL_CCSUFFIX}:do_populate_sysroot"
96 addtask compileconfigs after do_patch before do_configure