[glsdk/meta-ti-glsdk.git] / recipes-bsp / u-boot / u-boot-am180x-2010.12 / am180x-evm / 0001-da850evm-change-default-memory-to-not-limit-at-32MB.patch
1 From df5c87c4e1be1670475eba1187301a2f7a7aca30 Mon Sep 17 00:00:00 2001
2 From: Chase Maupin <Chase.Maupin@ti.com>
3 Date: Wed, 22 Jun 2011 12:12:09 -0500
4 Subject: [PATCH] da850evm: change default memory to not limit at 32MB
6 * Change the default mem= option passed to the Linux kernel to
7 not limit the memory to 32MB.
8 * This change is used by AM devices that do not need to reserve
9 space for the DSP image. By removing the mem= option we get
10 access to all of the memory on the system.
11 * Limiting the memory to 32MB causes out-of-memory errors
12 when running large applications such as web browsers
14 Signed-off-by: Chase Maupin <Chase.Maupin@ti.com>
15 ---
16 include/configs/da850evm.h | 2 +-
17 1 files changed, 1 insertions(+), 1 deletions(-)
19 diff --git a/include/configs/da850evm.h b/include/configs/da850evm.h
20 index 4a1e0af..55badc9 100755
21 --- a/include/configs/da850evm.h
22 +++ b/include/configs/da850evm.h
23 @@ -184,7 +184,7 @@
24 #define CONFIG_CMDLINE_TAG
25 #define CONFIG_REVISION_TAG
26 #define CONFIG_SETUP_MEMORY_TAGS
27 -#define CONFIG_BOOTARGS "mem=32M console=ttyS2,115200n8 root=/dev/mmcblk0p2 rw rootwait ip=off"
28 +#define CONFIG_BOOTARGS "console=ttyS2,115200n8 root=/dev/mmcblk0p2 rw rootwait ip=off"
29 #define CONFIG_BOOTCOMMAND "if mmc rescan 0; then if fatload mmc 0 0xc0600000 boot.scr; then source 0xc0600000; else fatload mmc 0 0xc0700000 uImage; bootm c0700000; fi; else sf probe 0; sf read 0xc0700000 0x80000 0x220000; bootm 0xc0700000; fi"
30 #define CONFIG_BOOTDELAY 3
32 --
33 1.7.0.4