u-boot: Add am3517 u-boot recipe
[glsdk/meta-ti-glsdk.git] / recipes-bsp / u-boot / u-boot-am3517_2011.09.bb
1 require u-boot-ti.inc
3 DESCRIPTION = "u-boot bootloader for ARM MPU devices"
5 COMPATIBLE_MACHINE = "omap3"
7 DEFAULT_PREFERENCE = "-1"
9 PR = "r0+gitr${SRCPV}"
11 SRC_URI = "git://arago-project.org/git/projects/u-boot-am33x.git;protocol=git;branch=${BRANCH}"
13 BRANCH = "AM335XPSP_04.06.00.08"
15 # Lock to the commit corresponding to tag "v2011.09_AM335xPSP_04.06.00.08"
16 SRCREV = "1e4626f0d5f3bb04ec974e76a5d9029875269d31"
18 # Set the name of the SPL that will built so that it is also packaged with u-boot.
19 SPL_BINARY = "MLO"