]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/meta-ti-glsdk.git/blob - recipes-bsp/u-boot/u-boot-am37x-2012.04.01/0001-omap3_beagle-add-usbethaddr-setting-to-enable-networ.patch
u-boot 2011.12: modify multi-machine version for the new .inc file
[glsdk/meta-ti-glsdk.git] / recipes-bsp / u-boot / u-boot-am37x-2012.04.01 / 0001-omap3_beagle-add-usbethaddr-setting-to-enable-networ.patch
1 From c56786770eb0ccb95204cb72b961c44c65ff343b Mon Sep 17 00:00:00 2001
2 From: Chase Maupin <Chase.Maupin@ti.com>
3 Date: Thu, 17 May 2012 09:51:50 -0500
4 Subject: [PATCH] omap3_beagle: add usbethaddr setting to enable networking
6 * In order for the SMSC USB ethernet device to work the
7   usbethaddr setting must be set when the "usb start" command
8   is executed and the network device is discovered.
9 * Currently set this for de:ad:be:ef until we can start
10   generating random or semi-random MAC addresses.
11 * Based on work by Steve Kipisz and Joel Fernandez
13 Upstream-Status: Not Upstreamable
14     * We cannot upstream this hard coded MAC address setting.
15     * User's should look at the following web page for information on
16       how to generate a MAC address, but this patch enables the out
17       of box experience for the SDK.
18         http://www.denx.de/wiki/view/DULG/WhereCanIGetAValidMACAddress
21 Signed-off-by: Chase Maupin <Chase.Maupin@ti.com>
22 ---
23  include/configs/omap3_beagle.h |    1 +
24  1 files changed, 1 insertions(+), 0 deletions(-)
26 diff --git a/include/configs/omap3_beagle.h b/include/configs/omap3_beagle.h
27 index ddeb414..58a29b8 100644
28 --- a/include/configs/omap3_beagle.h
29 +++ b/include/configs/omap3_beagle.h
30 @@ -219,6 +219,7 @@
31         "loadaddr=0x80200000\0" \
32         "rdaddr=0x81000000\0" \
33         "usbtty=cdc_acm\0" \
34 +       "usbethaddr=de:ad:be:ef\0" \
35         "bootfile=uImage.beagle\0" \
36         "console=ttyO2,115200n8\0" \
37         "mpurate=auto\0" \
38 -- 
39 1.7.0.4