]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/meta-ti-glsdk.git/blob - recipes-bsp/u-boot/u-boot-am37x-2012.04.01/0002-omap3evm-Make-the-board-start-at-800MHz.patch
u-boot-am37x: modify am37x specific version to use new namespace feature
[glsdk/meta-ti-glsdk.git] / recipes-bsp / u-boot / u-boot-am37x-2012.04.01 / 0002-omap3evm-Make-the-board-start-at-800MHz.patch
1 From a0f4f7b85d004db36a24cc05e9c34f137186270b Mon Sep 17 00:00:00 2001
2 From: Chase Maupin <Chase.Maupin@ti.com>
3 Date: Wed, 23 May 2012 09:25:06 -0500
4 Subject: [PATCH 2/3] omap3evm: Make the board start at 800MHz
6 * It is safe to start the the 3630 silicon at 800MHz for all
7   revisions.  Go ahead and bump the speed to 800MHz during boot
8   instead of using the default 500MHz speed.
9 * This patch was based on work by Tom Rini <trini@ti.com> at
10   http://arago-project.org/git/projects/?p=u-boot-am33x.git;a=commit;h=ad130035df754931f2939902e453cc3736412f5f
12 Upstream-Status: Pending
13     * Will be submitted upstream since it is safe for all silicon
14       revisions to boot at 800MHz according to HW team.
16 Signed-off-by: Chase Maupin <Chase.Maupin@ti.com>
17 ---
18  board/ti/evm/evm.c |    2 +-
19  1 files changed, 1 insertions(+), 1 deletions(-)
21 diff --git a/board/ti/evm/evm.c b/board/ti/evm/evm.c
22 index 91eb93d..0d0b4a2 100644
23 --- a/board/ti/evm/evm.c
24 +++ b/board/ti/evm/evm.c
25 @@ -180,7 +180,7 @@ int misc_init_r(void)
26  
27          if (get_cpu_family() == CPU_OMAP36XX) {
28                 twl4030_power_mpu_init();
29 -               set_mpu_clk(500);
30 +               set_mpu_clk(800);
31         }
32         return 0;
33  }
34 -- 
35 1.7.0.4