[glsdk/meta-ti-glsdk.git] / recipes-kernel / linux / linux-3.0 / pm-wip / voltdm / 0080-OMAP-hwmod-Wait-the-idle-status-to-be-disabled.patch
1 From c847909c6cdb2b6fcb1f7679a8881ef489f63d7b Mon Sep 17 00:00:00 2001
2 From: Benoit Cousson <b-cousson@ti.com>
3 Date: Sun, 10 Jul 2011 05:56:30 -0600
4 Subject: [PATCH 080/149] OMAP: hwmod: Wait the idle status to be disabled
6 It is mandatory to wait for a module to be in disabled state before
7 potentially disabling source clock or re-asserting a reset.
9 omap_hwmod_idle and omap_hwmod_shutdown does not wait for
10 the module to be fully idle.
12 Add a cm_xxx accessor to wait the clkctrl idle status to be disabled.
13 Fix hwmod_[idle|shutdown] to use this API.
15 Based on Rajendra's initial patch.
17 Please note that most interconnects hwmod will return one timeout because
18 it is impossible for them to be in idle since the processor is accessing
19 the registers though the interconnect.
21 Signed-off-by: Benoit Cousson <b-cousson@ti.com>
22 Signed-off-by: Rajendra Nayak <rnayak@ti.com>
23 Cc: Paul Walmsley <paul@pwsan.com>
24 Cc: Todd Poynor <toddpoynor@google.com>
25 [paul@pwsan.com: move cpu_is_*() tests to the top of _wait_target_disable();
26 incorporate some feedback from Todd]
27 Signed-off-by: Paul Walmsley <paul@pwsan.com>
28 ---
29 arch/arm/mach-omap2/cminst44xx.c | 25 +++++++++++++++++++++++
30 arch/arm/mach-omap2/cminst44xx.h | 1 +
31 arch/arm/mach-omap2/omap_hwmod.c | 40 ++++++++++++++++++++++++++++++++++++++
32 3 files changed, 66 insertions(+), 0 deletions(-)
34 diff --git a/arch/arm/mach-omap2/cminst44xx.c b/arch/arm/mach-omap2/cminst44xx.c
35 index 9033dd4..0fe3f14 100644
36 --- a/arch/arm/mach-omap2/cminst44xx.c
37 +++ b/arch/arm/mach-omap2/cminst44xx.c
38 @@ -284,3 +284,28 @@ int omap4_cminst_wait_module_ready(u8 part, u16 inst, s16 cdoffs,
39 return (i < MAX_MODULE_READY_TIME) ? 0 : -EBUSY;
40 }
42 +/**
43 + * omap4_cminst_wait_module_idle - wait for a module to be in 'disabled'
44 + * state
45 + * @part: PRCM partition ID that the CM_CLKCTRL register exists in
46 + * @inst: CM instance register offset (*_INST macro)
47 + * @cdoffs: Clockdomain register offset (*_CDOFFS macro)
48 + * @clkctrl_offs: Module clock control register offset (*_CLKCTRL macro)
49 + *
50 + * Wait for the module IDLEST to be disabled. Some PRCM transition,
51 + * like reset assertion or parent clock de-activation must wait the
52 + * module to be fully disabled.
53 + */
54 +int omap4_cminst_wait_module_idle(u8 part, u16 inst, s16 cdoffs, u16 clkctrl_offs)
55 +{
56 + int i = 0;
57 +
58 + if (!clkctrl_offs)
59 + return 0;
60 +
61 + omap_test_timeout((_clkctrl_idlest(part, inst, cdoffs, clkctrl_offs) ==
62 + CLKCTRL_IDLEST_DISABLED),
63 + MAX_MODULE_READY_TIME, i);
64 +
65 + return (i < MAX_MODULE_READY_TIME) ? 0 : -EBUSY;
66 +}
67 diff --git a/arch/arm/mach-omap2/cminst44xx.h b/arch/arm/mach-omap2/cminst44xx.h
68 index 8eba2ae..a985400 100644
69 --- a/arch/arm/mach-omap2/cminst44xx.h
70 +++ b/arch/arm/mach-omap2/cminst44xx.h
71 @@ -18,6 +18,7 @@ extern void omap4_cminst_clkdm_force_sleep(u8 part, s16 inst, u16 cdoffs);
72 extern void omap4_cminst_clkdm_force_wakeup(u8 part, s16 inst, u16 cdoffs);
74 extern int omap4_cminst_wait_module_ready(u8 part, u16 inst, s16 cdoffs, u16 clkctrl_offs);
75 +extern int omap4_cminst_wait_module_idle(u8 part, u16 inst, s16 cdoffs, u16 clkctrl_offs);
77 /*
78 * In an ideal world, we would not export these low-level functions,
79 diff --git a/arch/arm/mach-omap2/omap_hwmod.c b/arch/arm/mach-omap2/omap_hwmod.c
80 index 00241ea..d21f49b 100644
81 --- a/arch/arm/mach-omap2/omap_hwmod.c
82 +++ b/arch/arm/mach-omap2/omap_hwmod.c
83 @@ -1102,6 +1102,36 @@ static int _wait_target_ready(struct omap_hwmod *oh)
84 }
86 /**
87 + * _wait_target_disable - wait for a module to be disabled
88 + * @oh: struct omap_hwmod *
89 + *
90 + * Wait for a module @oh to enter slave idle. Returns 0 if the module
91 + * does not have an IDLEST bit or if the module successfully enters
92 + * slave idle; otherwise, pass along the return value of the
93 + * appropriate *_cm*_wait_module_idle() function.
94 + */
95 +static int _wait_target_disable(struct omap_hwmod *oh)
96 +{
97 + /* TODO: For now just handle OMAP4+ */
98 + if (cpu_is_omap24xx() || cpu_is_omap34xx())
99 + return 0;
100 +
101 + if (!oh)
102 + return -EINVAL;
103 +
104 + if (oh->_int_flags & _HWMOD_NO_MPU_PORT)
105 + return 0;
106 +
107 + if (oh->flags & HWMOD_NO_IDLEST)
108 + return 0;
109 +
110 + return omap4_cminst_wait_module_idle(oh->clkdm->prcm_partition,
111 + oh->clkdm->cm_inst,
112 + oh->clkdm->clkdm_offs,
113 + oh->prcm.omap4.clkctrl_offs);
114 +}
115 +
116 +/**
117 * _lookup_hardreset - fill register bit info for this hwmod/reset line
118 * @oh: struct omap_hwmod *
119 * @name: name of the reset line in the context of this hwmod
120 @@ -1410,6 +1440,8 @@ static int _enable(struct omap_hwmod *oh)
121 */
122 static int _idle(struct omap_hwmod *oh)
123 {
124 + int ret;
125 +
126 pr_debug("omap_hwmod: %s: idling\n", oh->name);
128 if (oh->_state != _HWMOD_STATE_ENABLED) {
129 @@ -1422,6 +1454,10 @@ static int _idle(struct omap_hwmod *oh)
130 _idle_sysc(oh);
131 _del_initiator_dep(oh, mpu_oh);
132 _disable_clocks(oh);
133 + ret = _wait_target_disable(oh);
134 + if (ret)
135 + pr_warn("omap_hwmod: %s: _wait_target_disable failed\n",
136 + oh->name);
138 /* Mux pins for device idle if populated */
139 if (oh->mux && oh->mux->pads_dynamic)
140 @@ -1514,6 +1550,10 @@ static int _shutdown(struct omap_hwmod *oh)
141 _del_initiator_dep(oh, mpu_oh);
142 /* XXX what about the other system initiators here? dma, dsp */
143 _disable_clocks(oh);
144 + ret = _wait_target_disable(oh);
145 + if (ret)
146 + pr_warn("omap_hwmod: %s: _wait_target_disable failed\n",
147 + oh->name);
148 }
149 /* XXX Should this code also force-disable the optional clocks? */
151 --
152 1.6.6.1