[glsdk/meta-ti-glsdk.git] / recipes-kernel / linux / linux-omap-2.6.39 / pm / linux-omap-2.6.39-ti-pm-wip-cpufreq / 0046-OMAP3-PM-CPUFreq-driver-for-OMAP3.patch
1 From a5072bdf333b8fb1080aac5d2b986553ea8de0f9 Mon Sep 17 00:00:00 2001
2 From: Rajendra Nayak <rnayak@ti.com>
3 Date: Mon, 10 Nov 2008 17:00:25 +0530
4 Subject: [PATCH 46/59] OMAP3 PM: CPUFreq driver for OMAP3
6 CPUFreq driver for OMAP3
8 With additional fixes and cleanups from Tero Kristo:
9 - Fix rate calculation bug in omap3_select_table_rate
10 - Refreshed DVFS VDD1 control against latest clock fw
12 Signed-off-by: Tero Kristo <tero.kristo@nokia.com>
13 Signed-off-by: Rajendra Nayak <rnayak@ti.com>
15 OMAP3: PM: CPUFreq: Fix omap_getspeed.
17 Signed-off-by: Peter 'p2' De Schrijver <peter.de-schrijver@nokia.com>
19 Make sure omap cpufreq driver initializes after cpufreq framework and governors
21 Signed-off-by: Peter 'p2' De Schrijver <peter.de-schrijver@nokia.com>
23 merge: CPUFreq: remove obsolete funcs
25 OMAP3 clock: Update cpufreq driver
27 This patch removes all refrences to virtual clock
28 nodes in CPUFreq driver.
30 Signed-off-by: Rajendra Nayak <rnayak@ti.com>
31 Signed-off-by: Tero Kristo <tero.kristo@nokia.com>
32 Signed-off-by: Jean Pihet <jpihet@mvista.com>
34 PM: Prevent direct cpufreq scaling during initialization
36 It is seen that the OMAP specific cpufreq initialization code tries to
37 scale the MPU frequency to the highest possible without taking care of
38 the voltage level. On power on reset the power IC does not provide the
39 necessary voltage for the highest available MPU frequency (that would
40 satisfy all Si families). This potentially is an window of opportunity
41 for things to go wrong.
43 Signed-off-by: Romit Dasgupta <romit@ti.com>
44 Signed-off-by: Kevin Hilman <khilman@deeprootsystems.com>
46 OMAP3: PM: enable 600MHz (overdrive) OPP
48 Signed-off-by: Kevin Hilman <khilman@deeprootsystems.com>
50 omap3: introduce cpufreq
52 OMAP OPP layer functions now have dependencies of CONFIG_CPU_FREQ only.
54 With this patch, omap opp layer now has its compilation flags
55 bound to CONFIG_CPU_FREQ. Also its code has been removed from pm34xx.c.
57 A new file has been created to contain cpu freq code related to
58 OMAP3: cpufreq34xx.c
60 OMAP34xx and OMAP36xx family OPPs are made available
62 Signed-off-by: Eduardo Valentin <eduardo.valentin@nokia.com>
63 Signed-off-by: Paul Walmsley <paul@pwsan.com>
64 Signed-off-by: Nishanth Menon <nm@ti.com>
65 Signed-off-by: Vishwanath BS <vishwanath.bs@ti.com>
66 Signed-off-by: Kevin Hilman <khilman@deeprootsystems.com>
67 Signed-off-by: Romit Dasgupta <romit@ti.com>
68 Signed-off-by: Rajendra Nayak <rnayak@ti.com>
70 omap3: cpufreq: allow default opp table init
72 For board files which choose to override the defaults, the existing
73 mechanism will work, for boards that would like to work with defaults,
74 allow init_common_hw to call init_opp_table to initialize if not
75 already initialized. this will allow all omap boards which have opp
76 tables predefined for a silicon to use the same.
78 Originally reported for overo:
79 http://marc.info/?t=127265269400004&r=1&w=2
81 Signed-off-by: Nishanth Menon <nm@ti.com>
82 Reported-by: Peter Tseng <tsenpet09@gmail.com>
83 Cc: Cliff Brake <cliff.brake@gmail.com>
84 Cc: Kevin Hilman <khilman@deeprootsystems.com>
86 OMAP2: update OPP data to be device based
88 Cc: Nishanth Menon <nm@ti.com>
89 Signed-off-by: Kevin Hilman <khilman@deeprootsystems.com>
91 OMAP3: CPUfreq: update to device-based OPP API
93 Update usage of OPP API to use new device-based API. This requires
94 getting the 'struct device' for the MPU and using that with the OPP
95 API.
97 Signed-off-by: Kevin Hilman <khilman@deeprootsystems.com>
99 omap3: opp: make independent of cpufreq
101 Make opp3xx data which is registered with the opp layer
102 dependent purely on CONFIG_PM as opp layer and pm.c users
103 are CONFIG_PM dependent not cpufreq dependent.
104 so we rename the data definition to opp3xxx_data.c (inline with what
105 we have for omap2), also move the build definition to be under
106 the existing CONFIG_PM build instead of CPUFREQ.
108 Cc: Eduardo Valentin <eduardo.valentin@nokia.com>
109 Cc: Kevin Hilman <khilman@deeprootsystems.com>
110 Cc: Paul Walmsley <paul@pwsan.com>
111 Cc: Rajendra Nayak <rnayak@ti.com>
112 Cc: Sanjeev Premi <premi@ti.com>
113 Cc: Thara Gopinath <thara@ti.com>
114 Cc: Tony Lindgren <tony@atomide.com>
116 Signed-off-by: Nishanth Menon <nm@ti.com>
117 ---
118 arch/arm/mach-omap2/clock.h | 14 +++++++++++++-
119 arch/arm/mach-omap2/clock34xx.c | 2 ++
120 arch/arm/plat-omap/cpu-omap.c | 34 +++++++++++++++++++++++++++++++---
121 3 files changed, 46 insertions(+), 4 deletions(-)
123 diff --git a/arch/arm/mach-omap2/clock.h b/arch/arm/mach-omap2/clock.h
124 index e10ff2b..0a07e50 100644
125 --- a/arch/arm/mach-omap2/clock.h
126 +++ b/arch/arm/mach-omap2/clock.h
127 @@ -141,7 +141,9 @@ extern const struct clksel_rate gpt_sys_rates[];
128 extern const struct clksel_rate gfx_l3_rates[];
129 extern const struct clksel_rate dsp_ick_rates[];
131 -#if defined(CONFIG_ARCH_OMAP2) && defined(CONFIG_CPU_FREQ)
132 +#ifdef CONFIG_CPU_FREQ
133 +
134 +#ifdef CONFIG_ARCH_OMAP2
135 extern void omap2_clk_init_cpufreq_table(struct cpufreq_frequency_table **table);
136 extern void omap2_clk_exit_cpufreq_table(struct cpufreq_frequency_table **table);
137 #else
138 @@ -149,6 +151,16 @@ extern void omap2_clk_exit_cpufreq_table(struct cpufreq_frequency_table **table)
139 #define omap2_clk_exit_cpufreq_table 0
140 #endif
142 +#ifdef CONFIG_ARCH_OMAP3
143 +extern void omap3_clk_init_cpufreq_table(struct cpufreq_frequency_table **table);
144 +extern void omap3_clk_exit_cpufreq_table(struct cpufreq_frequency_table **table);
145 +#else
146 +#define omap3_clk_init_cpufreq_table 0
147 +#define omap3_clk_exit_cpufreq_table 0
148 +#endif
149 +
150 +#endif /* CONFIG_CPU_FREQ */
151 +
152 extern const struct clkops clkops_omap2_iclk_dflt_wait;
153 extern const struct clkops clkops_omap2_iclk_dflt;
154 extern const struct clkops clkops_omap2_iclk_idle_only;
155 diff --git a/arch/arm/mach-omap2/clock34xx.c b/arch/arm/mach-omap2/clock34xx.c
156 index 1fc96b9..119e135 100644
157 --- a/arch/arm/mach-omap2/clock34xx.c
158 +++ b/arch/arm/mach-omap2/clock34xx.c
159 @@ -20,6 +20,8 @@
160 #include <linux/kernel.h>
161 #include <linux/clk.h>
162 #include <linux/io.h>
163 +#include <linux/err.h>
164 +#include <linux/cpufreq.h>
166 #include <plat/clock.h>
168 diff --git a/arch/arm/plat-omap/cpu-omap.c b/arch/arm/plat-omap/cpu-omap.c
169 index 1b36664..f0f9430 100644
170 --- a/arch/arm/plat-omap/cpu-omap.c
171 +++ b/arch/arm/plat-omap/cpu-omap.c
172 @@ -8,6 +8,10 @@
173 *
174 * Based on cpu-sa1110.c, Copyright (C) 2001 Russell King
175 *
176 + * Copyright (C) 2007-2008 Texas Instruments, Inc.
177 + * Updated to support OMAP3
178 + * Rajendra Nayak <rnayak@ti.com>
179 + *
180 * This program is free software; you can redistribute it and/or modify
181 * it under the terms of the GNU General Public License version 2 as
182 * published by the Free Software Foundation.
183 @@ -26,12 +30,19 @@
184 #include <plat/clock.h>
185 #include <asm/system.h>
187 +#if defined(CONFIG_ARCH_OMAP3) && !defined(CONFIG_OMAP_PM_NONE)
188 +#include <plat/omap-pm.h>
189 +#include <plat/opp.h>
190 +#endif
191 +
192 #define VERY_HI_RATE 900000000
194 static struct cpufreq_frequency_table *freq_table;
196 #ifdef CONFIG_ARCH_OMAP1
197 #define MPU_CLK "mpu"
198 +#elif CONFIG_ARCH_OMAP3
199 +#define MPU_CLK "arm_fck"
200 #else
201 #define MPU_CLK "virt_prcm_set"
202 #endif
203 @@ -73,7 +84,13 @@ static int omap_target(struct cpufreq_policy *policy,
204 unsigned int target_freq,
205 unsigned int relation)
206 {
207 +#ifdef CONFIG_ARCH_OMAP1
208 struct cpufreq_freqs freqs;
209 +#endif
210 +#if defined(CONFIG_ARCH_OMAP3) && !defined(CONFIG_OMAP_PM_NONE)
211 + unsigned long freq;
212 + struct device *mpu_dev = omap2_get_mpuss_device();
213 +#endif
214 int ret = 0;
216 /* Ensure desired rate is within allowed range. Some govenors
217 @@ -83,13 +100,13 @@ static int omap_target(struct cpufreq_policy *policy,
218 if (target_freq > policy->max)
219 target_freq = policy->max;
221 +#ifdef CONFIG_ARCH_OMAP1
222 freqs.old = omap_getspeed(0);
223 freqs.new = clk_round_rate(mpu_clk, target_freq * 1000) / 1000;
224 freqs.cpu = 0;
226 if (freqs.old == freqs.new)
227 return ret;
228 -
229 cpufreq_notify_transition(&freqs, CPUFREQ_PRECHANGE);
230 #ifdef CONFIG_CPU_FREQ_DEBUG
231 printk(KERN_DEBUG "cpufreq-omap: transition: %u --> %u\n",
232 @@ -97,7 +114,11 @@ static int omap_target(struct cpufreq_policy *policy,
233 #endif
234 ret = clk_set_rate(mpu_clk, freqs.new * 1000);
235 cpufreq_notify_transition(&freqs, CPUFREQ_POSTCHANGE);
236 -
237 +#elif defined(CONFIG_ARCH_OMAP3) && !defined(CONFIG_OMAP_PM_NONE)
238 + freq = target_freq * 1000;
239 + if (opp_find_freq_ceil(mpu_dev, &freq))
240 + omap_pm_cpu_set_freq(freq);
241 +#endif
242 return ret;
243 }
245 @@ -114,7 +135,14 @@ static int __cpuinit omap_cpu_init(struct cpufreq_policy *policy)
247 policy->cur = policy->min = policy->max = omap_getspeed(0);
249 - clk_init_cpufreq_table(&freq_table);
250 + if (!cpu_is_omap34xx()) {
251 + clk_init_cpufreq_table(&freq_table);
252 + } else {
253 + struct device *mpu_dev = omap2_get_mpuss_device();
254 +
255 + opp_init_cpufreq_table(mpu_dev, &freq_table);
256 + }
257 +
258 if (freq_table) {
259 result = cpufreq_frequency_table_cpuinfo(policy, freq_table);
260 if (!result)
261 --
262 1.6.6.1