1 SECTION = "kernel"
2 DESCRIPTION = "Linux kernel for TI devices"
3 LICENSE = "GPLv2"
4 LIC_FILES_CHKSUM = "file://COPYING;md5=d7810fab7487fb0aad327b76f1be7cd7"
5 KERNEL_IMAGETYPE = "uImage"
7 inherit kernel
9 # This function must be here BEFORE the require of linux-dtb.inc below.
10 # There is a "bug" in the base kernel.bbclass that after it's do_deploy
11 # step it does not return back to the ${S} directory but stays in the
12 # DEPLOY_DIR. However, the do_deploy_append defined in linux-dtb.inc
13 # assumes that it is being run in the ${S} directory. A patch is
14 # being submitted to fix this issue by either changing the do_deploy
15 # in the kernel.bbclass to do "cd -" as the last step or to add
16 # "cd ${S}" as the first line of do_deploy in linux-dtb.inc and this
17 # function can be removed once that change is available.
18 # If the function is not placed BEFORE the require then the change
19 # directory is not appended before the linux-dtb.inc changes.
20 do_deploy_append() {
21 cd ${S}
22 }
24 require recipes-kernel/linux/linux-dtb.inc
25 require recipes-kernel/linux/setup-defconfig.inc
27 # Stage the power management firmware before building the kernel
28 # for ti33x SOC_FAMILY devices
29 DEPENDS_ti33x += "am33x-cm3"
31 # Default is to package all dts files for ti33x devices unless building
32 # for the specific beaglebone machine.
33 KERNEL_DEVICETREE_ti33x = "arch/arm/boot/dts/am335x-evm.dts arch/arm/boot/dts/am335x-evmsk.dts arch/arm/boot/dts/am335x-bone.dts"
34 KERNEL_DEVICETREE_beaglebone = "arch/arm/boot/dts/am335x-bone.dts"
35 KERNEL_DEVICETREE_omap5-evm = "arch/arm/boot/dts/omap5-sevm.dts arch/arm/boot/dts/omap5-uevm.dts"
37 COMPATIBLE_MACHINE = "ti33x|omap-a15"
39 S = "${WORKDIR}/git"
41 BRANCH = "ti-linux-3.8.y"
43 SRCREV = "881dfafeae47da3a8f5ff8c791753e4b4df8065b"
44 PV = "3.8.5"
46 # Append to the MACHINE_KERNEL_PR so that a new SRCREV will cause a rebuild
47 MACHINE_KERNEL_PR_append = "d+gitr${SRCPV}"
49 SRC_URI = "git://git.ti.com/ti-linux-kernel/ti-linux-kernel.git;protocol=git;branch=${BRANCH} \
50 file://defconfig \
51 "
53 # Copy the am33x-cm3 firmware if it is available for ti33x SOC_FAMILY devices
54 do_compile_prepend_ti33x() {
55 if [ -e "${STAGING_DIR_HOST}/${base_libdir}/firmware/am335x-pm-firmware.bin" ]
56 then
57 cp "${STAGING_DIR_HOST}/${base_libdir}/firmware/am335x-pm-firmware.bin" "${S}/firmware"
58 fi
59 }