[glsdk/meta-ti-glsdk.git] / recipes-kernel / linux / linux-ti33x-psp-3.1 / can / 0001-can-d_can-Added-support-for-Bosch-D_CAN-controller.patch
1 From 7fedac525f38a0b47d27d959d1325945d188d787 Mon Sep 17 00:00:00 2001
2 From: Anil Kumar Ch <anilkumar@ti.com>
3 Date: Sun, 6 Nov 2011 13:56:35 +0530
4 Subject: [PATCH 1/7] can: d_can: Added support for Bosch D_CAN controller
6 Bosch D_CAN controller is a full-CAN implementation which is compliant
7 to CAN protocol version 2.0 part A and B. Bosch D_CAN user manual can be
8 obtained from:
10 http://www.semiconductors.bosch.de/media/en/pdf/ipmodules_1/can/d_can_users_manual_111.pdf
12 This patch adds the support for this controller.
13 The following are the design choices made while writing the controller
14 driver:
15 1. Interface Register set IF1 has be used for transmit and IF2 is used for
16 receive message objects.
17 2. Out of the total Message objects available, half of it are kept aside for RX
18 purposes and the rest for TX purposes.
19 3. NAPI implementation is such that both the TX and RX paths functions
20 in polling mode.
22 This patch adds the dcan driver support to am335x chip.
24 Signed-off-by: Anil Kumar Ch <anilkumar@ti.com>
25 ---
26 drivers/net/can/Kconfig | 2 +
27 drivers/net/can/Makefile | 1 +
28 drivers/net/can/d_can/Kconfig | 14 +
29 drivers/net/can/d_can/Makefile | 8 +
30 drivers/net/can/d_can/d_can.c | 1336 ++++++++++++++++++++++++++++++++
31 drivers/net/can/d_can/d_can.h | 67 ++
32 drivers/net/can/d_can/d_can_platform.c | 256 ++++++
33 include/linux/can/platform/d_can.h | 53 ++
34 8 files changed, 1737 insertions(+), 0 deletions(-)
35 create mode 100644 drivers/net/can/d_can/Kconfig
36 create mode 100644 drivers/net/can/d_can/Makefile
37 create mode 100644 drivers/net/can/d_can/d_can.c
38 create mode 100644 drivers/net/can/d_can/d_can.h
39 create mode 100644 drivers/net/can/d_can/d_can_platform.c
40 create mode 100644 include/linux/can/platform/d_can.h
42 diff --git a/drivers/net/can/Kconfig b/drivers/net/can/Kconfig
43 index f6c98fb..6851445 100644
44 --- a/drivers/net/can/Kconfig
45 +++ b/drivers/net/can/Kconfig
46 @@ -116,6 +116,8 @@ source "drivers/net/can/sja1000/Kconfig"
48 source "drivers/net/can/c_can/Kconfig"
50 +source "drivers/net/can/d_can/Kconfig"
51 +
52 source "drivers/net/can/usb/Kconfig"
54 source "drivers/net/can/softing/Kconfig"
55 diff --git a/drivers/net/can/Makefile b/drivers/net/can/Makefile
56 index 24ebfe8..3377679 100644
57 --- a/drivers/net/can/Makefile
58 +++ b/drivers/net/can/Makefile
59 @@ -14,6 +14,7 @@ obj-y += softing/
60 obj-$(CONFIG_CAN_SJA1000) += sja1000/
61 obj-$(CONFIG_CAN_MSCAN) += mscan/
62 obj-$(CONFIG_CAN_C_CAN) += c_can/
63 +obj-$(CONFIG_CAN_D_CAN) += d_can/
64 obj-$(CONFIG_CAN_AT91) += at91_can.o
65 obj-$(CONFIG_CAN_TI_HECC) += ti_hecc.o
66 obj-$(CONFIG_CAN_MCP251X) += mcp251x.o
67 diff --git a/drivers/net/can/d_can/Kconfig b/drivers/net/can/d_can/Kconfig
68 new file mode 100644
69 index 0000000..e5e9dcf
70 --- /dev/null
71 +++ b/drivers/net/can/d_can/Kconfig
72 @@ -0,0 +1,14 @@
73 +menuconfig CAN_D_CAN
74 + tristate "Bosch D_CAN devices"
75 + depends on CAN_DEV && HAS_IOMEM
76 +
77 +if CAN_D_CAN
78 +
79 +config CAN_D_CAN_PLATFORM
80 + tristate "Generic Platform Bus based D_CAN driver"
81 + ---help---
82 + This driver adds support for the D_CAN chips connected to
83 + the "platform bus" (Linux abstraction for directly to the
84 + processor attached devices) which can be found on am335x
85 + and dm814x boards from TI (http://www.ti.com).
86 +endif
87 diff --git a/drivers/net/can/d_can/Makefile b/drivers/net/can/d_can/Makefile
88 new file mode 100644
89 index 0000000..80560c5
90 --- /dev/null
91 +++ b/drivers/net/can/d_can/Makefile
92 @@ -0,0 +1,8 @@
93 +#
94 +# Makefile for the Bosch D_CAN controller drivers.
95 +#
96 +
97 +obj-$(CONFIG_CAN_D_CAN) += d_can.o
98 +obj-$(CONFIG_CAN_D_CAN_PLATFORM) += d_can_platform.o
99 +
100 +ccflags-$(CONFIG_CAN_DEBUG_DEVICES) := -DDEBUG
101 diff --git a/drivers/net/can/d_can/d_can.c b/drivers/net/can/d_can/d_can.c
102 new file mode 100644
103 index 0000000..e001db0
104 --- /dev/null
105 +++ b/drivers/net/can/d_can/d_can.c
106 @@ -0,0 +1,1336 @@
107 +/*
108 + * CAN bus driver for Bosch D_CAN controller
109 + *
110 + * Copyright (C) 2011 Texas Instruments, Inc. - http://www.ti.com/
111 + * Anil Kumar Ch <anilkumar@ti.com>
112 + *
113 + * Base taken from C_CAN driver
114 + * Copyright (C) 2010 ST Microelectronics
115 + * - Bhupesh Sharma <bhupesh.sharma@st.com>
116 + *
117 + * Borrowed heavily from the C_CAN driver originally written by:
118 + * Copyright (C) 2007
119 + * - Sascha Hauer, Marc Kleine-Budde, Pengutronix <s.hauer@pengutronix.de>
120 + * - Simon Kallweit, intefo AG <simon.kallweit@intefo.ch>
121 + *
122 + * Bosch D_CAN controller is compliant to CAN protocol version 2.0 part A and B.
123 + * Bosch D_CAN user manual can be obtained from:
124 + * http://www.semiconductors.bosch.de/media/en/pdf/ipmodules_1/can/
125 + * d_can_users_manual_111.pdf
126 + *
127 + * This program is free software; you can redistribute it and/or
128 + * modify it under the terms of the GNU General Public License as
129 + * published by the Free Software Foundation version 2.
130 + *
131 + * This program is distributed "as is" WITHOUT ANY WARRANTY of any
132 + * kind, whether express or implied; without even the implied warranty
133 + * of MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
134 + * GNU General Public License for more details.
135 + */
136 +
137 +#include <linux/kernel.h>
138 +#include <linux/module.h>
139 +#include <linux/interrupt.h>
140 +#include <linux/delay.h>
141 +#include <linux/netdevice.h>
142 +#include <linux/if_arp.h>
143 +#include <linux/if_ether.h>
144 +#include <linux/list.h>
145 +#include <linux/io.h>
146 +
147 +#include <linux/can.h>
148 +#include <linux/can/dev.h>
149 +#include <linux/can/error.h>
150 +
151 +#include "d_can.h"
152 +
153 +/* TI D_CAN module registers */
154 +#define D_CAN_CTL 0x0 /* CAN control register */
155 +#define D_CAN_ES 0x4 /* Error and status */
156 +#define D_CAN_PEEOI_REG 0x4 /* Parity error EOI */
157 +#define D_CAN_ERRC 0x8 /* Error counter */
158 +#define D_CAN_BTR 0xC /* Bit timing */
159 +#define D_CAN_INT 0x10 /* Interrupt register */
160 +#define D_CAN_TEST 0x14 /* Test register */
161 +#define D_CAN_PERR 0x1C /* Parity Error Code */
162 +#define D_CAN_ABOTR 0x80 /* Auto-Bus-On Time */
163 +#define D_CAN_TXRQ_X 0x84 /* Transmission Request X */
164 +#define D_CAN_TXRQ(n) (0x88 + (n * 4)) /* Transmission request */
165 +#define D_CAN_NWDAT_X 0x98 /* New data X register */
166 +#define D_CAN_NWDAT(n) (0x9C + (n * 4)) /* New data */
167 +#define D_CAN_INTPND_X 0xAC /* Interrupt Pending X */
168 +#define D_CAN_INTPND(n) (0xB0 + (n * 4)) /* Interrupt Pending */
169 +#define D_CAN_MSGVAL_X 0xC0 /* Message Valid X */
170 +#define D_CAN_MSGVAL(n) (0xC4 + (n * 4)) /* Message Valid */
171 +#define D_CAN_INTMUX(n) (0xD8 + (n * 4)) /* Interrupt Multiplexer */
172 +#define D_CAN_IFCMD(n) (0x100 + (n * 0x20)) /* Command */
173 +#define D_CAN_IFMSK(n) (0x104 + (n * 0x20)) /* Mask */
174 +#define D_CAN_IFARB(n) (0x108 + (n * 0x20)) /* Arbitration */
175 +#define D_CAN_IFMCTL(n) (0x10c + (n * 0x20)) /* Message ctl */
176 +#define D_CAN_IFDATA(n) (0x110 + (n * 0x20)) /* DATA A */
177 +#define D_CAN_IFDATB(n) (0x114 + (n * 0x20)) /* DATA B */
178 +#define D_CAN_IF3OBS 0x140 /* IF3 Observation */
179 +#define D_CAN_IF3UPD(n) (0x160 + (n * 4)) /* Update enable */
180 +#define D_CAN_TIOC 0x1E0 /* CAN TX IO Control */
181 +#define D_CAN_RIOC 0x1E4 /* CAN RX IO Control */
182 +
183 +/* Control register Bit fields */
184 +#define D_CAN_CTL_WUBA BIT(26) /* Automatic wake-up on bus activity */
185 +#define D_CAN_CTL_PDR BIT(24) /* Request for local low power mode */
186 +#define D_CAN_CTL_DE3 BIT(20) /* Enable DMA request line for IF3 */
187 +#define D_CAN_CTL_DE2 BIT(19) /* Enable DMA request line for IF2 */
188 +#define D_CAN_CTL_DE1 BIT(18) /* Enable DMA request line for IF1 */
189 +#define D_CAN_CTL_IE1 BIT(17) /* Interrupt line 1 enable */
190 +#define D_CAN_CTL_INITDBG BIT(16) /* Init state for debug access */
191 +#define D_CAN_CTL_SWR BIT(15) /* S/W reset enable */
192 +#define D_CAN_CTL_PMD (0xF << 10) /* Parity on/off */
193 +#define D_CAN_CTL_ABO BIT(9) /* Auto bus on enable */
194 +#define D_CAN_CTL_IDS BIT(8) /* Interruption debug support enable */
195 +#define D_CAN_CTL_TEST BIT(7) /* Test mode enable */
196 +#define D_CAN_CTL_CCE BIT(6) /* Configuration change enable */
197 +#define D_CAN_CTL_DISABLE_AR BIT(5) /* Disable automatic retransmission */
198 +#define D_CAN_CTL_ENABLE_AR (0 << 5)
199 +#define D_CAN_CTL_EIE BIT(3) /* Error interrupt enable */
200 +#define D_CAN_CTL_SIE BIT(2) /* Status change int enable */
201 +#define D_CAN_CTL_IE0 BIT(1) /* Interrupt line 0 enable */
202 +#define D_CAN_CTL_INIT BIT(0) /* D_CAN initialization mode */
203 +
204 +/* D_CAN Error and Status and Parity Error EOI reg bit fields */
205 +#define D_CAN_ES_PDA BIT(10) /* Local power-down ACK */
206 +#define D_CAN_ES_WUP BIT(9) /* Wkae up pending */
207 +#define D_CAN_ES_PER BIT(8) /* Parity error detected */
208 +#define D_CAN_ES_BOFF BIT(7) /* Bus off state */
209 +#define D_CAN_ES_EWARN BIT(6) /* Warning state */
210 +#define D_CAN_ES_EPASS BIT(5) /* Error passive state */
211 +#define D_CAN_ES_RXOK BIT(4) /* Received a msg successfully */
212 +#define D_CAN_ES_TXOK BIT(3) /* Transmitted a msg successfully */
213 +#define D_CAN_ES_LEC_MASK 0x7 /* Last error code */
214 +
215 +/* Parity error reg bit fields */
216 +#define D_CAN_PEEOI BIT(8) /* EOI indication for parity error */
217 +
218 +/* Error counter reg bit fields */
219 +#define D_CAN_ERRC_RP_SHIFT 15
220 +#define D_CAN_ERRC_RP_MASK BIT(15) /* Receive error passive */
221 +#define D_CAN_ERRC_REC_SHIFT 8
222 +#define D_CAN_ERRC_REC_MASK (0x7F << 8) /* Receive err counter */
223 +#define D_CAN_ERRC_TEC_SHIFT 0
224 +#define D_CAN_ERRC_TEC_MASK (0xFF << 0) /* Transmit err counter */
225 +
226 +/* Bit timing reg bit fields */
227 +#define D_CAN_BTR_BRPE_SHIFT 16
228 +#define D_CAN_BTR_BRPE_MASK (0xF << 16) /* Baud rate prescaler ext */
229 +#define D_CAN_BTR_TSEG2_SHIFT 12
230 +#define D_CAN_BTR_TSEG2_MASK (0x7 << 12) /* Time seg after smpl point */
231 +#define D_CAN_BTR_TSEG1_SHIFT 8
232 +#define D_CAN_BTR_TSEG1_MASK (0xF << 8) /* Time seg before smpl point */
233 +#define D_CAN_BTR_SJW_SHIFT 6
234 +#define D_CAN_BTR_SJW_MASK (0x3 << 6) /* Syncronization jump width */
235 +#define D_CAN_BTR_BRP_SHIFT 0
236 +#define D_CAN_BTR_BRP_MASK (0x3F << 0) /* Baud rate prescaler */
237 +
238 +/* D_CAN Test register bit fields */
239 +#define D_CAN_TEST_RDA BIT(9) /* RAM direct access enable */
240 +#define D_CAN_TEST_EXL BIT(8) /* External loopback mode */
241 +#define D_CAN_TEST_RX BIT(7) /* Monitors the reveive pin */
242 +#define D_CAN_TEST_TX (0x3 << 5) /* Control of CAN_TX pin */
243 +#define D_CAN_TEST_LBACK BIT(4) /* Loopback mode */
244 +#define D_CAN_TEST_SILENT BIT(3) /* Silent mdoe */
245 +
246 +/* D_CAN Parity error reg bit fields */
247 +#define D_CAN_PERR_WN_MASK (0x7 << 8) /* Parity error word nuber */
248 +#define D_CAN_PERR_MN_MASK 0xFF /* Parity error msg object */
249 +
250 +/* D_CAN X registers bit fields */
251 +#define D_CAN_BIT_FIELD(n) (0x3 << (2 * n)) /* X reg's bit field 1 mask */
252 +
253 +/* D_CAN IF command reg bit fields */
254 +#define D_CAN_IF_CMD_WR BIT(23) /* Write/read */
255 +#define D_CAN_IF_CMD_MASK BIT(22) /* Access mask bits */
256 +#define D_CAN_IF_CMD_ARB BIT(21) /* Access arbitration bits */
257 +#define D_CAN_IF_CMD_CONTROL BIT(20) /* Acess control bits */
258 +#define D_CAN_IF_CMD_CIP BIT(19) /* Clear int pending */
259 +#define D_CAN_IF_CMD_TXRQST BIT(18) /* Access transmission request */
260 +#define D_CAN_IF_CMD_DATAA BIT(17) /* Access Data Bytes 0-3 */
261 +#define D_CAN_IF_CMD_DATAB BIT(16) /* Access Data Bytes 4-7 */
262 +#define D_CAN_IF_CMD_BUSY BIT(15) /* Busy flag */
263 +#define D_CAN_IF_CMD_DAM BIT(14) /* Activation of DMA */
264 +#define D_CAN_IF_CMD_MN_MASK 0xFF /* No. of msg's used for DMA T/F */
265 +#define D_CAN_IF_CMD_ALL (D_CAN_IF_CMD_MASK | D_CAN_IF_CMD_ARB | \
266 + D_CAN_IF_CMD_CONTROL | D_CAN_IF_CMD_TXRQST | \
267 + D_CAN_IF_CMD_DATAA | D_CAN_IF_CMD_DATAB)
268 +
269 +/* D_CAN IF mask reg bit fields */
270 +#define D_CAN_IF_MASK_MX BIT(31) /* Mask Extended Identifier */
271 +#define D_CAN_IF_MASK_MD BIT(30) /* Mask Message direction */
272 +
273 +/* D_CAN IF Arbitration */
274 +#define D_CAN_IF_ARB_MSGVAL BIT(31) /* Message Vaild */
275 +#define D_CAN_IF_ARB_MSGXTD BIT(30) /* Extended Identifier 0-11 1-29 */
276 +#define D_CAN_IF_ARB_DIR_XMIT BIT(29) /* Message direction 0-R 1-T */
277 +
278 +/* D_CAN IF Message control */
279 +#define D_CAN_IF_MCTL_NEWDAT BIT(15) /* New data available */
280 +#define D_CAN_IF_MCTL_MSGLST BIT(14) /* Message lost, only for receive */
281 +#define D_CAN_IF_MCTL_CLR_MSGLST (0 << 14)
282 +#define D_CAN_IF_MCTL_INTPND BIT(13) /* Interrupt pending */
283 +#define D_CAN_IF_MCTL_UMASK BIT(12) /* Use acceptance mask */
284 +#define D_CAN_IF_MCTL_TXIE BIT(11) /* Transmit int enable */
285 +#define D_CAN_IF_MCTL_RXIE BIT(10) /* Receive int enable */
286 +#define D_CAN_IF_MCTL_RMTEN BIT(9) /* Remote enable */
287 +#define D_CAN_IF_MCTL_TXRQST BIT(8) /* Transmit request */
288 +#define D_CAN_IF_MCTL_EOB BIT(7) /* Data frames */
289 +#define D_CAN_IF_MCTL_DLC_MASK 0xF /* Data length code */
290 +
291 +/* D_CAN IF3 Observation reg bit fields */
292 +#define D_CAN_IF3OBS_UP BIT(15) /* Update data status */
293 +#define D_CAN_IF3OBS_SDB BIT(12) /* DataB read out status */
294 +#define D_CAN_IF3OBS_SDA BIT(11) /* DataA read out status */
295 +#define D_CAN_IF3OBS_SC BIT(10) /* Contol bits read out status */
296 +#define D_CAN_IF3OBS_SA BIT(9) /* Arbitration read out status */
297 +#define D_CAN_IF3OBS_SM BIT(8) /* Mask bits read out status */
298 +#define D_CAN_IF3OBS_DB BIT(4) /* Data B read observation */
299 +#define D_CAN_IF3OBS_DA BIT(3) /* Data A read observation */
300 +#define D_CAN_IF3OBS_CTL BIT(2) /* Control read observation */
301 +#define D_CAN_IF3OBS_ARB BIT(1) /* Arbitration data read observation */
302 +#define D_CAN_IF3OBS_MASK BIT(0) /* Mask data read observation */
303 +
304 +/* D_CAN TX I/O reg bit fields */
305 +#define D_CAN_TIOC_PU BIT(18) /* CAN_TX pull up/down select */
306 +#define D_CAN_TIOC_PD BIT(17) /* CAN_TX pull disable */
307 +#define D_CAN_TIOC_OD BIT(16) /* CAN_TX open drain enable */
308 +#define D_CAN_TIOC_FUNC BIT(3) /* CAN_TX function */
309 +#define D_CAN_TIOC_DIR BIT(2) /* CAN_TX data direction */
310 +#define D_CAN_TIOC_OUT BIT(1) /* CAN_TX data out write */
311 +#define D_CAN_TIOC_IN BIT(0) /* CAN_TX data in */
312 +
313 +/* D_CAN RX I/O reg bit fields */
314 +#define D_CAN_RIOC_PU BIT(18) /* CAN_RX pull up/down select */
315 +#define D_CAN_RIOC_PD BIT(17) /* CAN_RX pull disable */
316 +#define D_CAN_RIOC_OD BIT(16) /* CAN_RX open drain enable */
317 +#define D_CAN_RIOC_FUNC BIT(3) /* CAN_RX function */
318 +#define D_CAN_RIOC_DIR BIT(2) /* CAN_RX data direction */
319 +#define D_CAN_RIOC_OUT BIT(1) /* CAN_RX data out write */
320 +#define D_CAN_RTIOC_IN BIT(0) /* CAN_RX data in */
321 +
322 +#define D_CAN_SET_REG 0xFFFFFFFF
323 +
324 +#define D_CAN_CANMID_IDE BIT(31) /* Extended frame format */
325 +#define D_CAN_CANMID_AME BIT(30) /* Acceptance mask enable */
326 +#define D_CAN_CANMID_AAM BIT(29) /* Auto answer mode */
327 +
328 +/*
329 + * IF register masks:
330 + */
331 +#define IFX_WRITE_IDR(x) ((x) & 0x1FFFFFFF)
332 +
333 +#define IFX_CMD_BITS(x) ((x) & 0xFFFFFF00)
334 +#define IFX_CMD_MSG_NUMBER(x) ((x) & 0xFF)
335 +
336 +/* message object split */
337 +#define D_CAN_NUM_OF_OBJECTS 64
338 +#define D_CAN_MSG_OBJ_RX_NUM 32
339 +#define D_CAN_MSG_OBJ_TX_NUM 32
340 +
341 +#define D_CAN_MSG_OBJ_RX_FIRST 1
342 +#define D_CAN_MSG_OBJ_RX_LAST (D_CAN_MSG_OBJ_RX_FIRST + \
343 + D_CAN_MSG_OBJ_RX_NUM - 1)
344 +
345 +#define D_CAN_MSG_OBJ_TX_FIRST (D_CAN_MSG_OBJ_RX_LAST + 1)
346 +#define D_CAN_MSG_OBJ_TX_LAST (D_CAN_MSG_OBJ_TX_FIRST + \
347 + D_CAN_MSG_OBJ_TX_NUM - 1)
348 +
349 +#define D_CAN_MSG_OBJ_RX_SPLIT 17
350 +#define D_CAN_MSG_OBJ_RX_LOW_LAST (D_CAN_MSG_OBJ_RX_SPLIT - 1)
351 +
352 +#define D_CAN_NEXT_MSG_OBJ_MASK (D_CAN_MSG_OBJ_TX_NUM - 1)
353 +
354 +/* status interrupt */
355 +#define STATUS_INTERRUPT 0x8000
356 +
357 +/* global interrupt masks */
358 +#define ENABLE_ALL_INTERRUPTS 1
359 +#define DISABLE_ALL_INTERRUPTS 0
360 +
361 +/* minimum timeout for checking BUSY status */
362 +#define MIN_TIMEOUT_VALUE 6
363 +
364 +/* Wait for ~1 sec for INIT bit */
365 +#define D_CAN_WAIT_COUNT 100
366 +
367 +#define D_CAN_IF_RX_NUM 0
368 +#define D_CAN_IF_TX_NUM 1
369 +
370 +#define D_CAN_GET_XREG_NUM(priv, reg) (__ffs(d_can_read(priv, reg))/4)
371 +
372 +/* CAN Bittiming constants as per D_CAN specs */
373 +static struct can_bittiming_const d_can_bittiming_const = {
374 + .name = D_CAN_DRV_NAME,
375 + .tseg1_min = 1, /* Time segment 1 = prop_seg + phase_seg1 */
376 + .tseg1_max = 16,
377 + .tseg2_min = 1, /* Time segment 2 = phase_seg2 */
378 + .tseg2_max = 8,
379 + .sjw_max = 4,
380 + .brp_min = 1,
381 + .brp_max = 1024, /* 6-bit BRP field + 4-bit BRPE field*/
382 + .brp_inc = 1,
383 +};
384 +
385 +/* d_can lec values */
386 +enum d_can_lec_type {
387 + LEC_NO_ERROR = 0,
388 + LEC_STUFF_ERROR,
389 + LEC_FORM_ERROR,
390 + LEC_ACK_ERROR,
391 + LEC_BIT1_ERROR,
392 + LEC_BIT0_ERROR,
393 + LEC_CRC_ERROR,
394 + LEC_UNUSED,
395 +};
396 +
397 +/*
398 + * d_can error types:
399 + * Bus errors (BUS_OFF, ERROR_WARNING, ERROR_PASSIVE) are supported
400 + */
401 +enum d_can_bus_error_types {
402 + D_CAN_NO_ERROR = 0,
403 + D_CAN_BUS_OFF,
404 + D_CAN_ERROR_WARNING,
405 + D_CAN_ERROR_PASSIVE,
406 +};
407 +
408 +static inline void d_can_write(struct d_can_priv *priv, u32 reg, u32 val)
409 +{
410 + __raw_writel(val, priv->base + reg);
411 +}
412 +
413 +static inline u32 d_can_read(struct d_can_priv *priv, int reg)
414 +{
415 + return __raw_readl(priv->base + reg);
416 +}
417 +
418 +static inline void d_can_set_bit(struct d_can_priv *priv, int reg,
419 + u32 bit_mask)
420 +{
421 + d_can_write(priv, reg, d_can_read(priv, reg) | bit_mask);
422 +}
423 +
424 +static inline u32 d_can_get_bit(struct d_can_priv *priv, int reg,
425 + u32 bit_mask)
426 +{
427 + return (d_can_read(priv, reg) & bit_mask) ? 1 : 0;
428 +}
429 +
430 +static inline void d_can_clear_bit(struct d_can_priv *priv, int reg,
431 + u32 bit_mask)
432 +{
433 + d_can_write(priv, reg, d_can_read(priv, reg) & ~bit_mask);
434 +}
435 +
436 +static inline int get_tx_next_msg_obj(const struct d_can_priv *priv)
437 +{
438 + return (priv->tx_next & D_CAN_NEXT_MSG_OBJ_MASK) +
439 + D_CAN_MSG_OBJ_TX_FIRST;
440 +}
441 +
442 +static inline int get_tx_echo_msg_obj(const struct d_can_priv *priv)
443 +{
444 + return (priv->tx_echo & D_CAN_NEXT_MSG_OBJ_MASK) +
445 + D_CAN_MSG_OBJ_TX_FIRST;
446 +}
447 +
448 +static void d_can_interrupts(struct d_can_priv *priv, int enable)
449 +{
450 + unsigned int cntrl_save = d_can_read(priv, D_CAN_CTL);
451 +
452 + if (enable)
453 + cntrl_save |= (D_CAN_CTL_IE1 | D_CAN_CTL_EIE |
454 + D_CAN_CTL_IE0);
455 + else
456 + cntrl_save &= ~(D_CAN_CTL_IE1 | D_CAN_CTL_SIE |
457 + D_CAN_CTL_EIE | D_CAN_CTL_IE0);
458 +
459 + d_can_write(priv, D_CAN_CTL, cntrl_save);
460 +}
461 +
462 +static inline int d_can_msg_obj_is_busy(struct d_can_priv *priv, int iface)
463 +{
464 + int count = MIN_TIMEOUT_VALUE;
465 +
466 + while (count && d_can_read(priv, D_CAN_IFCMD(iface)) &
467 + D_CAN_IF_CMD_BUSY) {
468 + count--;
469 + udelay(1);
470 + }
471 +
472 + if (!count)
473 + return 1;
474 +
475 + return 0;
476 +}
477 +
478 +static inline void d_can_object_get(struct net_device *dev,
479 + int iface, int objno, int mask)
480 +{
481 + struct d_can_priv *priv = netdev_priv(dev);
482 +
483 + /*
484 + * As per specs, after writting the message object number in the
485 + * IF command register the transfer b/w interface register and
486 + * message RAM must be complete in 12 CAN-CLK period.
487 + */
488 + d_can_write(priv, D_CAN_IFCMD(iface), IFX_CMD_BITS(mask) |
489 + IFX_CMD_MSG_NUMBER(objno));
490 +
491 + if (d_can_msg_obj_is_busy(priv, iface))
492 + netdev_err(dev, "timed out in object get\n");
493 +}
494 +
495 +static inline void d_can_object_put(struct net_device *dev,
496 + int iface, int objno, int mask)
497 +{
498 + struct d_can_priv *priv = netdev_priv(dev);
499 +
500 + /*
501 + * As per specs, after writting the message object number in the
502 + * IF command request register the transfer b/w interface
503 + * register and message RAM must be complete in 12 CAN-CLK
504 + * period.
505 + */
506 + d_can_write(priv, D_CAN_IFCMD(iface), D_CAN_IF_CMD_WR |
507 + IFX_CMD_BITS(mask) | IFX_CMD_MSG_NUMBER(objno));
508 +
509 + if (d_can_msg_obj_is_busy(priv, iface))
510 + netdev_err(dev, "timed out in object put\n");
511 +}
512 +
513 +static void d_can_write_msg_object(struct net_device *dev,
514 + int iface, struct can_frame *frame, int objno)
515 +{
516 + int i;
517 + u32 flags = 0;
518 + unsigned int id;
519 + u32 dataA = 0;
520 + u32 dataB = 0;
521 + struct d_can_priv *priv = netdev_priv(dev);
522 +
523 + if (!(frame->can_id & CAN_RTR_FLAG))
524 + flags |= D_CAN_IF_ARB_DIR_XMIT;
525 +
526 + if (frame->can_id & CAN_EFF_FLAG) {
527 + id = frame->can_id & CAN_EFF_MASK;
528 + flags |= D_CAN_IF_ARB_MSGXTD;
529 + } else
530 + id = ((frame->can_id & CAN_SFF_MASK) << 18);
531 +
532 + flags |= D_CAN_IF_ARB_MSGVAL;
533 + d_can_write(priv, D_CAN_IFARB(iface), IFX_WRITE_IDR(id) | flags);
534 +
535 + for (i = 0; i < frame->can_dlc; i++) {
536 + if (i < 4)
537 + dataA |= (frame->data[i] << (8 * i));
538 + else
539 + dataB |= (frame->data[i] << (8 * (i - 4)));
540 + }
541 +
542 + /* DATA write to Message object registers DATAA and DATAB */
543 + if (frame->can_dlc < 4)
544 + d_can_write(priv, D_CAN_IFDATA(iface), dataA);
545 + else {
546 + d_can_write(priv, D_CAN_IFDATB(iface), dataB);
547 + d_can_write(priv, D_CAN_IFDATA(iface), dataA);
548 + }
549 +
550 + /* enable interrupt for this message object */
551 + d_can_write(priv, D_CAN_IFMCTL(iface),
552 + D_CAN_IF_MCTL_TXIE | D_CAN_IF_MCTL_EOB |
553 + D_CAN_IF_MCTL_TXRQST | D_CAN_IF_MCTL_NEWDAT |
554 + frame->can_dlc);
555 +
556 + /* Put message data into message RAM */
557 + d_can_object_put(dev, iface, objno, D_CAN_IF_CMD_ALL);
558 +}
559 +
560 +static inline void d_can_mark_rx_msg_obj(struct net_device *dev,
561 + int iface, int ctrl_mask,
562 + int obj)
563 +{
564 + struct d_can_priv *priv = netdev_priv(dev);
565 +
566 + d_can_write(priv, D_CAN_IFMCTL(iface), ctrl_mask
567 + & ~(D_CAN_IF_MCTL_MSGLST | D_CAN_IF_MCTL_INTPND));
568 +
569 + d_can_object_put(dev, iface, obj, D_CAN_IF_CMD_CONTROL);
570 +}
571 +
572 +static inline void d_can_activate_all_lower_rx_msg_obj(struct net_device *dev,
573 + int iface,
574 + int ctrl_mask)
575 +{
576 + int i;
577 + struct d_can_priv *priv = netdev_priv(dev);
578 +
579 + for (i = D_CAN_MSG_OBJ_RX_FIRST; i <= D_CAN_MSG_OBJ_RX_LOW_LAST; i++) {
580 + d_can_write(priv, D_CAN_IFMCTL(iface),
581 + ctrl_mask & ~(D_CAN_IF_MCTL_MSGLST |
582 + D_CAN_IF_MCTL_INTPND | D_CAN_IF_MCTL_NEWDAT));
583 + d_can_object_put(dev, iface, i, D_CAN_IF_CMD_CONTROL);
584 + }
585 +}
586 +
587 +static inline void d_can_activate_rx_msg_obj(struct net_device *dev,
588 + int iface, int ctrl_mask,
589 + int obj)
590 +{
591 + struct d_can_priv *priv = netdev_priv(dev);
592 +
593 + d_can_write(priv, D_CAN_IFMCTL(iface),
594 + ctrl_mask & ~(D_CAN_IF_MCTL_MSGLST |
595 + D_CAN_IF_MCTL_INTPND | D_CAN_IF_MCTL_NEWDAT));
596 + d_can_object_put(dev, iface, obj, D_CAN_IF_CMD_CONTROL);
597 +}
598 +
599 +static void d_can_handle_lost_msg_obj(struct net_device *dev,
600 + int iface, int objno)
601 +{
602 + struct d_can_priv *priv = netdev_priv(dev);
603 + struct net_device_stats *stats = &dev->stats;
604 + struct sk_buff *skb;
605 + struct can_frame *frame;
606 +
607 + netdev_err(dev, "msg lost in buffer %d\n", objno);
608 +
609 + d_can_object_get(dev, iface, objno, D_CAN_IF_CMD_ALL &
610 + ~D_CAN_IF_CMD_TXRQST);
611 +
612 + d_can_write(priv, D_CAN_IFMCTL(iface), D_CAN_IF_MCTL_CLR_MSGLST);
613 +
614 + d_can_object_put(dev, iface, objno, D_CAN_IF_CMD_CONTROL);
615 +
616 + /* create an error msg */
617 + skb = alloc_can_err_skb(dev, &frame);
618 + if (unlikely(!skb))
619 + return;
620 +
621 + frame->can_id |= CAN_ERR_CRTL;
622 + frame->data[1] = CAN_ERR_CRTL_RX_OVERFLOW;
623 + stats->rx_errors++;
624 + stats->rx_over_errors++;
625 +
626 + netif_receive_skb(skb);
627 +}
628 +
629 +static int d_can_read_msg_object(struct net_device *dev, int iface, int ctrl)
630 +{
631 + int i;
632 + u32 dataA = 0;
633 + u32 dataB = 0;
634 + unsigned int arb_val;
635 + unsigned int mctl_val;
636 + struct d_can_priv *priv = netdev_priv(dev);
637 + struct net_device_stats *stats = &dev->stats;
638 + struct sk_buff *skb;
639 + struct can_frame *frame;
640 +
641 + skb = alloc_can_skb(dev, &frame);
642 + if (!skb) {
643 + stats->rx_dropped++;
644 + return -ENOMEM;
645 + }
646 +
647 + frame->can_dlc = get_can_dlc(ctrl & 0x0F);
648 +
649 + arb_val = d_can_read(priv, D_CAN_IFARB(iface));
650 + mctl_val = d_can_read(priv, D_CAN_IFMCTL(iface));
651 +
652 + if (arb_val & D_CAN_IF_ARB_MSGXTD)
653 + frame->can_id = (arb_val & CAN_EFF_MASK) | CAN_EFF_FLAG;
654 + else
655 + frame->can_id = (arb_val >> 18) & CAN_SFF_MASK;
656 +
657 + if (mctl_val & D_CAN_IF_MCTL_RMTEN)
658 + frame->can_id |= CAN_RTR_FLAG;
659 + else {
660 + dataA = d_can_read(priv, D_CAN_IFDATA(iface));
661 + dataB = d_can_read(priv, D_CAN_IFDATB(iface));
662 + for (i = 0; i < frame->can_dlc; i++) {
663 + /* Writing MO higher 4 data bytes to skb */
664 + if (i <= 3)
665 + frame->data[i] = dataA >> (8 * i); /* Lower */
666 + if (i > 3)
667 + frame->data[i] = dataB >> (8 * (i-4));
668 + }
669 + }
670 +
671 + netif_receive_skb(skb);
672 +
673 + stats->rx_packets++;
674 + stats->rx_bytes += frame->can_dlc;
675 +
676 + return 0;
677 +}
678 +
679 +static void d_can_setup_receive_object(struct net_device *dev, int iface,
680 + int objno, unsigned int mask,
681 + unsigned int id, unsigned int mcont)
682 +{
683 + struct d_can_priv *priv = netdev_priv(dev);
684 +
685 + d_can_write(priv, D_CAN_IFMSK(iface), IFX_WRITE_IDR(mask));
686 + d_can_write(priv, D_CAN_IFARB(iface), IFX_WRITE_IDR(id) |
687 + D_CAN_IF_ARB_MSGVAL);
688 + d_can_write(priv, D_CAN_IFMCTL(iface), mcont);
689 +
690 + d_can_object_put(dev, iface, objno, D_CAN_IF_CMD_ALL &
691 + ~D_CAN_IF_CMD_TXRQST);
692 +
693 + netdev_dbg(dev, "obj no:%d, msgval:0x%08x\n", objno, d_can_read(priv,
694 + D_CAN_MSGVAL(D_CAN_GET_XREG_NUM(priv, D_CAN_MSGVAL_X))));
695 +}
696 +
697 +static void d_can_inval_msg_object(struct net_device *dev, int iface, int objno)
698 +{
699 + struct d_can_priv *priv = netdev_priv(dev);
700 +
701 + d_can_write(priv, D_CAN_IFARB(iface), 0);
702 + d_can_write(priv, D_CAN_IFMCTL(iface), 0);
703 +
704 + d_can_object_put(dev, iface, objno, D_CAN_IF_CMD_ARB |
705 + D_CAN_IF_CMD_CONTROL);
706 +
707 + netdev_dbg(dev, "obj no:%d, msgval:0x%08x\n", objno, d_can_read(priv,
708 + D_CAN_MSGVAL(D_CAN_GET_XREG_NUM(priv, D_CAN_MSGVAL_X))));
709 +}
710 +
711 +static inline int d_can_is_next_tx_obj_busy(struct d_can_priv *priv, int objno)
712 +{
713 + u32 txrq_x_reg_val = D_CAN_GET_XREG_NUM(priv, D_CAN_TXRQ_X);
714 +
715 + /*
716 + * as transmission request register's bit n-1 corresponds to
717 + * message object n, we need to handle the same properly.
718 + */
719 + if (d_can_read(priv, D_CAN_TXRQ(txrq_x_reg_val)) &
720 + (1 << (objno - 1)))
721 + return 1;
722 +
723 + return 0;
724 +}
725 +
726 +static netdev_tx_t d_can_start_xmit(struct sk_buff *skb,
727 + struct net_device *dev)
728 +{
729 + u32 msg_obj_no;
730 + struct d_can_priv *priv = netdev_priv(dev);
731 + struct can_frame *frame = (struct can_frame *)skb->data;
732 +
733 + if (can_dropped_invalid_skb(dev, skb))
734 + return NETDEV_TX_OK;
735 +
736 + msg_obj_no = get_tx_next_msg_obj(priv);
737 +
738 + /* prepare message object for transmission */
739 + d_can_write_msg_object(dev, D_CAN_IF_TX_NUM, frame, msg_obj_no);
740 + can_put_echo_skb(skb, dev, msg_obj_no - D_CAN_MSG_OBJ_TX_FIRST);
741 +
742 + /*
743 + * we have to stop the queue in case of a wrap around or
744 + * if the next TX message object is still in use
745 + */
746 + priv->tx_next++;
747 + if (d_can_is_next_tx_obj_busy(priv, get_tx_next_msg_obj(priv)) ||
748 + (priv->tx_next & D_CAN_NEXT_MSG_OBJ_MASK)
749 + == 0)
750 + netif_stop_queue(dev);
751 +
752 + return NETDEV_TX_OK;
753 +}
754 +
755 +static int d_can_set_bittiming(struct net_device *dev)
756 +{
757 + struct d_can_priv *priv = netdev_priv(dev);
758 + const struct can_bittiming *bt = &priv->can.bittiming;
759 + u32 can_btc;
760 +
761 + can_btc = ((bt->phase_seg2 - 1) & 0x7) << D_CAN_BTR_TSEG2_SHIFT;
762 + can_btc |= ((bt->phase_seg1 + bt->prop_seg - 1)
763 + & 0xF) << D_CAN_BTR_TSEG1_SHIFT;
764 +
765 + can_btc |= ((bt->sjw - 1) & 0x3) << D_CAN_BTR_SJW_SHIFT;
766 +
767 + /* Ten bits contains the BRP, 6 bits for BRP and upper 4 bits for brpe*/
768 + can_btc |= ((bt->brp - 1) & 0x3F) << D_CAN_BTR_BRP_SHIFT;
769 + can_btc |= ((((bt->brp - 1) >> 6) & 0xF) << D_CAN_BTR_BRPE_SHIFT);
770 +
771 + d_can_write(priv, D_CAN_BTR, can_btc);
772 +
773 + netdev_info(dev, "setting CAN BT = %#x\n", can_btc);
774 +
775 + return 0;
776 +}
777 +
778 +/*
779 + * Configure D_CAN message objects for Tx and Rx purposes:
780 + * D_CAN provides a total of 64 message objects that can be configured
781 + * either for Tx or Rx purposes. In this driver first 32 message objects
782 + * are used as a reception FIFO and the reception FIFO is signified by the
783 + * EoB bit being SET. The remaining 32 message objects are kept aside for
784 + * Tx purposes. See user guide document for further details on configuring
785 + * message objects.
786 + */
787 +static void d_can_configure_msg_objects(struct net_device *dev)
788 +{
789 + unsigned int i;
790 +
791 + /* first invalidate all message objects */
792 + for (i = D_CAN_MSG_OBJ_RX_FIRST; i <= D_CAN_NUM_OF_OBJECTS; i++)
793 + d_can_inval_msg_object(dev, D_CAN_IF_RX_NUM, i);
794 +
795 + /* setup receive message objects */
796 + for (i = D_CAN_MSG_OBJ_RX_FIRST; i < D_CAN_MSG_OBJ_RX_LAST; i++)
797 + d_can_setup_receive_object(dev, D_CAN_IF_RX_NUM, i, 0, 0,
798 + (D_CAN_IF_MCTL_RXIE | D_CAN_IF_MCTL_UMASK) &
799 + ~D_CAN_IF_MCTL_EOB);
800 +
801 + /* Last object EoB bit should be 1 for terminate */
802 + d_can_setup_receive_object(dev, D_CAN_IF_RX_NUM, D_CAN_MSG_OBJ_RX_LAST,
803 + 0, 0, D_CAN_IF_MCTL_RXIE | D_CAN_IF_MCTL_UMASK |
804 + D_CAN_IF_MCTL_EOB);
805 +}
806 +
807 +static void d_can_test_mode(struct net_device *dev)
808 +{
809 + struct d_can_priv *priv = netdev_priv(dev);
810 +
811 + /* Test mode is enabled in this step & the specific TEST bits
812 + * are enabled accordingly */
813 + d_can_write(priv, D_CAN_CTL, D_CAN_CTL_EIE |
814 + D_CAN_CTL_IE1 | D_CAN_CTL_IE0 | D_CAN_CTL_TEST);
815 +
816 + if (priv->can.ctrlmode & CAN_CTRLMODE_LISTENONLY) {
817 + /* silent mode : bus-monitoring mode */
818 + d_can_write(priv, D_CAN_TEST, D_CAN_TEST_SILENT);
819 + } else if (priv->can.ctrlmode & CAN_CTRLMODE_LOOPBACK) {
820 + /* loopback mode : useful for self-test function */
821 + d_can_write(priv, D_CAN_TEST, D_CAN_TEST_LBACK);
822 + } else {
823 + /* loopback + silent mode : useful for hot self-test */
824 + d_can_write(priv, D_CAN_TEST, D_CAN_TEST_LBACK |
825 + D_CAN_TEST_SILENT);
826 + }
827 +}
828 +
829 +/*
830 + * Configure D_CAN chip:
831 + * - enable/disable auto-retransmission
832 + * - set operating mode
833 + * - configure message objects
834 + */
835 +static void d_can_init(struct net_device *dev)
836 +{
837 + struct d_can_priv *priv = netdev_priv(dev);
838 + u32 cnt;
839 +
840 + netdev_dbg(dev, "resetting d_can ...\n");
841 + d_can_set_bit(priv, D_CAN_CTL, D_CAN_CTL_SWR);
842 +
843 + /* Enter initialization mode by setting the Init bit */
844 + d_can_set_bit(priv, D_CAN_CTL, D_CAN_CTL_INIT);
845 +
846 + /* enable automatic retransmission */
847 + d_can_set_bit(priv, D_CAN_CTL, D_CAN_CTL_ENABLE_AR);
848 +
849 + /* Set the Configure Change Enable ( CCE) bit */
850 + d_can_set_bit(priv, D_CAN_CTL, D_CAN_CTL_CCE);
851 +
852 + /* Wait for the Init bit to get set */
853 + cnt = D_CAN_WAIT_COUNT;
854 + while (!d_can_get_bit(priv, D_CAN_CTL, D_CAN_CTL_INIT) && cnt != 0) {
855 + --cnt;
856 + udelay(10);
857 + }
858 +
859 + /* set bittiming params */
860 + d_can_set_bittiming(dev);
861 +
862 + d_can_clear_bit(priv, D_CAN_CTL, D_CAN_CTL_INIT | D_CAN_CTL_CCE);
863 +
864 + /* Wait for the Init bit to get clear */
865 + cnt = D_CAN_WAIT_COUNT;
866 + while (d_can_get_bit(priv, D_CAN_CTL, D_CAN_CTL_INIT) && cnt != 0) {
867 + --cnt;
868 + udelay(10);
869 + }
870 +
871 + if (!priv->test_mode) {
872 + /* normal mode*/
873 + d_can_write(priv, D_CAN_CTL, D_CAN_CTL_EIE | D_CAN_CTL_IE1 |
874 + D_CAN_CTL_IE0);
875 + } else
876 + d_can_test_mode(dev);
877 +
878 + /* Enable TX and RX I/O Control pins */
879 + d_can_write(priv, D_CAN_TIOC, D_CAN_TIOC_FUNC);
880 + d_can_write(priv, D_CAN_RIOC, D_CAN_RIOC_FUNC);
881 +
882 + /* configure message objects */
883 + d_can_configure_msg_objects(dev);
884 +
885 + /* set a `lec` value so that we can check for updates later */
886 + d_can_write(priv, D_CAN_ES, LEC_UNUSED);
887 +}
888 +
889 +static void d_can_start(struct net_device *dev)
890 +{
891 + struct d_can_priv *priv = netdev_priv(dev);
892 +
893 + /* basic d_can initialization */
894 + d_can_init(dev);
895 +
896 + priv->can.state = CAN_STATE_ERROR_ACTIVE;
897 +
898 + /* reset tx helper pointers */
899 + priv->tx_next = priv->tx_echo = 0;
900 +
901 + /* enable status change, error and module interrupts */
902 + d_can_interrupts(priv, ENABLE_ALL_INTERRUPTS);
903 +}
904 +
905 +static void d_can_stop(struct net_device *dev)
906 +{
907 + struct d_can_priv *priv = netdev_priv(dev);
908 +
909 + /* disable all interrupts */
910 + d_can_interrupts(priv, DISABLE_ALL_INTERRUPTS);
911 +
912 + /* set the state as STOPPED */
913 + priv->can.state = CAN_STATE_STOPPED;
914 +}
915 +
916 +static int d_can_set_mode(struct net_device *dev, enum can_mode mode)
917 +{
918 + switch (mode) {
919 + case CAN_MODE_START:
920 + d_can_start(dev);
921 + netif_wake_queue(dev);
922 + break;
923 + default:
924 + return -EOPNOTSUPP;
925 + }
926 +
927 + return 0;
928 +}
929 +
930 +static int d_can_get_berr_counter(const struct net_device *dev,
931 + struct can_berr_counter *bec)
932 +{
933 + unsigned int reg_err_counter;
934 + struct d_can_priv *priv = netdev_priv(dev);
935 +
936 + reg_err_counter = d_can_read(priv, D_CAN_ERRC);
937 + bec->rxerr = (reg_err_counter & D_CAN_ERRC_REC_MASK) >>
938 + D_CAN_ERRC_REC_SHIFT;
939 + bec->txerr = reg_err_counter & D_CAN_ERRC_TEC_MASK;
940 +
941 + return 0;
942 +}
943 +
944 +/*
945 + * theory of operation:
946 + *
947 + * priv->tx_echo holds the number of the oldest can_frame put for
948 + * transmission into the hardware, but not yet ACKed by the CAN tx
949 + * complete IRQ.
950 + *
951 + * We iterate from priv->tx_echo to priv->tx_next and check if the
952 + * packet has been transmitted, echo it back to the CAN framework.
953 + * If we discover a not yet transmitted package, stop looking for more.
954 + */
955 +static void d_can_do_tx(struct net_device *dev)
956 +{
957 + u32 msg_obj_no;
958 + struct d_can_priv *priv = netdev_priv(dev);
959 + struct net_device_stats *stats = &dev->stats;
960 + u32 txrq_x_reg_val;
961 + u32 txrq_reg_val;
962 +
963 + for (/* nix */; (priv->tx_next - priv->tx_echo) > 0; priv->tx_echo++) {
964 + msg_obj_no = get_tx_echo_msg_obj(priv);
965 + txrq_x_reg_val = D_CAN_GET_XREG_NUM(priv, D_CAN_TXRQ_X);
966 + txrq_reg_val = d_can_read(priv, D_CAN_TXRQ(txrq_x_reg_val));
967 + if (!(txrq_reg_val & (1 << (msg_obj_no - 1)))) {
968 + can_get_echo_skb(dev,
969 + msg_obj_no - D_CAN_MSG_OBJ_TX_FIRST);
970 + stats->tx_bytes += d_can_read(priv,
971 + D_CAN_IFMCTL(D_CAN_IF_TX_NUM))
972 + & D_CAN_IF_MCTL_DLC_MASK;
973 + stats->tx_packets++;
974 + d_can_inval_msg_object(dev, D_CAN_IF_TX_NUM,
975 + msg_obj_no);
976 + } else
977 + break;
978 + }
979 +
980 + /* restart queue if wrap-up or if queue stalled on last pkt */
981 + if (((priv->tx_next & D_CAN_NEXT_MSG_OBJ_MASK) != 0)
982 + || ((priv->tx_echo & D_CAN_NEXT_MSG_OBJ_MASK)
983 + == 0))
984 + netif_wake_queue(dev);
985 +}
986 +
987 +/*
988 + * theory of operation:
989 + *
990 + * d_can core saves a received CAN message into the first free message
991 + * object it finds free (starting with the lowest). Bits NEWDAT and
992 + * INTPND are set for this message object indicating that a new message
993 + * has arrived. To work-around this issue, we keep two groups of message
994 + * objects whose partitioning is defined by D_CAN_MSG_OBJ_RX_SPLIT.
995 + *
996 + * To ensure in-order frame reception we use the following
997 + * approach while re-activating a message object to receive further
998 + * frames:
999 + * - if the current message object number is lower than
1000 + * D_CAN_MSG_RX_LOW_LAST, do not clear the NEWDAT bit while clearing
1001 + * the INTPND bit.
1002 + * - if the current message object number is equal to
1003 + * D_CAN_MSG_RX_LOW_LAST then clear the NEWDAT bit of all lower
1004 + * receive message objects.
1005 + * - if the current message object number is greater than
1006 + * D_CAN_MSG_RX_LOW_LAST then clear the NEWDAT bit of
1007 + * only this message object.
1008 + */
1009 +static int d_can_do_rx_poll(struct net_device *dev, int quota)
1010 +{
1011 + struct d_can_priv *priv = netdev_priv(dev);
1012 + unsigned int msg_obj, mctrl_reg_val;
1013 + u32 num_rx_pkts = 0;
1014 + u32 intpnd_x_reg_val;
1015 + u32 intpnd_reg_val;
1016 +
1017 + for (msg_obj = D_CAN_MSG_OBJ_RX_FIRST; msg_obj <= D_CAN_MSG_OBJ_RX_LAST
1018 + && quota > 0; msg_obj++) {
1019 +
1020 + intpnd_x_reg_val = D_CAN_GET_XREG_NUM(priv, D_CAN_INTPND_X);
1021 + intpnd_reg_val = d_can_read(priv,
1022 + D_CAN_INTPND(intpnd_x_reg_val));
1023 +
1024 + /*
1025 + * as interrupt pending register's bit n-1 corresponds to
1026 + * message object n, we need to handle the same properly.
1027 + */
1028 + if (intpnd_reg_val & (1 << (msg_obj - 1))) {
1029 +
1030 + d_can_object_get(dev, D_CAN_IF_RX_NUM, msg_obj,
1031 + D_CAN_IF_CMD_ALL &
1032 + ~D_CAN_IF_CMD_TXRQST);
1033 +
1034 + mctrl_reg_val = d_can_read(priv,
1035 + D_CAN_IFMCTL(D_CAN_IF_RX_NUM));
1036 +
1037 + if (!(mctrl_reg_val & D_CAN_IF_MCTL_NEWDAT))
1038 + continue;
1039 +
1040 + /* read the data from the message object */
1041 + d_can_read_msg_object(dev, D_CAN_IF_RX_NUM,
1042 + mctrl_reg_val);
1043 +
1044 + if (mctrl_reg_val & D_CAN_IF_MCTL_EOB)
1045 + d_can_setup_receive_object(dev, D_CAN_IF_RX_NUM,
1046 + D_CAN_MSG_OBJ_RX_LAST, 0, 0,
1047 + D_CAN_IF_MCTL_RXIE | D_CAN_IF_MCTL_UMASK
1048 + | D_CAN_IF_MCTL_EOB);
1049 +
1050 + if (mctrl_reg_val & D_CAN_IF_MCTL_MSGLST) {
1051 + d_can_handle_lost_msg_obj(dev, D_CAN_IF_RX_NUM,
1052 + msg_obj);
1053 + num_rx_pkts++;
1054 + quota--;
1055 + continue;
1056 + }
1057 +
1058 + if (msg_obj < D_CAN_MSG_OBJ_RX_LOW_LAST)
1059 + d_can_mark_rx_msg_obj(dev, D_CAN_IF_RX_NUM,
1060 + mctrl_reg_val, msg_obj);
1061 + else if (msg_obj > D_CAN_MSG_OBJ_RX_LOW_LAST)
1062 + /* activate this msg obj */
1063 + d_can_activate_rx_msg_obj(dev, D_CAN_IF_RX_NUM,
1064 + mctrl_reg_val, msg_obj);
1065 + else if (msg_obj == D_CAN_MSG_OBJ_RX_LOW_LAST)
1066 + /* activate all lower message objects */
1067 + d_can_activate_all_lower_rx_msg_obj(dev,
1068 + D_CAN_IF_RX_NUM, mctrl_reg_val);
1069 +
1070 + num_rx_pkts++;
1071 + quota--;
1072 + }
1073 + }
1074 +
1075 + return num_rx_pkts;
1076 +}
1077 +
1078 +static inline int d_can_has_and_handle_berr(struct d_can_priv *priv)
1079 +{
1080 + return (priv->can.ctrlmode & CAN_CTRLMODE_BERR_REPORTING) &&
1081 + (priv->current_status & LEC_UNUSED);
1082 +}
1083 +
1084 +static int d_can_handle_state_change(struct net_device *dev,
1085 + enum d_can_bus_error_types error_type)
1086 +{
1087 + unsigned int reg_err_counter;
1088 + unsigned int rx_err_passive;
1089 + struct d_can_priv *priv = netdev_priv(dev);
1090 + struct net_device_stats *stats = &dev->stats;
1091 + struct can_frame *cf;
1092 + struct sk_buff *skb;
1093 + struct can_berr_counter bec;
1094 +
1095 + /* propagate the error condition to the CAN stack */
1096 + skb = alloc_can_err_skb(dev, &cf);
1097 + if (unlikely(!skb))
1098 + return 0;
1099 +
1100 + d_can_get_berr_counter(dev, &bec);
1101 + reg_err_counter = d_can_read(priv, D_CAN_ERRC);
1102 + rx_err_passive = (reg_err_counter & D_CAN_ERRC_RP_MASK) >>
1103 + D_CAN_ERRC_RP_SHIFT;
1104 +
1105 + switch (error_type) {
1106 + case D_CAN_ERROR_WARNING:
1107 + /* error warning state */
1108 + priv->can.can_stats.error_warning++;
1109 + priv->can.state = CAN_STATE_ERROR_WARNING;
1110 + cf->can_id |= CAN_ERR_CRTL;
1111 + cf->data[1] = (bec.txerr > bec.rxerr) ?
1112 + CAN_ERR_CRTL_TX_WARNING :
1113 + CAN_ERR_CRTL_RX_WARNING;
1114 + cf->data[6] = bec.txerr;
1115 + cf->data[7] = bec.rxerr;
1116 +
1117 + break;
1118 + case D_CAN_ERROR_PASSIVE:
1119 + /* error passive state */
1120 + priv->can.can_stats.error_passive++;
1121 + priv->can.state = CAN_STATE_ERROR_PASSIVE;
1122 + cf->can_id |= CAN_ERR_CRTL;
1123 + if (rx_err_passive)
1124 + cf->data[1] |= CAN_ERR_CRTL_RX_PASSIVE;
1125 + if (bec.txerr > 127)
1126 + cf->data[1] |= CAN_ERR_CRTL_TX_PASSIVE;
1127 +
1128 + cf->data[6] = bec.txerr;
1129 + cf->data[7] = bec.rxerr;
1130 + break;
1131 + case D_CAN_BUS_OFF:
1132 + /* bus-off state */
1133 + priv->can.state = CAN_STATE_BUS_OFF;
1134 + cf->can_id |= CAN_ERR_BUSOFF;
1135 + /*
1136 + * disable all interrupts in bus-off mode to ensure that
1137 + * the CPU is not hogged down
1138 + */
1139 + d_can_interrupts(priv, DISABLE_ALL_INTERRUPTS);
1140 + can_bus_off(dev);
1141 + break;
1142 + default:
1143 + break;
1144 + }
1145 +
1146 + netif_receive_skb(skb);
1147 + stats->rx_packets++;
1148 + stats->rx_bytes += cf->can_dlc;
1149 +
1150 + return 1;
1151 +}
1152 +
1153 +static int d_can_handle_bus_err(struct net_device *dev,
1154 + enum d_can_lec_type lec_type)
1155 +{
1156 + struct d_can_priv *priv = netdev_priv(dev);
1157 + struct net_device_stats *stats = &dev->stats;
1158 + struct can_frame *cf;
1159 + struct sk_buff *skb;
1160 +
1161 + /*
1162 + * early exit if no lec update or no error.
1163 + * no lec update means that no CAN bus event has been detected
1164 + * since CPU wrote 0x7 value to status reg.
1165 + */
1166 + if (lec_type == LEC_UNUSED || lec_type == LEC_NO_ERROR)
1167 + return 0;
1168 +
1169 + /* propagate the error condition to the CAN stack */
1170 + skb = alloc_can_err_skb(dev, &cf);
1171 + if (unlikely(!skb))
1172 + return 0;
1173 +
1174 + /*
1175 + * check for 'last error code' which tells us the
1176 + * type of the last error to occur on the CAN bus
1177 + */
1178 +
1179 + /* common for all type of bus errors */
1180 + priv->can.can_stats.bus_error++;
1181 + stats->rx_errors++;
1182 + cf->can_id |= CAN_ERR_PROT | CAN_ERR_BUSERROR;
1183 + cf->data[2] |= CAN_ERR_PROT_UNSPEC;
1184 +
1185 + switch (lec_type) {
1186 + case LEC_STUFF_ERROR:
1187 + netdev_dbg(dev, "stuff error\n");
1188 + cf->data[2] |= CAN_ERR_PROT_STUFF;
1189 + break;
1190 + case LEC_FORM_ERROR:
1191 + netdev_dbg(dev, "form error\n");
1192 + cf->data[2] |= CAN_ERR_PROT_FORM;
1193 + break;
1194 + case LEC_ACK_ERROR:
1195 + netdev_dbg(dev, "ack error\n");
1196 + cf->data[2] |= (CAN_ERR_PROT_LOC_ACK |
1197 + CAN_ERR_PROT_LOC_ACK_DEL);
1198 + break;
1199 + case LEC_BIT1_ERROR:
1200 + netdev_dbg(dev, "bit1 error\n");
1201 + cf->data[2] |= CAN_ERR_PROT_BIT1;
1202 + break;
1203 + case LEC_BIT0_ERROR:
1204 + netdev_dbg(dev, "bit0 error\n");
1205 + cf->data[2] |= CAN_ERR_PROT_BIT0;
1206 + break;
1207 + case LEC_CRC_ERROR:
1208 + netdev_dbg(dev, "CRC error\n");
1209 + cf->data[2] |= (CAN_ERR_PROT_LOC_CRC_SEQ |
1210 + CAN_ERR_PROT_LOC_CRC_DEL);
1211 + break;
1212 + default:
1213 + break;
1214 + }
1215 +
1216 + /* set a `lec` value so that we can check for updates later */
1217 + d_can_write(priv, D_CAN_ES, LEC_UNUSED);
1218 +
1219 + netif_receive_skb(skb);
1220 + stats->rx_packets++;
1221 + stats->rx_bytes += cf->can_dlc;
1222 +
1223 + return 1;
1224 +}
1225 +
1226 +static int d_can_poll(struct napi_struct *napi, int quota)
1227 +{
1228 + int lec_type = 0;
1229 + int work_done = 0;
1230 + struct net_device *dev = napi->dev;
1231 + struct d_can_priv *priv = netdev_priv(dev);
1232 +
1233 + priv->irqstatus = d_can_read(priv, D_CAN_INT);
1234 + if (!priv->irqstatus)
1235 + goto end;
1236 +
1237 + /* status events have the highest priority */
1238 + if (priv->irqstatus == STATUS_INTERRUPT) {
1239 + priv->current_status = d_can_read(priv, D_CAN_ES);
1240 +
1241 + /* handle Tx/Rx events */
1242 + if (priv->current_status & D_CAN_ES_TXOK)
1243 + d_can_write(priv, D_CAN_ES,
1244 + priv->current_status & ~D_CAN_ES_TXOK);
1245 +
1246 + if (priv->current_status & D_CAN_ES_RXOK)
1247 + d_can_write(priv, D_CAN_ES,
1248 + priv->current_status & ~D_CAN_ES_RXOK);
1249 +
1250 + /* handle state changes */
1251 + if ((priv->current_status & D_CAN_ES_EWARN) &&
1252 + (!(priv->last_status & D_CAN_ES_EWARN))) {
1253 + netdev_dbg(dev, "entered error warning state\n");
1254 + work_done += d_can_handle_state_change(dev,
1255 + D_CAN_ERROR_WARNING);
1256 + }
1257 + if ((priv->current_status & D_CAN_ES_EPASS) &&
1258 + (!(priv->last_status & D_CAN_ES_EPASS))) {
1259 + netdev_dbg(dev, "entered error passive state\n");
1260 + work_done += d_can_handle_state_change(dev,
1261 + D_CAN_ERROR_PASSIVE);
1262 + }
1263 + if ((priv->current_status & D_CAN_ES_BOFF) &&
1264 + (!(priv->last_status & D_CAN_ES_BOFF))) {
1265 + netdev_dbg(dev, "entered bus off state\n");
1266 + work_done += d_can_handle_state_change(dev,
1267 + D_CAN_BUS_OFF);
1268 + }
1269 +
1270 + /* handle bus recovery events */
1271 + if ((!(priv->current_status & D_CAN_ES_BOFF)) &&
1272 + (priv->last_status & D_CAN_ES_BOFF)) {
1273 + netdev_dbg(dev, "left bus off state\n");
1274 + priv->can.state = CAN_STATE_ERROR_ACTIVE;
1275 + }
1276 + if ((!(priv->current_status & D_CAN_ES_EPASS)) &&
1277 + (priv->last_status & D_CAN_ES_EPASS)) {
1278 + netdev_dbg(dev, "left error passive state\n");
1279 + priv->can.state = CAN_STATE_ERROR_ACTIVE;
1280 + }
1281 +
1282 + priv->last_status = priv->current_status;
1283 +
1284 + /* handle lec errors on the bus */
1285 + lec_type = d_can_has_and_handle_berr(priv);
1286 + if (lec_type)
1287 + work_done += d_can_handle_bus_err(dev, lec_type);
1288 + } else if ((priv->irqstatus >= D_CAN_MSG_OBJ_RX_FIRST) &&
1289 + (priv->irqstatus <= D_CAN_MSG_OBJ_RX_LAST)) {
1290 + /* handle events corresponding to receive message objects */
1291 + work_done += d_can_do_rx_poll(dev, (quota - work_done));
1292 + } else if ((priv->irqstatus >= D_CAN_MSG_OBJ_TX_FIRST) &&
1293 + (priv->irqstatus <= D_CAN_MSG_OBJ_TX_LAST)) {
1294 + /* handle events corresponding to transmit message objects */
1295 + d_can_do_tx(dev);
1296 + }
1297 +
1298 +end:
1299 + if (work_done < quota) {
1300 + napi_complete(napi);
1301 + /* enable all IRQs */
1302 + d_can_interrupts(priv, ENABLE_ALL_INTERRUPTS);
1303 + }
1304 +
1305 + return work_done;
1306 +}
1307 +
1308 +static irqreturn_t d_can_isr(int irq, void *dev_id)
1309 +{
1310 + struct net_device *dev = (struct net_device *)dev_id;
1311 + struct d_can_priv *priv = netdev_priv(dev);
1312 +
1313 + priv->irqstatus = d_can_read(priv, D_CAN_INT);
1314 + if (!priv->irqstatus)
1315 + return IRQ_NONE;
1316 +
1317 + /* disable all interrupts and schedule the NAPI */
1318 + d_can_interrupts(priv, DISABLE_ALL_INTERRUPTS);
1319 + napi_schedule(&priv->napi);
1320 +
1321 + return IRQ_HANDLED;
1322 +}
1323 +
1324 +static int d_can_open(struct net_device *ndev)
1325 +{
1326 + int err;
1327 + struct d_can_priv *priv = netdev_priv(ndev);
1328 +
1329 + /* Open common can device */
1330 + err = open_candev(ndev);
1331 + if (err) {
1332 + netdev_err(ndev, "open_candev() failed %d\n", err);
1333 + return err;
1334 + }
1335 +
1336 + /* register interrupt handler for Message Object (MO)
1337 + * and Error + status change (ES) */
1338 + err = request_irq(ndev->irq, &d_can_isr, IRQF_SHARED, ndev->name,
1339 + ndev);
1340 + if (err) {
1341 + netdev_err(ndev, "failed to request MO_ES interrupt\n");
1342 + goto exit_close_candev;
1343 + }
1344 +
1345 + /* register interrupt handler for only Message Object */
1346 + err = request_irq(priv->irq_obj, &d_can_isr, IRQF_SHARED, ndev->name,
1347 + ndev);
1348 + if (err) {
1349 + netdev_err(ndev, "failed to request MO interrupt\n");
1350 + goto exit_free_irq;
1351 + }
1352 +
1353 + /* start the d_can controller */
1354 + d_can_start(ndev);
1355 +
1356 + napi_enable(&priv->napi);
1357 + netif_start_queue(ndev);
1358 +
1359 + return 0;
1360 +exit_free_irq:
1361 + free_irq(ndev->irq, ndev);
1362 +exit_close_candev:
1363 + close_candev(ndev);
1364 + return err;
1365 +}
1366 +
1367 +static int d_can_close(struct net_device *ndev)
1368 +{
1369 + struct d_can_priv *priv = netdev_priv(ndev);
1370 +
1371 + netif_stop_queue(ndev);
1372 + napi_disable(&priv->napi);
1373 + d_can_stop(ndev);
1374 + free_irq(ndev->irq, ndev);
1375 + free_irq(priv->irq_obj, ndev);
1376 + close_candev(ndev);
1377 +
1378 + return 0;
1379 +}
1380 +
1381 +struct net_device *alloc_d_can_dev(int num_objs)
1382 +{
1383 + struct net_device *dev;
1384 + struct d_can_priv *priv;
1385 +
1386 + dev = alloc_candev(sizeof(struct d_can_priv), num_objs/2);
1387 + if (!dev)
1388 + return NULL;
1389 +
1390 + priv = netdev_priv(dev);
1391 + netif_napi_add(dev, &priv->napi, d_can_poll, num_objs/2);
1392 +
1393 + priv->dev = dev;
1394 + priv->can.bittiming_const = &d_can_bittiming_const;
1395 + priv->can.do_set_mode = d_can_set_mode;
1396 + priv->can.do_get_berr_counter = d_can_get_berr_counter;
1397 + priv->can.ctrlmode_supported = (CAN_CTRLMODE_LOOPBACK |
1398 + CAN_CTRLMODE_LISTENONLY |
1399 + CAN_CTRLMODE_BERR_REPORTING |
1400 + CAN_CTRLMODE_3_SAMPLES);
1401 +
1402 + return dev;
1403 +}
1404 +EXPORT_SYMBOL_GPL(alloc_d_can_dev);
1405 +
1406 +void free_d_can_dev(struct net_device *dev)
1407 +{
1408 + free_candev(dev);
1409 +}
1410 +EXPORT_SYMBOL_GPL(free_d_can_dev);
1411 +
1412 +static const struct net_device_ops d_can_netdev_ops = {
1413 + .ndo_open = d_can_open,
1414 + .ndo_stop = d_can_close,
1415 + .ndo_start_xmit = d_can_start_xmit,
1416 +};
1417 +
1418 +int register_d_can_dev(struct net_device *dev)
1419 +{
1420 + /* we support local echo */
1421 + dev->flags |= IFF_ECHO;
1422 + dev->netdev_ops = &d_can_netdev_ops;
1423 +
1424 + return register_candev(dev);
1425 +}
1426 +EXPORT_SYMBOL_GPL(register_d_can_dev);
1427 +
1428 +void unregister_d_can_dev(struct net_device *dev)
1429 +{
1430 + struct d_can_priv *priv = netdev_priv(dev);
1431 +
1432 + /* disable all interrupts */
1433 + d_can_interrupts(priv, DISABLE_ALL_INTERRUPTS);
1434 +
1435 + unregister_candev(dev);
1436 +}
1437 +EXPORT_SYMBOL_GPL(unregister_d_can_dev);
1438 +
1439 +MODULE_AUTHOR("Anil Kumar Ch <anilkumar@ti.com>");
1440 +MODULE_LICENSE("GPL v2");
1441 +MODULE_VERSION(D_CAN_VERSION);
1442 +MODULE_DESCRIPTION(D_CAN_DRV_DESC);
1443 diff --git a/drivers/net/can/d_can/d_can.h b/drivers/net/can/d_can/d_can.h
1444 new file mode 100644
1445 index 0000000..f096944
1446 --- /dev/null
1447 +++ b/drivers/net/can/d_can/d_can.h
1448 @@ -0,0 +1,67 @@
1449 +/*
1450 + * CAN bus driver for Bosch D_CAN controller
1451 + *
1452 + * Copyright (C) 2011 Texas Instruments, Inc. - http://www.ti.com/
1453 + * Anil Kumar Ch <anilkumar@ti.com>
1454 + *
1455 + * Base taken from C_CAN driver
1456 + * Copyright (C) 2010 ST Microelectronics
1457 + * - Bhupesh Sharma <bhupesh.sharma@st.com>
1458 + *
1459 + * Borrowed heavily from the C_CAN driver originally written by:
1460 + * Copyright (C) 2007
1461 + * - Sascha Hauer, Marc Kleine-Budde, Pengutronix <s.hauer@pengutronix.de>
1462 + * - Simon Kallweit, intefo AG <simon.kallweit@intefo.ch>
1463 + *
1464 + * Bosch D_CAN controller is compliant to CAN protocol version 2.0 part A and B.
1465 + * Bosch D_CAN user manual can be obtained from:
1466 + * http://www.semiconductors.bosch.de/media/en/pdf/ipmodules_1/can/
1467 + * d_can_users_manual_111.pdf
1468 + *
1469 + * This program is free software; you can redistribute it and/or
1470 + * modify it under the terms of the GNU General Public License as
1471 + * published by the Free Software Foundation version 2.
1472 + *
1473 + * This program is distributed "as is" WITHOUT ANY WARRANTY of any
1474 + * kind, whether express or implied; without even the implied warranty
1475 + * of MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
1476 + * GNU General Public License for more details.
1477 + */
1478 +
1479 +#ifndef D_CAN_H
1480 +#define D_CAN_H
1481 +
1482 +#define D_CAN_DRV_NAME "d_can"
1483 +#define D_CAN_VERSION "1.0"
1484 +#define D_CAN_DRV_DESC "CAN bus driver for Bosch D_CAN controller " \
1485 + D_CAN_VERSION
1486 +
1487 +/* d_can private data structure */
1488 +struct d_can_priv {
1489 + struct can_priv can; /* must be the first member */
1490 + struct napi_struct napi;
1491 + struct net_device *dev;
1492 + int current_status;
1493 + int last_status;
1494 + unsigned int irqstatus;
1495 + void __iomem *base;
1496 + u32 napi_weight;
1497 + struct clk *fck;
1498 + struct clk *ick;
1499 + bool test_mode;
1500 + unsigned int irq; /* device IRQ number, for all MO and ES */
1501 + unsigned int irq_obj; /* device IRQ number for only Msg Object */
1502 + unsigned int irq_parity; /* device IRQ number for parity error */
1503 + unsigned long irq_flags; /* for request_irq() */
1504 + unsigned int tx_next;
1505 + unsigned int tx_echo;
1506 + unsigned int rx_next;
1507 + void *priv; /* for board-specific data */
1508 +};
1509 +
1510 +struct net_device *alloc_d_can_dev(int);
1511 +void free_d_can_dev(struct net_device *dev);
1512 +int register_d_can_dev(struct net_device *dev);
1513 +void unregister_d_can_dev(struct net_device *dev);
1514 +
1515 +#endif /* D_CAN_H */
1516 diff --git a/drivers/net/can/d_can/d_can_platform.c b/drivers/net/can/d_can/d_can_platform.c
1517 new file mode 100644
1518 index 0000000..b430a18
1519 --- /dev/null
1520 +++ b/drivers/net/can/d_can/d_can_platform.c
1521 @@ -0,0 +1,256 @@
1522 +/*
1523 + * Platform CAN bus driver for Bosch D_CAN controller
1524 + *
1525 + * Copyright (C) 2011 Texas Instruments, Inc. - http://www.ti.com/
1526 + * Anil Kumar Ch <anilkumar@ti.com>
1527 + *
1528 + * Base taken from C_CAN driver
1529 + * Copyright (C) 2010 ST Microelectronics
1530 + * - Bhupesh Sharma <bhupesh.sharma@st.com>
1531 + *
1532 + * Borrowed heavily from the C_CAN driver originally written by:
1533 + * Copyright (C) 2007
1534 + * - Sascha Hauer, Marc Kleine-Budde, Pengutronix <s.hauer@pengutronix.de>
1535 + * - Simon Kallweit, intefo AG <simon.kallweit@intefo.ch>
1536 + *
1537 + * Bosch D_CAN controller is compliant to CAN protocol version 2.0 part A and B.
1538 + * Bosch D_CAN user manual can be obtained from:
1539 + * http://www.semiconductors.bosch.de/media/en/pdf/ipmodules_1/can/
1540 + * d_can_users_manual_111.pdf
1541 + *
1542 + * This program is free software; you can redistribute it and/or
1543 + * modify it under the terms of the GNU General Public License as
1544 + * published by the Free Software Foundation version 2.
1545 + *
1546 + * This program is distributed "as is" WITHOUT ANY WARRANTY of any
1547 + * kind, whether express or implied; without even the implied warranty
1548 + * of MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
1549 + * GNU General Public License for more details.
1550 + */
1551 +
1552 +/*
1553 + * Your platform definitions should specify module ram offsets and interrupt
1554 + * number to use as follows:
1555 + *
1556 + * static struct d_can_platform_data am33xx_evm_d_can_pdata = {
1557 + * .d_can_offset = 0,
1558 + * .d_can_ram_offset = 0x1000,
1559 + * .num_of_msg_objs = 64,
1560 + * .dma_support = true,
1561 + * .test_mode_enable = false,
1562 + * .parity_check = false,
1563 + * .version = 0x1,
1564 + * .hw_raminit = d_can_hw_raminit,
1565 + * };
1566 + *
1567 + * Please see include/linux/can/platform/d_can.h for description of
1568 + * above fields.
1569 + *
1570 + */
1571 +
1572 +#include <linux/kernel.h>
1573 +#include <linux/module.h>
1574 +#include <linux/interrupt.h>
1575 +#include <linux/delay.h>
1576 +#include <linux/netdevice.h>
1577 +#include <linux/if_arp.h>
1578 +#include <linux/if_ether.h>
1579 +#include <linux/list.h>
1580 +#include <linux/io.h>
1581 +#include <linux/platform_device.h>
1582 +#include <linux/can/platform/d_can.h>
1583 +#include <linux/clk.h>
1584 +#include <linux/slab.h>
1585 +#include <linux/can/dev.h>
1586 +
1587 +#include "d_can.h"
1588 +
1589 +#define D_CAN_CLK_NAME_LEN 40
1590 +
1591 +static int __devinit d_can_plat_probe(struct platform_device *pdev)
1592 +{
1593 + int ret = 0;
1594 + void __iomem *addr;
1595 + struct net_device *ndev;
1596 + struct d_can_priv *priv;
1597 + struct resource *mem;
1598 + struct d_can_platform_data *pdata;
1599 + char *clk_name;
1600 +
1601 + pdata = pdev->dev.platform_data;
1602 + if (!pdata) {
1603 + dev_err(&pdev->dev, "No platform data\n");
1604 + goto exit;
1605 + }
1606 +
1607 + /* allocate the d_can device */
1608 + ndev = alloc_d_can_dev(pdata->num_of_msg_objs);
1609 + if (!ndev) {
1610 + ret = -ENOMEM;
1611 + dev_err(&pdev->dev, "alloc_d_can_dev failed\n");
1612 + goto exit;
1613 + }
1614 +
1615 + clk_name = kzalloc(D_CAN_CLK_NAME_LEN + 1, GFP_KERNEL);
1616 + if (!clk_name)
1617 + goto exit;
1618 +
1619 + priv = netdev_priv(ndev);
1620 + clk_name = "dcan";
1621 + if (pdev->id == 0)
1622 + strcat(clk_name, "0_fck");
1623 + else
1624 + strcat(clk_name, "1_fck");
1625 + /* get the appropriate clk */
1626 + priv->fck = clk_get(&pdev->dev, clk_name);
1627 + if (IS_ERR(priv->fck)) {
1628 + dev_err(&pdev->dev, "%s is not found\n", clk_name);
1629 + ret = -ENODEV;
1630 + goto exit_free_ndev;
1631 + }
1632 + clk_enable(priv->fck);
1633 +
1634 + /* clk_name = D_CAN_DRV_NAME; */
1635 + clk_name = "dcan";
1636 + if (pdev->id == 0)
1637 + strcat(clk_name, "0_ick");
1638 + else
1639 + strcat(clk_name, "1_ick");
1640 + priv->ick = clk_get(&pdev->dev, clk_name);
1641 + if (IS_ERR(priv->ick)) {
1642 + dev_err(&pdev->dev, "%s is not found\n", clk_name);
1643 + ret = -ENODEV;
1644 + goto exit_free_fck;
1645 + }
1646 + clk_enable(priv->ick);
1647 +
1648 + /* get the platform data */
1649 + mem = platform_get_resource(pdev, IORESOURCE_MEM, 0);
1650 + if (!mem) {
1651 + ret = -ENODEV;
1652 + dev_err(&pdev->dev, "No mem resource\n");
1653 + goto exit_free_clks;
1654 + }
1655 +
1656 + if (!request_mem_region(mem->start, resource_size(mem),
1657 + D_CAN_DRV_NAME)) {
1658 + dev_err(&pdev->dev, "resource unavailable\n");
1659 + ret = -EBUSY;
1660 + goto exit_free_clks;
1661 + }
1662 +
1663 + addr = ioremap(mem->start, resource_size(mem));
1664 + if (!addr) {
1665 + dev_err(&pdev->dev, "ioremap failed\n");
1666 + ret = -ENOMEM;
1667 + goto exit_release_mem;
1668 + }
1669 +
1670 + /* IRQ specific to Error and status & can be used for Message Object */
1671 + ndev->irq = platform_get_irq_byname(pdev, "d_can_int0");
1672 + if (!ndev->irq) {
1673 + dev_err(&pdev->dev, "No irq0 resource\n");
1674 + goto exit_iounmap;
1675 + }
1676 +
1677 + /* IRQ specific for Message Object */
1678 + priv->irq_obj = platform_get_irq_byname(pdev, "d_can_int1");
1679 + if (!priv->irq_obj) {
1680 + dev_err(&pdev->dev, "No irq1 resource\n");
1681 + goto exit_iounmap;
1682 + }
1683 +
1684 + priv->base = addr;
1685 + priv->can.clock.freq = clk_get_rate(priv->fck);
1686 +
1687 + /* RAM init */
1688 + pdata->hw_raminit(pdev->id);
1689 +
1690 + priv->test_mode = pdata->test_mode_enable;
1691 +
1692 + platform_set_drvdata(pdev, ndev);
1693 + SET_NETDEV_DEV(ndev, &pdev->dev);
1694 +
1695 + ret = register_d_can_dev(ndev);
1696 + if (ret) {
1697 + dev_err(&pdev->dev, "registering %s failed (err=%d)\n",
1698 + D_CAN_DRV_NAME, ret);
1699 + goto exit_free_device;
1700 + }
1701 +
1702 + dev_info(&pdev->dev, "%s device registered (irq=%d, irq_obj=%d)\n",
1703 + D_CAN_DRV_NAME, ndev->irq, priv->irq_obj);
1704 +
1705 + return 0;
1706 +
1707 +exit_free_device:
1708 + platform_set_drvdata(pdev, NULL);
1709 +exit_iounmap:
1710 + iounmap(addr);
1711 +exit_release_mem:
1712 + release_mem_region(mem->start, resource_size(mem));
1713 +exit_free_clks:
1714 +#ifdef CONFIG_HAVE_CLK
1715 + clk_disable(priv->ick);
1716 + clk_put(priv->ick);
1717 +exit_free_fck:
1718 + clk_disable(priv->fck);
1719 + clk_put(priv->fck);
1720 +exit_free_ndev:
1721 + free_d_can_dev(ndev);
1722 +exit:
1723 +#endif
1724 + dev_err(&pdev->dev, "probe failed\n");
1725 +
1726 + return ret;
1727 +}
1728 +
1729 +static int __devexit d_can_plat_remove(struct platform_device *pdev)
1730 +{
1731 + struct net_device *ndev = platform_get_drvdata(pdev);
1732 + struct d_can_priv *priv = netdev_priv(ndev);
1733 + struct resource *mem;
1734 +
1735 + free_d_can_dev(ndev);
1736 + iounmap(priv->base);
1737 + mem = platform_get_resource(pdev, IORESOURCE_MEM, 0);
1738 + release_mem_region(mem->start, resource_size(mem));
1739 +#ifdef CONFIG_HAVE_CLK
1740 + clk_disable(priv->ick);
1741 + clk_disable(priv->fck);
1742 + clk_put(priv->ick);
1743 + clk_put(priv->fck);
1744 +#endif
1745 + unregister_d_can_dev(ndev);
1746 + platform_set_drvdata(pdev, NULL);
1747 +
1748 + return 0;
1749 +}
1750 +
1751 +static struct platform_driver d_can_plat_driver = {
1752 + .driver = {
1753 + .name = D_CAN_DRV_NAME,
1754 + .owner = THIS_MODULE,
1755 + },
1756 + .probe = d_can_plat_probe,
1757 + .remove = __devexit_p(d_can_plat_remove),
1758 +};
1759 +
1760 +static int __init d_can_plat_init(void)
1761 +{
1762 + printk(KERN_INFO D_CAN_DRV_DESC "\n");
1763 + return platform_driver_register(&d_can_plat_driver);
1764 +}
1765 +module_init(d_can_plat_init);
1766 +
1767 +static void __exit d_can_plat_exit(void)
1768 +{
1769 + printk(KERN_INFO D_CAN_DRV_DESC " unloaded\n");
1770 + platform_driver_unregister(&d_can_plat_driver);
1771 +}
1772 +module_exit(d_can_plat_exit);
1773 +
1774 +MODULE_AUTHOR("Anil Kumar Ch <anilkumar@ti.com>");
1775 +MODULE_LICENSE("GPL v2");
1776 +MODULE_VERSION(D_CAN_VERSION);
1777 +MODULE_DESCRIPTION(D_CAN_DRV_DESC);
1778 diff --git a/include/linux/can/platform/d_can.h b/include/linux/can/platform/d_can.h
1779 new file mode 100644
1780 index 0000000..b139e05
1781 --- /dev/null
1782 +++ b/include/linux/can/platform/d_can.h
1783 @@ -0,0 +1,53 @@
1784 +#ifndef __CAN_PLATFORM_TI_D_CAN_H__
1785 +#define __CAN_PLATFORM_TI_D_CAN_H__
1786 +
1787 +/*
1788 + * D_CAN controller driver platform header
1789 + *
1790 + * Copyright (C) 2011 Texas Instruments, Inc. - http://www.ti.com/
1791 + * Anil Kumar Ch <anilkumar@ti.com>
1792 + *
1793 + * Bosch D_CAN controller is compliant to CAN protocol version 2.0 part A and B.
1794 + * Bosch D_CAN user manual can be obtained from:
1795 + * http://www.semiconductors.bosch.de/media/en/pdf/ipmodules_1/can/
1796 + * d_can_users_manual_111.pdf
1797 + *
1798 + * This program is free software; you can redistribute it and/or
1799 + * modify it under the terms of the GNU General Public License as
1800 + * published by the Free Software Foundation version 2.
1801 + *
1802 + * This program is distributed "as is" WITHOUT ANY WARRANTY of any
1803 + * kind, whether express or implied; without even the implied warranty
1804 + * of MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
1805 + * GNU General Public License for more details.
1806 + */
1807 +
1808 +/**
1809 + * struct d_can_platform_data - DCAN Platform Data
1810 + *
1811 + * @d_can_offset: mostly 0 - should really never change
1812 + * @d_can_ram_offset: d_can RAM offset
1813 + * @msg_obj_offset: Mailbox RAM offset
1814 + * @num_of_msg_objs: Number of message objects
1815 + * @dma_support: DMA support is required/not
1816 + * test_mode_enable: Test mode enable bit
1817 + * @parity_check: Parity error checking is needed/not
1818 + * @version: version for future use
1819 + * @hw_raminit: platform specific callback fn for h/w ram init
1820 + *
1821 + * Platform data structure to get all platform specific settings.
1822 + * this structure also accounts the fact that the IP may have different
1823 + * RAM and mailbox offsets for different SOC's
1824 + */
1825 +struct d_can_platform_data {
1826 + u32 d_can_offset;
1827 + u32 d_can_ram_offset;
1828 + u32 msg_obj_offset;
1829 + u32 num_of_msg_objs;
1830 + bool dma_support;
1831 + bool test_mode_enable;
1832 + bool parity_check;
1833 + u32 version;
1834 + void (*hw_raminit) (unsigned int);
1835 +};
1836 +#endif
1837 --
1838 1.7.2.5