[glsdk/meta-ti-glsdk.git] / recipes-kernel / linux / linux-ti33x-psp-3.2 / 3.2.2 / 0056-UBIFS-make-debugging-messages-light-again.patch
1 From 400fba6cfdfd168d550113f665c3b168cf9214cf Mon Sep 17 00:00:00 2001
2 From: Artem Bityutskiy <artem.bityutskiy@linux.intel.com>
3 Date: Wed, 11 Jan 2012 15:13:27 +0200
4 Subject: [PATCH 056/129] UBIFS: make debugging messages light again
6 commit 1f5d78dc4823a85f112aaa2d0f17624f8c2a6c52 upstream.
8 We switch to dynamic debugging in commit
9 56e46742e846e4de167dde0e1e1071ace1c882a5 but did not take into account that
10 now we do not control anymore whether a specific message is enabled or not.
11 So now we lock the "dbg_lock" and release it in every debugging macro, which
12 make them not so light-weight.
14 This commit removes the "dbg_lock" protection from the debugging macros to
15 fix the issue.
17 The downside is that now our DBGKEY() stuff is broken, but this is not
18 critical at all and will be fixed later.
20 Signed-off-by: Artem Bityutskiy <artem.bityutskiy@linux.intel.com>
21 Signed-off-by: Greg Kroah-Hartman <gregkh@suse.de>
22 ---
23 fs/ubifs/debug.h | 12 +++++-------
24 1 file changed, 5 insertions(+), 7 deletions(-)
26 diff --git a/fs/ubifs/debug.h b/fs/ubifs/debug.h
27 index 3f65829..c9d2941 100644
28 --- a/fs/ubifs/debug.h
29 +++ b/fs/ubifs/debug.h
30 @@ -175,19 +175,17 @@ const char *dbg_key_str1(const struct ubifs_info *c,
31 const union ubifs_key *key);
33 /*
34 - * DBGKEY macros require @dbg_lock to be held, which it is in the dbg message
35 - * macros.
36 + * TODO: these macros are now broken because there is no locking around them
37 + * and we use a global buffer for the key string. This means that in case of
38 + * concurrent execution we will end up with incorrect and messy key strings.
39 */
40 #define DBGKEY(key) dbg_key_str0(c, (key))
41 #define DBGKEY1(key) dbg_key_str1(c, (key))
43 extern spinlock_t dbg_lock;
45 -#define ubifs_dbg_msg(type, fmt, ...) do { \
46 - spin_lock(&dbg_lock); \
47 - pr_debug("UBIFS DBG " type ": " fmt "\n", ##__VA_ARGS__); \
48 - spin_unlock(&dbg_lock); \
49 -} while (0)
50 +#define ubifs_dbg_msg(type, fmt, ...) \
51 + pr_debug("UBIFS DBG " type ": " fmt "\n", ##__VA_ARGS__)
53 /* Just a debugging messages not related to any specific UBIFS subsystem */
54 #define dbg_msg(fmt, ...) \
55 --
56 1.7.9.5