[glsdk/meta-ti-glsdk.git] / recipes-kernel / linux / linux-ti33x-psp-3.2 / 3.2.24 / 0046-block-fix-infinite-loop-in-__getblk_slow.patch
1 From 898f4d272514d19aafee8cd66b796c0553fca080 Mon Sep 17 00:00:00 2001
2 From: Jeff Moyer <jmoyer@redhat.com>
3 Date: Thu, 12 Jul 2012 09:43:14 -0400
4 Subject: [PATCH 046/109] block: fix infinite loop in __getblk_slow
6 commit 91f68c89d8f35fe98ea04159b9a3b42d0149478f upstream.
8 Commit 080399aaaf35 ("block: don't mark buffers beyond end of disk as
9 mapped") exposed a bug in __getblk_slow that causes mount to hang as it
10 loops infinitely waiting for a buffer that lies beyond the end of the
11 disk to become uptodate.
13 The problem was initially reported by Torsten Hilbrich here:
15 https://lkml.org/lkml/2012/6/18/54
17 and also reported independently here:
19 http://www.sysresccd.org/forums/viewtopic.php?f=13&t=4511
21 and then Richard W.M. Jones and Marcos Mello noted a few separate
22 bugzillas also associated with the same issue. This patch has been
23 confirmed to fix:
25 https://bugzilla.redhat.com/show_bug.cgi?id=835019
27 The main problem is here, in __getblk_slow:
29 for (;;) {
30 struct buffer_head * bh;
31 int ret;
33 bh = __find_get_block(bdev, block, size);
34 if (bh)
35 return bh;
37 ret = grow_buffers(bdev, block, size);
38 if (ret < 0)
39 return NULL;
40 if (ret == 0)
41 free_more_memory();
42 }
44 __find_get_block does not find the block, since it will not be marked as
45 mapped, and so grow_buffers is called to fill in the buffers for the
46 associated page. I believe the for (;;) loop is there primarily to
47 retry in the case of memory pressure keeping grow_buffers from
48 succeeding. However, we also continue to loop for other cases, like the
49 block lying beond the end of the disk. So, the fix I came up with is to
50 only loop when grow_buffers fails due to memory allocation issues
51 (return value of 0).
53 The attached patch was tested by myself, Torsten, and Rich, and was
54 found to resolve the problem in call cases.
56 Signed-off-by: Jeff Moyer <jmoyer@redhat.com>
57 Reported-and-Tested-by: Torsten Hilbrich <torsten.hilbrich@secunet.com>
58 Tested-by: Richard W.M. Jones <rjones@redhat.com>
59 Reviewed-by: Josh Boyer <jwboyer@redhat.com>
60 [ Jens is on vacation, taking this directly - Linus ]
61 --
62 Stable Notes: this patch requires backport to 3.0, 3.2 and 3.3.
63 Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
64 Signed-off-by: Ben Hutchings <ben@decadent.org.uk>
65 ---
66 fs/buffer.c | 22 +++++++++++++---------
67 1 files changed, 13 insertions(+), 9 deletions(-)
69 diff --git a/fs/buffer.c b/fs/buffer.c
70 index c807931..4115eca 100644
71 --- a/fs/buffer.c
72 +++ b/fs/buffer.c
73 @@ -1087,6 +1087,9 @@ grow_buffers(struct block_device *bdev, sector_t block, int size)
74 static struct buffer_head *
75 __getblk_slow(struct block_device *bdev, sector_t block, int size)
76 {
77 + int ret;
78 + struct buffer_head *bh;
79 +
80 /* Size must be multiple of hard sectorsize */
81 if (unlikely(size & (bdev_logical_block_size(bdev)-1) ||
82 (size < 512 || size > PAGE_SIZE))) {
83 @@ -1099,20 +1102,21 @@ __getblk_slow(struct block_device *bdev, sector_t block, int size)
84 return NULL;
85 }
87 - for (;;) {
88 - struct buffer_head * bh;
89 - int ret;
90 +retry:
91 + bh = __find_get_block(bdev, block, size);
92 + if (bh)
93 + return bh;
95 + ret = grow_buffers(bdev, block, size);
96 + if (ret == 0) {
97 + free_more_memory();
98 + goto retry;
99 + } else if (ret > 0) {
100 bh = __find_get_block(bdev, block, size);
101 if (bh)
102 return bh;
103 -
104 - ret = grow_buffers(bdev, block, size);
105 - if (ret < 0)
106 - return NULL;
107 - if (ret == 0)
108 - free_more_memory();
109 }
110 + return NULL;
111 }
113 /*
114 --
115 1.7.7.6