[glsdk/meta-ti-glsdk.git] / recipes-kernel / linux / linux-ti33x-psp-3.2 / 3.2.24 / 0067-UBIFS-fix-a-bug-in-empty-space-fix-up.patch
1 From f6ba94c29333fa6df9b3b553415e93bafbd3c831 Mon Sep 17 00:00:00 2001
2 From: Artem Bityutskiy <Artem.Bityutskiy@linux.intel.com>
3 Date: Sat, 14 Jul 2012 14:33:09 +0300
4 Subject: [PATCH 067/109] UBIFS: fix a bug in empty space fix-up
6 commit c6727932cfdb13501108b16c38463c09d5ec7a74 upstream.
8 UBIFS has a feature called "empty space fix-up" which is a quirk to work-around
9 limitations of dumb flasher programs. Namely, of those flashers that are unable
10 to skip NAND pages full of 0xFFs while flashing, resulting in empty space at
11 the end of half-filled eraseblocks to be unusable for UBIFS. This feature is
12 relatively new (introduced in v3.0).
14 The fix-up routine (fixup_free_space()) is executed only once at the very first
15 mount if the superblock has the 'space_fixup' flag set (can be done with -F
16 option of mkfs.ubifs). It basically reads all the UBIFS data and metadata and
17 writes it back to the same LEB. The routine assumes the image is pristine and
18 does not have anything in the journal.
20 There was a bug in 'fixup_free_space()' where it fixed up the log incorrectly.
21 All but one LEB of the log of a pristine file-system are empty. And one
22 contains just a commit start node. And 'fixup_free_space()' just unmapped this
23 LEB, which resulted in wiping the commit start node. As a result, some users
24 were unable to mount the file-system next time with the following symptom:
26 UBIFS error (pid 1): replay_log_leb: first log node at LEB 3:0 is not CS node
27 UBIFS error (pid 1): replay_log_leb: log error detected while replaying the log at LEB 3:0
29 The root-cause of this bug was that 'fixup_free_space()' wrongly assumed
30 that the beginning of empty space in the log head (c->lhead_offs) was known
31 on mount. However, it is not the case - it was always 0. UBIFS does not store
32 in it the master node and finds out by scanning the log on every mount.
34 The fix is simple - just pass commit start node size instead of 0 to
35 'fixup_leb()'.
37 Signed-off-by: Artem Bityutskiy <Artem.Bityutskiy@linux.intel.com>
38 Reported-by: Iwo Mergler <Iwo.Mergler@netcommwireless.com>
39 Tested-by: Iwo Mergler <Iwo.Mergler@netcommwireless.com>
40 Reported-by: James Nute <newten82@gmail.com>
41 Signed-off-by: Ben Hutchings <ben@decadent.org.uk>
42 ---
43 fs/ubifs/sb.c | 8 ++++++--
44 1 files changed, 6 insertions(+), 2 deletions(-)
46 diff --git a/fs/ubifs/sb.c b/fs/ubifs/sb.c
47 index 6094c5a..b73ecd8 100644
48 --- a/fs/ubifs/sb.c
49 +++ b/fs/ubifs/sb.c
50 @@ -715,8 +715,12 @@ static int fixup_free_space(struct ubifs_info *c)
51 lnum = ubifs_next_log_lnum(c, lnum);
52 }
54 - /* Fixup the current log head */
55 - err = fixup_leb(c, c->lhead_lnum, c->lhead_offs);
56 + /*
57 + * Fixup the log head which contains the only a CS node at the
58 + * beginning.
59 + */
60 + err = fixup_leb(c, c->lhead_lnum,
61 + ALIGN(UBIFS_CS_NODE_SZ, c->min_io_size));
62 if (err)
63 goto out;
65 --
66 1.7.7.6