[glsdk/meta-ti-glsdk.git] / recipes-kernel / linux / linux-ti33x-psp-3.2 / 3.2.6 / 0029-PM-Hibernate-Fix-s2disk-regression-related-to-freezi.patch
1 From d483054fe4c66eeb7a03fdc97519b07edb1dc803 Mon Sep 17 00:00:00 2001
2 From: "Rafael J. Wysocki" <rjw@sisk.pl>
3 Date: Sun, 29 Jan 2012 20:35:52 +0100
4 Subject: [PATCH 29/87] PM / Hibernate: Fix s2disk regression related to
5 freezing workqueues
7 commit 181e9bdef37bfcaa41f3ab6c948a2a0d60a268b5 upstream.
9 Commit 2aede851ddf08666f68ffc17be446420e9d2a056
11 PM / Hibernate: Freeze kernel threads after preallocating memory
13 introduced a mechanism by which kernel threads were frozen after
14 the preallocation of hibernate image memory to avoid problems with
15 frozen kernel threads not responding to memory freeing requests.
16 However, it overlooked the s2disk code path in which the
17 SNAPSHOT_CREATE_IMAGE ioctl was run directly after SNAPSHOT_FREE,
18 which caused freeze_workqueues_begin() to BUG(), because it saw
19 that worqueues had been already frozen.
21 Although in principle this issue might be addressed by removing
22 the relevant BUG_ON() from freeze_workqueues_begin(), that would
23 reintroduce the very problem that commit 2aede851ddf08666f68ffc17be4
24 attempted to avoid into that particular code path. For this reason,
25 to fix the issue at hand, introduce thaw_kernel_threads() and make
26 the SNAPSHOT_FREE ioctl execute it.
28 Special thanks to Srivatsa S. Bhat for detailed analysis of the
29 problem.
31 Reported-and-tested-by: Jiri Slaby <jslaby@suse.cz>
32 Signed-off-by: Rafael J. Wysocki <rjw@sisk.pl>
33 Acked-by: Srivatsa S. Bhat <srivatsa.bhat@linux.vnet.ibm.com>
34 Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
35 ---
36 include/linux/freezer.h | 2 ++
37 kernel/power/process.c | 9 +++++++++
38 kernel/power/user.c | 9 +++++++++
39 3 files changed, 20 insertions(+), 0 deletions(-)
41 diff --git a/include/linux/freezer.h b/include/linux/freezer.h
42 index a5386e3..b5d6b6a 100644
43 --- a/include/linux/freezer.h
44 +++ b/include/linux/freezer.h
45 @@ -51,6 +51,7 @@ extern void refrigerator(void);
46 extern int freeze_processes(void);
47 extern int freeze_kernel_threads(void);
48 extern void thaw_processes(void);
49 +extern void thaw_kernel_threads(void);
51 static inline int try_to_freeze(void)
52 {
53 @@ -185,6 +186,7 @@ static inline void refrigerator(void) {}
54 static inline int freeze_processes(void) { return -ENOSYS; }
55 static inline int freeze_kernel_threads(void) { return -ENOSYS; }
56 static inline void thaw_processes(void) {}
57 +static inline void thaw_kernel_threads(void) {}
59 static inline int try_to_freeze(void) { return 0; }
61 diff --git a/kernel/power/process.c b/kernel/power/process.c
62 index addbbe5..3d4b954 100644
63 --- a/kernel/power/process.c
64 +++ b/kernel/power/process.c
65 @@ -203,3 +203,12 @@ void thaw_processes(void)
66 printk("done.\n");
67 }
69 +void thaw_kernel_threads(void)
70 +{
71 + printk("Restarting kernel threads ... ");
72 + thaw_workqueues();
73 + thaw_tasks(true);
74 + schedule();
75 + printk("done.\n");
76 +}
77 +
78 diff --git a/kernel/power/user.c b/kernel/power/user.c
79 index 6d8f535..3565b15 100644
80 --- a/kernel/power/user.c
81 +++ b/kernel/power/user.c
82 @@ -303,6 +303,15 @@ static long snapshot_ioctl(struct file *filp, unsigned int cmd,
83 swsusp_free();
84 memset(&data->handle, 0, sizeof(struct snapshot_handle));
85 data->ready = 0;
86 + /*
87 + * It is necessary to thaw kernel threads here, because
88 + * SNAPSHOT_CREATE_IMAGE may be invoked directly after
89 + * SNAPSHOT_FREE. In that case, if kernel threads were not
90 + * thawed, the preallocation of memory carried out by
91 + * hibernation_snapshot() might run into problems (i.e. it
92 + * might fail or even deadlock).
93 + */
94 + thaw_kernel_threads();
95 break;
97 case SNAPSHOT_SET_IMAGE_SIZE:
98 --
99 1.7.7.4