1 # This .inc file allows you to build and deploy multiple sets of kernel + modules with different defconfigs
2 #
3 # Note that this include will NOT stage anything nor create packages, since that is virtually impossible
4 # Userspace should be built against the 'regular' kernel
5 #
6 # The intended usecase is for machines that have mutually exclusive drivers due to e.g. pinmuxing issues.
7 # For example the LogicPD omap-l138 experimenter board can have multiple mutually exclusive expansion boards
8 # like lcd, ethernet, sound, 20x2 character LCD, etc. To be able to easily test all of those you can use this .inc
9 #
10 # To make it easier finding the original defconfig from a running kernel, this also forcefully turns on
11 # CONFIG_IKCONFIG_PROC so people can do 'zcat /proc/config.gz' on the target.
13 require linux.inc
15 SRC_URI += " \
16 file://configs/* "
18 MULTI_CONFIG_BASE_SUFFIX = "multi-config-"
20 do_compileconfigs () {
22 # fixup for fetcher change
23 if [ -e ${WORKDIR}/configs/configs ] ; then
24 if [ -e ${WORKDIR}/configs/configs/.empty ] ; then
25 mv ${WORKDIR}/configs/configs/.empty ${WORKDIR}/configs/
26 fi
27 mv ${WORKDIR}/configs/configs/* ${WORKDIR}/configs/
28 rm -rf ${WORKDIR}/configs/configs
29 fi
31 # Compile and Install additional kernel configs if found
32 if [ -e ${WORKDIR}/configs/.empty ] ; then
33 echo "No configs found in configs/ directory, skipping to regular build"
34 else
35 echo "Multiple configs found, building those first"
37 # Context Save the regular 'defconfig'
38 cp ${WORKDIR}/defconfig ${WORKDIR}/defconfig.save
40 for config in ${WORKDIR}/configs/* ; do
42 # Copy in alternative config
43 cd ${S}
44 cp $config ${WORKDIR}/defconfig
46 # Enable config to be viewed on the target
47 echo "CONFIG_IKCONFIG=y" >> ${WORKDIR}/defconfig
48 echo "CONFIG_IKCONFIG_PROC=y" >> ${WORKDIR}/defconfig
50 # Build and Install this alternative kernel
51 do_configure
52 kernel_do_compile
53 do_compile_kernelmodules
54 kernel_do_install
56 # Drop the resulting images in the deploy dir
57 install -d ${DEPLOY_DIR_IMAGE}
58 install -m 0644 ${KERNEL_OUTPUT} ${DEPLOY_DIR_IMAGE}/${KERNEL_IMAGE_BASE_NAME}.${MULTI_CONFIG_BASE_SUFFIX}$(basename $config).bin
60 if [ -d "${D}/lib" ]; then
61 tar --owner=root --group=root -cvzf ${DEPLOY_DIR_IMAGE}/${MODULES_IMAGE_BASE_NAME}.${MULTI_CONFIG_BASE_SUFFIX}$(basename $config).tgz -C ${D} lib
62 fi
64 # Install the final config alongside the images
65 cp .config ${DEPLOY_DIR_IMAGE}/config-${PV}-${PR}-${MACHINE}.${MULTI_CONFIG_BASE_SUFFIX}$(basename $config).config
67 # Create symlinks
68 cd ${DEPLOY_DIR_IMAGE}
69 rm -f ${KERNEL_IMAGE_SYMLINK_NAME}.${MULTI_CONFIG_BASE_SUFFIX}$(basename $config).bin
70 ln -sf ${KERNEL_IMAGE_BASE_NAME}.${MULTI_CONFIG_BASE_SUFFIX}$(basename $config).bin ${KERNEL_IMAGE_SYMLINK_NAME}.${MULTI_CONFIG_BASE_SUFFIX}$(basename $config).bin
71 rm -f modules-${MACHINE}.${MULTI_CONFIG_BASE_SUFFIX}$(basename $config).tgz
72 ln -sf ${MODULES_IMAGE_BASE_NAME}.${MULTI_CONFIG_BASE_SUFFIX}$(basename $config).tgz modules-${MACHINE}.${MULTI_CONFIG_BASE_SUFFIX}$(basename $config).tgz
73 rm -f config-${MACHINE}.${MULTI_CONFIG_BASE_SUFFIX}$(basename $config).config
74 ln -sf config-${PV}-${PR}-${MACHINE}.${MULTI_CONFIG_BASE_SUFFIX}$(basename $config).config config-${MACHINE}.${MULTI_CONFIG_BASE_SUFFIX}$(basename $config).config
76 done
78 # Restore the regular 'defconfig'
79 cp ${WORKDIR}/defconfig.save ${WORKDIR}/defconfig
80 fi
81 }
83 # For reference, copy .config to deploy image
84 do_deploy_append () {
86 install -d ${DEPLOY_DIR_IMAGE}
88 # Drop the regular defconfig along side the others for consistency
89 cd ${S}
90 cp .config ${DEPLOY_DIR_IMAGE}/config-${PV}-${PR}-${MACHINE}.config
92 # add symlink
93 cd ${DEPLOY_DIR_IMAGE}
94 rm -f config-${MACHINE}.config
95 ln -s config-${PV}-${PR}-${MACHINE}.config config-${MACHINE}.config
97 rm -f modules-${MACHINE}.tgz
98 ln -sf ${MODULES_IMAGE_BASE_NAME}.tgz modules-${MACHINE}.tgz
100 }
102 do_compileconfigs[depends] += "u-boot-mkimage-native:do_populate_sysroot virtual/${TARGET_PREFIX}gcc:do_populate_sysroot virtual/${TARGET_PREFIX}gcc${KERNEL_CCSUFFIX}:do_populate_sysroot"
103 addtask compileconfigs after do_patch before do_configure