]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/meta-ti-glsdk.git/blob - recipes-kernel/linux/multi-kernel.inc
multi-kernel: match oe-core for MODULE_IMAGE_BASE_NAME, set it conditionally
[glsdk/meta-ti-glsdk.git] / recipes-kernel / linux / multi-kernel.inc
1 # This .inc file allows building and deploying multiple sets of kernel + modules
2 # with different defconfigs
3 #
4 # Note that this include will NOT stage anything nor create packages, since that
5 # is virtually impossible. Userspace should be built against the 'regular' kernel
6 #
7 # The intended usecase is for machines that have mutually exclusive drivers due
8 # to e.g. pinmuxing issues. For example the LogicPD omap-l138 experimenter board
9 # can have multiple mutually exclusive expansion boards like lcd, ethernet,
10 # sound, 20x2 character LCD, etc. To be able to easily test all of those you can
11 # use this .inc
12 #
13 # To make it easier finding the original defconfig from a running kernel, this
14 # also forcefully turns on CONFIG_IKCONFIG_PROC so people can do
15 # 'zcat /proc/config.gz' on the target.
16 #
17 # The function get_kernelversion uses generated header files to extract the
18 # version number. But those files are not available until do_compile, and
19 # do_compileconfigs is injected before that, hence the version becomes None
20 # and breaks in several places. Introduce a task do_preparekernel that calls
21 # "make prepare" in the kernel tree to generate all the necessary files.
23 require linux.inc
25 SRC_URI += " \
26            file://configs "
28 MULTI_CONFIG_BASE_SUFFIX = "multi-config-"
29 MODULE_IMAGE_BASE_NAME ?= "modules-${PE}-${PV}-${PR}-${MACHINE}-${DATETIME}"
31 do_preparekernel () {
32         unset CFLAGS CPPFLAGS CXXFLAGS LDFLAGS MACHINE
33         oe_runmake prepare CC="${KERNEL_CC}" LD="${KERNEL_LD}"
34 }
36 addtask preparekernel after do_configure before do_compile
38 do_compileconfigs () {
40   # fixup for fetcher change
41   if [ -e ${WORKDIR}/configs/configs ] ; then
42       if [ -e ${WORKDIR}/configs/configs/empty ] ; then
43           mv ${WORKDIR}/configs/configs/empty ${WORKDIR}/configs/
44       fi
45       mv ${WORKDIR}/configs/configs/* ${WORKDIR}/configs/
46       rm -rf ${WORKDIR}/configs/configs
47   fi
49   # Compile and Install additional kernel configs if found
50   if [ -e ${WORKDIR}/configs/empty ] ; then
51        echo "No configs found in configs/ directory, skipping to regular build"
52   else
53       echo "Multiple configs found, building those first"
55       # Context Save the regular 'defconfig'
56       cp ${WORKDIR}/defconfig ${WORKDIR}/defconfig.save
58       for config in ${WORKDIR}/configs/* ; do
60         # Copy in alternative config
61         cd ${S}
62         cp $config ${WORKDIR}/defconfig
64         # Enable config to be viewed on the target
65         echo "CONFIG_IKCONFIG=y" >> ${WORKDIR}/defconfig
66         echo "CONFIG_IKCONFIG_PROC=y" >> ${WORKDIR}/defconfig
67         
68         # Build and Install this alternative kernel
69         do_configure
70         kernel_do_compile
71         do_compile_kernelmodules
72         kernel_do_install
74         # Drop the resulting images in the deploy dir
75         install -d ${DEPLOY_DIR_IMAGE}
76         install -m 0644 ${KERNEL_OUTPUT} ${DEPLOY_DIR_IMAGE}/${KERNEL_IMAGE_BASE_NAME}.${MULTI_CONFIG_BASE_SUFFIX}$(basename $config).bin
78         if [ -d "${D}/lib" ]; then
79             tar --owner=root --group=root -cvzf ${DEPLOY_DIR_IMAGE}/${MODULE_IMAGE_BASE_NAME}.${MULTI_CONFIG_BASE_SUFFIX}$(basename $config).tgz -C ${D} lib
80         fi
81  
82         # Install the final config alongside the images
83         cp .config ${DEPLOY_DIR_IMAGE}/config-${PV}-${PR}-${MACHINE}.${MULTI_CONFIG_BASE_SUFFIX}$(basename $config).config
85         # Create symlinks
86         cd ${DEPLOY_DIR_IMAGE}
87         rm -f ${KERNEL_IMAGE_SYMLINK_NAME}.${MULTI_CONFIG_BASE_SUFFIX}$(basename $config).bin
88         ln -sf ${KERNEL_IMAGE_BASE_NAME}.${MULTI_CONFIG_BASE_SUFFIX}$(basename $config).bin ${KERNEL_IMAGE_SYMLINK_NAME}.${MULTI_CONFIG_BASE_SUFFIX}$(basename $config).bin
89         rm -f modules-${MACHINE}.${MULTI_CONFIG_BASE_SUFFIX}$(basename $config).tgz
90         ln -sf ${MODULE_IMAGE_BASE_NAME}.${MULTI_CONFIG_BASE_SUFFIX}$(basename $config).tgz modules-${MACHINE}.${MULTI_CONFIG_BASE_SUFFIX}$(basename $config).tgz
91         rm -f config-${MACHINE}.${MULTI_CONFIG_BASE_SUFFIX}$(basename $config).config
92         ln -sf config-${PV}-${PR}-${MACHINE}.${MULTI_CONFIG_BASE_SUFFIX}$(basename $config).config config-${MACHINE}.${MULTI_CONFIG_BASE_SUFFIX}$(basename $config).config
94       done
96       # Restore the regular 'defconfig'
97       cp ${WORKDIR}/defconfig.save ${WORKDIR}/defconfig
98       cd ${S}
99       do_configure
100     fi
103 # For reference, copy .config to deploy image
104 do_deploy_append () {
106         install -d ${DEPLOY_DIR_IMAGE}
108     # Drop the regular defconfig along side the others for consistency
109     cd ${S}
110     cp .config ${DEPLOY_DIR_IMAGE}/config-${PV}-${PR}-${MACHINE}.config
112     # add symlink
113     cd ${DEPLOY_DIR_IMAGE}    
114     rm -f config-${MACHINE}.config
115     ln -s config-${PV}-${PR}-${MACHINE}.config config-${MACHINE}.config
117     rm -f modules-${MACHINE}.tgz
118     ln -sf ${MODULE_IMAGE_BASE_NAME}.tgz modules-${MACHINE}.tgz
122 do_compileconfigs[depends] += "u-boot-mkimage-native:do_populate_sysroot virtual/${TARGET_PREFIX}gcc:do_populate_sysroot"
123 addtask compileconfigs after do_preparekernel before do_compile