]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/meta-ti-glsdk.git/blob - recipes-ti/gstreamer-ti/gstreamer-ti/0006-Remove-the-repeat_with_refresh-feature.patch
recipes-kernel: Add GLSDK specific kernel tree for omap-a15
[glsdk/meta-ti-glsdk.git] / recipes-ti / gstreamer-ti / gstreamer-ti / 0006-Remove-the-repeat_with_refresh-feature.patch
1 From c1205a792fd519cdebc32c00a5f604ccd78d3eac Mon Sep 17 00:00:00 2001
2 From: Don Darling <don.osc2@gmail.com>
3 Date: Thu, 26 Aug 2010 18:30:13 -0500
4 Subject: [PATCH 6/8] Remove the "repeat_with_refresh" feature.
6 No platforms are using it any longer.
7 ---
8  .../ticodecplugin/src/gsttidmaivideosink.c         |   67 +-------------------
9  .../ticodecplugin/src/gsttidmaivideosink.h         |    1 -
10  2 files changed, 1 insertions(+), 67 deletions(-)
12 diff --git a/gstreamer_ti/ti_build/ticodecplugin/src/gsttidmaivideosink.c b/gstreamer_ti/ti_build/ticodecplugin/src/gsttidmaivideosink.c
13 index 3615bfd..0125ed2 100644
14 --- a/gstreamer_ti/ti_build/ticodecplugin/src/gsttidmaivideosink.c
15 +++ b/gstreamer_ti/ti_build/ticodecplugin/src/gsttidmaivideosink.c
16 @@ -170,8 +170,6 @@ static gboolean
17   gst_tidmaivideosink_event(GstBaseSink * bsink, GstEvent * event);
18  static void 
19      gst_tidmaivideosink_init_env(GstTIDmaiVideoSink *sink);
20 -static int
21 -    gst_tidmaivideosink_videostd_get_refresh_latency(VideoStd_Type videoStd);
22  static gboolean
23      gst_tidmaivideosink_alloc_display_buffers(GstTIDmaiVideoSink * sink,
24          Int32 bufSize);
25 @@ -441,7 +439,6 @@ static void gst_tidmaivideosink_init(GstTIDmaiVideoSink * dmaisink,
26      dmaisink->videoOutput               = NULL;
27      dmaisink->numBufs                   = -1;
28      dmaisink->framerepeat               = 0;
29 -    dmaisink->repeat_with_refresh       = FALSE;
30      dmaisink->can_set_display_framerate = FALSE;
31      dmaisink->rotation                  = -1;
32      dmaisink->tempDmaiBuf               = NULL;
33 @@ -755,55 +752,6 @@ static int gst_tidmaivideosink_videostd_get_attrs(VideoStd_Type videoStd,
34  
35  
36  /*******************************************************************************
37 - * gst_tidmaivideosink_videostd_get_refresh_latency
38 - *
39 - *    Return the refresh latency in us for the given display standard.
40 -*******************************************************************************/
41 -static int gst_tidmaivideosink_videostd_get_refresh_latency(
42 -               VideoStd_Type videoStd)
43 -{
44 -    switch (videoStd) {
45 -        case VideoStd_1080P_24:
46 -            return 41667;
47 -
48 -        case VideoStd_SIF_PAL:
49 -        case VideoStd_D1_PAL:
50 -        case VideoStd_1080P_25:
51 -        case VideoStd_1080I_25:
52 -            return 40000;
53 -
54 -        case VideoStd_CIF:
55 -        case VideoStd_SIF_NTSC:
56 -        case VideoStd_D1_NTSC:
57 -            return 33367;
58 -            
59 -        case VideoStd_1080I_30:
60 -        case VideoStd_1080P_30:
61 -            return 33333;
62 -
63 -        case VideoStd_576P:
64 -        case VideoStd_720P_50:
65 -            return 20000;
66 -
67 -        case VideoStd_480P:
68 -        case VideoStd_720P_60:
69 -        #if defined(Platform_dm6467t)
70 -        case VideoStd_1080P_60:
71 -        #endif
72 -            return 16667;
73 -
74 -        case VideoStd_VGA:
75 -            return 16667;
76 -
77 -        default:
78 -            break;
79 -    }
80 -    GST_ERROR("Unknown videoStd entered (VideoStd = %d)\n", videoStd);
81 -    return 0;
82 -}
83 -
84 -
85 -/*******************************************************************************
86   * gst_tidmaivideosink_find_videostd
87   *
88   *    This function will take in a VideoStd_Attrs structure and find the
89 @@ -1580,10 +1528,7 @@ static GstFlowReturn gst_tidmaivideosink_render(GstBaseSink * bsink,
90  
91      /* Display the frame as many times as specified by framerepeat.  By
92       * default, the input buffer is copied to a display buffer for each time
93 -     * it is to be repeated.  However, if repeat_with_refresh is TRUE, then
94 -     * the platform doesn't have the bandwidth for multiple copies.  In this
95 -     * case we copy and display the input buffer only once, but let it refresh
96 -     * multiple times.
97 +     * it is to be repeated.  
98       */
99      for (i = 0; i < sink->framerepeat; i++) {
100  
101 @@ -1594,16 +1539,6 @@ static GstFlowReturn gst_tidmaivideosink_render(GstBaseSink * bsink,
102              goto cleanup;
103          }
104  
105 -        /* If repeat_with_refresh was specified, wait for the display to
106 -         * refresh framerepeat-1 times to make sure it has finished displaying
107 -         * this buffer before we write new data into it.
108 -         */
109 -        while (sink->repeat_with_refresh && i < (sink->framerepeat-1)) {
110 -            usleep(gst_tidmaivideosink_videostd_get_refresh_latency(
111 -                sink->dAttrs.videoStd) + 1);
112 -            i++;
113 -        }
115          /* Retrieve the dimensions of the display buffer */
116          BufferGfx_getDimensions(hDispBuf, &dim);
117          GST_LOG("Display size %dx%d pitch %d\n",
118 diff --git a/gstreamer_ti/ti_build/ticodecplugin/src/gsttidmaivideosink.h b/gstreamer_ti/ti_build/ticodecplugin/src/gsttidmaivideosink.h
119 index 4800fcd..2a28e4f 100644
120 --- a/gstreamer_ti/ti_build/ticodecplugin/src/gsttidmaivideosink.h
121 +++ b/gstreamer_ti/ti_build/ticodecplugin/src/gsttidmaivideosink.h
122 @@ -123,7 +123,6 @@ struct _GstTIDmaiVideoSink {
123     * should be repeated to match the display output frame rate.
124     */
125    int           framerepeat;
126 -  gboolean      repeat_with_refresh;
127    gboolean      can_set_display_framerate;
128    gboolean      signal_handoffs;
129  
130 -- 
131 1.7.0.4