linux-ti33x-psp 3.2: add support for Towertech TT3201 CAN cape
[glsdk/meta-ti-glsdk.git] / recipes-ti / includes / ti-eula-unpack.inc
1 # This file defines function used for unpacking the .bin file downloaded over
2 # the http and display EULA.
3 #  BINFILE - name of the install jammer .bin file
4 #  TARFILE - name of the tar file inside the install jammer
5 #  TI_BIN_UNPK_CMDS   - contains list of commands separated with colon to be 
6 #                       passed while unpacking the bin file. The keyword 
7 #                       workdir expands to WORKDIR and commands are appendded
8 #                       with '\n'. Eg. TI_BIN_UNPK_CMDS="Y:Y: qY:workdir"
9 #  TI_BIN_UNPK_WDEXT  - This variable extends workdir path, if user wants to put
10 #                       the output in some internal directory
12 python do_unpack () {
13     bb.build.exec_func('base_do_unpack', d)
14     bb.build.exec_func('ti_bin_do_unpack', d)
15 }
17 TI_BIN_UNPK_WDEXT += ""
18 python ti_bin_do_unpack() {
20     import os
22     localdata = bb.data.createCopy(d)
23     bb.data.update_data(localdata)
25     binfile  = bb.data.getVar('BINFILE', localdata)
26     binfile  = bb.data.expand(binfile, localdata)
28     # Change to the working directory
29     save_cwd = os.getcwd()
30     workdir  = bb.data.getVar('WORKDIR', localdata)
31     workdir  = bb.data.expand(workdir, localdata)
32     os.chdir(workdir)
34     # Get unpack commands
35     cmd_string = bb.data.getVar('TI_BIN_UNPK_CMDS', localdata)
36     cmd_list = cmd_string.split( ":" )
38     # Make the InstallJammer binary executable so we can run it
39     os.chmod(binfile, 0755)
41     # Run the InstallJammer binary and accept the EULA
42     filename = "HOME=%s ./%s --mode console" % (workdir, binfile)
43     
44     # Test executable by printing installer version or help screen (--version currently broken for some installers) 
45     # - this is currently broken in some IJ installers - comment out for now
46     #if os.system(filename + " --version") != 0:
47     #   print "ERROR: ti-eula-unpack: failed to execute binary installer"
48     #   raise bb.build.FuncFailed()
49  
50     f = os.popen(filename,'w')
51     for cmd in cmd_list:
52         if cmd == "workdir":
53             wdext = bb.data.getVar('TI_BIN_UNPK_WDEXT', localdata)
54             wdext = bb.data.expand(wdext, localdata)
55             cmd = workdir+wdext
56         print >>f, "%s\n" % cmd
57     f.close()
59     # Expand the tarball that was created if required
60     tarfile  = bb.data.getVar('TARFILE', localdata)    
61     if bool(tarfile) == True:
62         tarfile  = bb.data.expand(tarfile, localdata)
63         tcmd = 'tar x --no-same-owner -f %s -C %s' % (tarfile, workdir)
64         if os.system(tcmd) != 0:
65             print "ERROR: ti-eula-unpack: failed to extract tarfile"
66             raise bb.build.FuncFailed()
68     # Return to the previous directory
69     os.chdir(save_cwd)
70 }