omap3, am37x, am3517, beagleboard: unify and cleanup configs
[glsdk/meta-ti-glsdk.git] / recipes-ti / includes / ti-eula-unpack.inc
1 # This file defines function used for unpacking the .bin file downloaded over
2 # the http and display EULA.
3 #  BINFILE - name of the install jammer .bin file
4 #  TARFILE - name of the tar file inside the install jammer
5 #  TI_BIN_UNPK_CMDS   - contains list of commands separated with colon to be 
6 #                       passed while unpacking the bin file. The keyword 
7 #                       workdir expands to WORKDIR and commands are appendded
8 #                       with '\n'. Eg. TI_BIN_UNPK_CMDS="Y:Y: qY:workdir"
9 #  TI_BIN_UNPK_WDEXT  - This variable extends workdir path, if user wants to put
10 #                       the output in some internal directory
12 python do_unpack () {
13     bb.build.exec_func('base_do_unpack', d)
14     bb.build.exec_func('ti_bin_do_unpack', d)
15 }
17 TI_BIN_UNPK_WDEXT ?= ""
18 python ti_bin_do_unpack() {
20     import os
22     # InstallJammer requires 32bit version of glibc
23     lib32path = '/lib'
24     if os.path.exists('/lib64') and (os.path.islink('/lib64') or os.path.islink('/lib') or os.path.exists('/lib32')):
25         lib32path = '/lib32'
26     if not os.path.exists('%s/libc.so.6' % lib32path):
27         bb.warn("TI installer requires 32bit glibc libraries for proper operation\nrun 'yum install glibc.i686' on Fedora or 'apt-get install ia32-libs' on Ubuntu/Debian")
29     localdata = bb.data.createCopy(d)
30     bb.data.update_data(localdata)
32     binfile  = bb.data.getVar('BINFILE', localdata)
33     binfile  = bb.data.expand(binfile, localdata)
35     # Change to the working directory
36     save_cwd = os.getcwd()
37     workdir  = bb.data.getVar('WORKDIR', localdata)
38     workdir  = bb.data.expand(workdir, localdata)
39     os.chdir(workdir)
41     # Get unpack commands
42     cmd_string = bb.data.getVar('TI_BIN_UNPK_CMDS', localdata)
43     cmd_list = cmd_string.split( ":" )
45     # Make the InstallJammer binary executable so we can run it
46     os.chmod(binfile, 0755)
48     # Run the InstallJammer binary and accept the EULA
49     filename = "HOME=%s ./%s --mode console" % (workdir, binfile)
50     
51     # Test executable by printing installer version or help screen (--version currently broken for some installers) 
52     # - this is currently broken in some IJ installers - comment out for now
53     #if os.system(filename + " --version") != 0:
54     #   print "ERROR: ti-eula-unpack: failed to execute binary installer"
55     #   raise bb.build.FuncFailed()
56  
57     f = os.popen(filename,'w')
58     for cmd in cmd_list:
59         if cmd == "workdir":
60             wdext = bb.data.getVar('TI_BIN_UNPK_WDEXT', localdata)
61             wdext = bb.data.expand(wdext, localdata)
62             cmd = workdir+wdext
63         f.write(cmd+'\n');
64     f.close()
66     # Expand the tarball that was created if required
67     tarfile  = bb.data.getVar('TARFILE', localdata)    
68     if bool(tarfile) == True:
69         tarfile  = bb.data.expand(tarfile, localdata)
70         tcmd = 'tar x --no-same-owner -f %s -C %s' % (tarfile, workdir)
71         if os.system(tcmd) != 0:
72             print "ERROR: ti-eula-unpack: failed to extract tarfile"
73             raise bb.build.FuncFailed()
75     # Return to the previous directory
76     os.chdir(save_cwd)
77 }