dcabe9d9edf0a846b8ddaaccf09d92b2775f6e7f
[glsdk/meta-ti-glsdk.git] / recipes-ti / includes / ti-eula-unpack.inc
1 # This file defines function used for unpacking the .bin file downloaded over
2 # the http and display EULA.
3 #  BINFILE - name of the install jammer .bin file
4 #  TARFILE - name of the tar file inside the install jammer
5 #  TI_BIN_UNPK_CMDS   - contains list of commands separated with colon to be 
6 #                       passed while unpacking the bin file. The keyword 
7 #                       workdir expands to WORKDIR and commands are appendded
8 #                       with '\n'. Eg. TI_BIN_UNPK_CMDS="Y:Y: qY:workdir"
9 #  TI_BIN_UNPK_WDEXT  - This variable extends workdir path, if user wants to put
10 #                       the output in some internal directory
12 python do_unpack () {
13     bb.build.exec_func('base_do_unpack', d)
14     bb.build.exec_func('ti_bin_do_unpack', d)
15 }
17 TI_BIN_UNPK_WDEXT += ""
18 python ti_bin_do_unpack() {
20     import os
22     # InstallJammer requires 32bit version of glibc
23     lib32path = '/lib'
24     if os.path.exists('/lib64') and ( os.path.islink('/lib64') or os.path.islink('/lib') ):
25        lib32path = '/lib32'
26     if not os.path.exists('%s/libc.so.6' % lib32path):
27         raise bb.build.FuncFailed, \
28         "\nTI installer requires 32bit glibc libraries for proper operation\n\trun 'yum install glibc.i686' on Fedora or 'apt-get install ia32-libs' on Ubuntu/Debian"
30     localdata = bb.data.createCopy(d)
31     bb.data.update_data(localdata)
33     binfile  = bb.data.getVar('BINFILE', localdata)
34     binfile  = bb.data.expand(binfile, localdata)
36     # Change to the working directory
37     save_cwd = os.getcwd()
38     workdir  = bb.data.getVar('WORKDIR', localdata)
39     workdir  = bb.data.expand(workdir, localdata)
40     os.chdir(workdir)
42     # Get unpack commands
43     cmd_string = bb.data.getVar('TI_BIN_UNPK_CMDS', localdata)
44     cmd_list = cmd_string.split( ":" )
46     # Make the InstallJammer binary executable so we can run it
47     os.chmod(binfile, 0755)
49     # Run the InstallJammer binary and accept the EULA
50     filename = "HOME=%s ./%s --mode console" % (workdir, binfile)
51     
52     # Test executable by printing installer version or help screen (--version currently broken for some installers) 
53     # - this is currently broken in some IJ installers - comment out for now
54     #if os.system(filename + " --version") != 0:
55     #   print "ERROR: ti-eula-unpack: failed to execute binary installer"
56     #   raise bb.build.FuncFailed()
57  
58     f = os.popen(filename,'w')
59     for cmd in cmd_list:
60         if cmd == "workdir":
61             wdext = bb.data.getVar('TI_BIN_UNPK_WDEXT', localdata)
62             wdext = bb.data.expand(wdext, localdata)
63             cmd = workdir+wdext
64         print >>f, cmd
65     f.close()
67     # Expand the tarball that was created if required
68     tarfile  = bb.data.getVar('TARFILE', localdata)    
69     if bool(tarfile) == True:
70         tarfile  = bb.data.expand(tarfile, localdata)
71         tcmd = 'tar x --no-same-owner -f %s -C %s' % (tarfile, workdir)
72         if os.system(tcmd) != 0:
73             print "ERROR: ti-eula-unpack: failed to extract tarfile"
74             raise bb.build.FuncFailed()
76     # Return to the previous directory
77     os.chdir(save_cwd)
78 }