This layer hard depends on: URI: git://git.openembedded.org/openembedded-core branch: master revision: HEAD URI: git://git.openembedded.org/meta-openembedded branch: master revision: HEAD And optionally depends on: URI: git://git.angstrom-distribution.org/meta-angstrom branch: master revision: HEAD Currently meta-ti only works with the Angstrom distribution and hence requires the meta-angstrom layer. There are known issues when using gcc-4.6 based toolchain from OpenEmbedded-Core, thus gcc-4.5 toolchain, provided by meta-openembedded, is needed. It is planned to fix these shortcomings in the near future and allow building the base BSP part of meta-ti with different distributions and layer stacks, such as: distro-less (only with OE-Core), with Yocto/Poky, with Angstrom or Arago. Due to the above, it is now recommended to follow the instructions at http://www.angstrom-distribution.org/building-angstrom This will set it up for the OpenEmbedded-core ('yocto') layout instead of the old "Classic" OpenEmbedded-dev layout. You can optionally tweak sources/layers.txt and conf/bblayers.conf to (de)select BSP layers. Send pull requests to meta-ti@yoctoproject.org Main layer maintainers: Denys Dmytriyenko Koen Kooi