From c56786770eb0ccb95204cb72b961c44c65ff343b Mon Sep 17 00:00:00 2001 From: Chase Maupin Date: Thu, 17 May 2012 09:51:50 -0500 Subject: [PATCH] omap3_beagle: add usbethaddr setting to enable networking * In order for the SMSC USB ethernet device to work the usbethaddr setting must be set when the "usb start" command is executed and the network device is discovered. * Currently set this for de:ad:be:ef until we can start generating random or semi-random MAC addresses. * Based on work by Steve Kipisz and Joel Fernandez Upstream-Status: Not Upstreamable * We cannot upstream this hard coded MAC address setting. * User's should look at the following web page for information on how to generate a MAC address, but this patch enables the out of box experience for the SDK. http://www.denx.de/wiki/view/DULG/WhereCanIGetAValidMACAddress Signed-off-by: Chase Maupin --- include/configs/omap3_beagle.h | 1 + 1 files changed, 1 insertions(+), 0 deletions(-) diff --git a/include/configs/omap3_beagle.h b/include/configs/omap3_beagle.h index ddeb414..58a29b8 100644 --- a/include/configs/omap3_beagle.h +++ b/include/configs/omap3_beagle.h @@ -219,6 +219,7 @@ "loadaddr=0x80200000\0" \ "rdaddr=0x81000000\0" \ "usbtty=cdc_acm\0" \ + "usbethaddr=de:ad:be:ef\0" \ "bootfile=uImage.beagle\0" \ "console=ttyO2,115200n8\0" \ "mpurate=auto\0" \ -- 1.7.0.4