From 58ca6009d4101e5fd45ef9df22aa360d1662e9e9 Mon Sep 17 00:00:00 2001 From: Alexander Holler Date: Mon, 24 Jan 2011 13:08:49 +0000 Subject: [PATCH 03/16] omap3_beagle: enable the use of a plain text file named uEnv.txt instead of boot.scr Using the new env import command it is possible to use plain text files instead of script-images. Plain text files are much easier to handle. E.g. If your boot.scr contains the following: ----------------------------------- setenv dvimode 1024x768-16@60 run loaduimage run mmcboot ----------------------------------- you could create a file named uEnv.txt and use that instead of boot.scr: ----------------------------------- dvimode=1024x768-16@60 uenvcmd=run loaduimage; run mmcboot ----------------------------------- The variable uenvcmd (if existent) will be executed (using run) after uEnv.txt was loaded. If uenvcmd doesn't exist the default boot sequence will be started, therefore you could just use ----------------------------------- dvimode=1024x768-16@60 ----------------------------------- as uEnv.txt because loaduimage and mmcboot is part of the default boot sequence. --- Changes for v2: - Eliminated else redundant clause that would be ignored if boot succeeds. Changes for v3: - Removed boot.scr Changes for v4: - Removed comment about boot.scr being supported. --- include/configs/omap3_beagle.h | 28 ++++++++++++++++------------ 1 files changed, 16 insertions(+), 12 deletions(-) diff --git a/include/configs/omap3_beagle.h b/include/configs/omap3_beagle.h index 8b580ef..c85537c 100644 --- a/include/configs/omap3_beagle.h +++ b/include/configs/omap3_beagle.h @@ -213,9 +213,9 @@ "omapdss.def_disp=${defaultdisplay} " \ "root=${nandroot} " \ "rootfstype=${nandrootfstype}\0" \ - "loadbootscript=fatload mmc ${mmcdev} ${loadaddr} boot.scr\0" \ - "bootscript=echo Running bootscript from mmc ...; " \ - "source ${loadaddr}\0" \ + "loadbootenv=fatload mmc ${mmcdev} ${loadaddr} uEnv.txt\0" \ + "importbootenv=echo Importing environment from mmc ...; " \ + "env import -t $loadaddr $filesize\0" \ "loaduimage=fatload mmc ${mmcdev} ${loadaddr} uImage\0" \ "mmcboot=echo Booting from mmc ...; " \ "run mmcargs; " \ @@ -227,15 +227,19 @@ #define CONFIG_BOOTCOMMAND \ "if mmc rescan ${mmcdev}; then " \ - "if run loadbootscript; then " \ - "run bootscript; " \ - "else " \ - "if run loaduimage; then " \ - "run mmcboot; " \ - "else run nandboot; " \ - "fi; " \ - "fi; " \ - "else run nandboot; fi" + "echo SD/MMC found on device ${mmcdev};" \ + "if run loadbootenv; then " \ + "run importbootenv;" \ + "fi;" \ + "if test -n $uenvcmd; then " \ + "echo Running uenvcmd ...;" \ + "run uenvcmd;" \ + "fi;" \ + "if run loaduimage; then " \ + "run mmcboot;" \ + "fi;" \ + "fi;" \ + "run nandboot;" \ #define CONFIG_AUTO_COMPLETE 1 /* -- 1.6.6.1