From 10fbd32a96aedd644b6bf38888a2af64cc13a35f Mon Sep 17 00:00:00 2001 From: Matt Porter Date: Mon, 5 Dec 2011 15:29:35 -0600 Subject: [PATCH] musb: update PIO mode help information in Kconfig * Updated the Kconfig help information for the PIO mode for MUSB to make it more clear to the customer when to select this option and which devices currently have issues with this option. * This is in accordance with the findings for CPPI4.1 DMA usage for MUSB Upstream-Status: Submitted * Submitted to the PSP team using the lpr list Signed-off-by: Matt Porter Signed-off-by: Chase Maupin --- drivers/usb/musb/Kconfig | 11 +++++++---- 1 files changed, 7 insertions(+), 4 deletions(-) diff --git a/drivers/usb/musb/Kconfig b/drivers/usb/musb/Kconfig index ee75cbc..d56f23d 100644 --- a/drivers/usb/musb/Kconfig +++ b/drivers/usb/musb/Kconfig @@ -107,10 +107,13 @@ config MUSB_PIO_ONLY All data is copied between memory and FIFO by the CPU. DMA controllers are ignored. - Do not select 'n' here unless DMA support for your SOC or board - is unavailable (or unstable). When DMA is enabled at compile time, - you can still disable it at run time using the "use_dma=n" module - parameter. + Select 'y' here if DMA support for your SOC or board + is unavailable (or unstable). On CPPI 4.1 DMA based + systems (AM335x, AM35x, and AM180x) DMA support is + considered unstable and this option should be enabled + in production. When DMA is enabled at compile time, + you can still disable it at run time using the "use_dma=n" + module parameter. config USB_UX500_DMA_HW select USB_UX500_DMA -- 1.7.0.4