SECTION = "kernel" DESCRIPTION = "Linux kernel for TI devices" LICENSE = "GPLv2" LIC_FILES_CHKSUM = "file://COPYING;md5=d7810fab7487fb0aad327b76f1be7cd7" KERNEL_IMAGETYPE = "uImage" inherit kernel # This function must be here BEFORE the require of linux-dtb.inc below. # There is a "bug" in the base kernel.bbclass that after it's do_deploy # step it does not return back to the ${S} directory but stays in the # DEPLOY_DIR. However, the do_deploy_append defined in linux-dtb.inc # assumes that it is being run in the ${S} directory. A patch is # being submitted to fix this issue by either changing the do_deploy # in the kernel.bbclass to do "cd -" as the last step or to add # "cd ${S}" as the first line of do_deploy in linux-dtb.inc and this # function can be removed once that change is available. # If the function is not placed BEFORE the require then the change # directory is not appended before the linux-dtb.inc changes. do_deploy_append() { cd ${S} } require recipes-kernel/linux/linux-dtb.inc require recipes-kernel/linux/setup-defconfig.inc # Stage the power management firmware before building the kernel # for ti33x SOC_FAMILY devices DEPENDS_ti33x += "am33x-cm3" # Default is to package all dts files for ti33x devices unless building # for the specific beaglebone machine. KERNEL_DEVICETREE_ti33x = "arch/arm/boot/dts/am335x-evm.dts arch/arm/boot/dts/am335x-evmsk.dts arch/arm/boot/dts/am335x-bone.dts" KERNEL_DEVICETREE_beaglebone = "arch/arm/boot/dts/am335x-bone.dts" COMPATIBLE_MACHINE = "ti33x" S = "${WORKDIR}/git" BRANCH = "ti-linux-3.8.y" SRCREV = "ed93a28fb0b1dc28cc252ee87f6fce3e07bf23fe" PV = "3.8.3" # Append to the MACHINE_KERNEL_PR so that a new SRCREV will cause a rebuild MACHINE_KERNEL_PR_append = "a+gitr${SRCPV}" SRC_URI = "git://git.ti.com/ti-linux-kernel/ti-linux-kernel.git;protocol=git;branch=${BRANCH} \ file://defconfig \ " # Copy the am33x-cm3 firmware if it is available for ti33x SOC_FAMILY devices do_compile_prepend_ti33x() { if [ -e "${STAGING_DIR_HOST}/${base_libdir}/firmware/am335x-pm-firmware.bin" ] then cp "${STAGING_DIR_HOST}/${base_libdir}/firmware/am335x-pm-firmware.bin" "${S}/firmware" fi }