# This .inc file allows you to build and deploy multiple sets of kernel + modules with different defconfigs # # Note that this include will NOT stage anything nor create packages, since that is virtually impossible # Userspace should be built against the 'regular' kernel # # The intended usecase is for machines that have mutually exclusive drivers due to e.g. pinmuxing issues. # For example the LogicPD omap-l138 experimenter board can have multiple mutually exclusive expansion boards # like lcd, ethernet, sound, 20x2 character LCD, etc. To be able to easily test all of those you can use this .inc # # To make it easier finding the original defconfig from a running kernel, this also forcefully turns on # CONFIG_IKCONFIG_PROC so people can do 'zcat /proc/config.gz' on the target. require linux.inc SRC_URI += " \ file://configs/* " MULTI_CONFIG_BASE_SUFFIX = "multi-config-" do_compileconfigs () { # fixup for fetcher change if [ -e ${WORKDIR}/configs/configs ] ; then if [ -e ${WORKDIR}/configs/configs/.empty ] ; then mv ${WORKDIR}/configs/configs/.empty ${WORKDIR}/configs/ fi mv ${WORKDIR}/configs/configs/* ${WORKDIR}/configs/ rm -rf ${WORKDIR}/configs/configs fi # Compile and Install additional kernel configs if found if [ -e ${WORKDIR}/configs/.empty ] ; then echo "No configs found in configs/ directory, skipping to regular build" else echo "Multiple configs found, building those first" # Context Save the regular 'defconfig' cp ${WORKDIR}/defconfig ${WORKDIR}/defconfig.save for config in ${WORKDIR}/configs/* ; do # Copy in alternative config cd ${S} cp $config ${WORKDIR}/defconfig # Enable config to be viewed on the target echo "CONFIG_IKCONFIG=y" >> ${WORKDIR}/defconfig echo "CONFIG_IKCONFIG_PROC=y" >> ${WORKDIR}/defconfig # Build and Install this alternative kernel do_configure kernel_do_compile do_compile_kernelmodules kernel_do_install # Drop the resulting images in the deploy dir install -d ${DEPLOY_DIR_IMAGE} install -m 0644 ${KERNEL_OUTPUT} ${DEPLOY_DIR_IMAGE}/${KERNEL_IMAGE_BASE_NAME}.${MULTI_CONFIG_BASE_SUFFIX}$(basename $config).bin if [ -d "${D}/lib" ]; then tar --owner=root --group=root -cvzf ${DEPLOY_DIR_IMAGE}/${MODULES_IMAGE_BASE_NAME}.${MULTI_CONFIG_BASE_SUFFIX}$(basename $config).tgz -C ${D} lib fi # Install the final config alongside the images cp .config ${DEPLOY_DIR_IMAGE}/config-${PV}-${PR}-${MACHINE}.${MULTI_CONFIG_BASE_SUFFIX}$(basename $config).config # Create symlinks cd ${DEPLOY_DIR_IMAGE} rm -f ${KERNEL_IMAGE_SYMLINK_NAME}.${MULTI_CONFIG_BASE_SUFFIX}$(basename $config).bin ln -sf ${KERNEL_IMAGE_BASE_NAME}.${MULTI_CONFIG_BASE_SUFFIX}$(basename $config).bin ${KERNEL_IMAGE_SYMLINK_NAME}.${MULTI_CONFIG_BASE_SUFFIX}$(basename $config).bin rm -f modules-${MACHINE}.${MULTI_CONFIG_BASE_SUFFIX}$(basename $config).tgz ln -sf ${MODULES_IMAGE_BASE_NAME}.${MULTI_CONFIG_BASE_SUFFIX}$(basename $config).tgz modules-${MACHINE}.${MULTI_CONFIG_BASE_SUFFIX}$(basename $config).tgz rm -f config-${MACHINE}.${MULTI_CONFIG_BASE_SUFFIX}$(basename $config).config ln -sf config-${PV}-${PR}-${MACHINE}.${MULTI_CONFIG_BASE_SUFFIX}$(basename $config).config config-${MACHINE}.${MULTI_CONFIG_BASE_SUFFIX}$(basename $config).config done # Restore the regular 'defconfig' cp ${WORKDIR}/defconfig.save ${WORKDIR}/defconfig fi } # For reference, copy .config to deploy image do_deploy_append () { install -d ${DEPLOY_DIR_IMAGE} # Drop the regular defconfig along side the others for consistency cd ${S} cp .config ${DEPLOY_DIR_IMAGE}/config-${PV}-${PR}-${MACHINE}.config # add symlink cd ${DEPLOY_DIR_IMAGE} rm -f config-${MACHINE}.config ln -s config-${PV}-${PR}-${MACHINE}.config config-${MACHINE}.config rm -f modules-${MACHINE}.tgz ln -sf ${MODULES_IMAGE_BASE_NAME}.tgz modules-${MACHINE}.tgz } do_compileconfigs[depends] += "u-boot-mkimage-native:do_populate_sysroot virtual/${TARGET_PREFIX}gcc:do_populate_sysroot virtual/${TARGET_PREFIX}gcc${KERNEL_CCSUFFIX}:do_populate_sysroot" addtask compileconfigs after do_patch before do_configure