DESCRIPTION = "SYSLINK Inter-Processor Communications (IPC) for TI ARM/DSP processors" HOMEPAGE = "http://software-dl.ti.com/dsps/dsps_public_sw/sdo_sb/targetcontent/syslink/index.html" SECTION = "devel" LICENSE = "BSD" LIC_FILES_CHKSUM = "file://docs/bsd.pdf;md5=9f2edd962cd129f8c24e9ef1bd641029" # TODO :: multi-machine, add m3 build as well? # TODO :: proper staging? # TODO :: kernel module examples? # TODO :: smarter handling of config.bld # TODO :: review XDC parallel make - why not happening automatically? # TODO :: smarter suffix management require ../includes/ti-paths.inc require ../includes/ti-staging.inc PROVIDES = "ti-syslink-module" PROVIDES += "ti-syslink-examples" # This package builds a kernel module, use kernel PR as base and append a local version PR = "${MACHINE_KERNEL_PR}" PR_append = "a" PVExtra = "" inherit module pkgconfig S = "${WORKDIR}/syslink_${PV}${PVExtra}" SRC_URI = "http://software-dl.ti.com/dsps/dsps_public_sw/sdo_sb/targetcontent/syslink/${PV}${PVExtra}/exports/syslink_${PV}${PVExtra}.tar.gz;name=syslinktarball \ file://syslink.pc \ " DEPENDS = "ti-sysbios ti-xdctools ti-cgt6x ti-ipc ti-cgt470" DEPENDS += "virtual/kernel" #common frameq gateMP heapBufMP heapMemMP knlNotify listMP messageQ notify ringIO ringIO_gpp sharedRegion slaveLoader tilerDaemon SYSLINKHLOSSAMPLES = "knlnotify slaveLoader frameq notify" #SYSLINKRTOSSAMPLES = "frameq gateMP heapBufMP heapMemMP listMP messageQ notify ringIO ringIO_gpp sharedRegion" # SOC_FAMILY configuration SYSLINKPLATFORM_omap3 = "OMAP3530" SYSLINKPLATFORM_omapl137 = "OMAPL1XX" SYSLINKPLATFORM_omapl138 = "OMAPL1XX" SYSLINKPLATFORM_ti816x = "TI81XX" SYSLINKPLATFORM_ti814x = "TI81XX" SYSLINKPLATFORM ?= "" SYSLINKVARIANT_omap3 = "OMAP3530" SYSLINKVARIANT_omapl137 = "OMAPL1XX" SYSLINKVARIANT_omapl138 = "OMAPL1XX" SYSLINKVARIANT_ti816x = "TI816X" SYSLINKVARIANT_ti814x = "TI814X" SYSLINKVARIANT ?= "" # COFF/ELF config - omap3 can be coff/elf, omapl only coff, ti816x and ti814x only elf # this really needs to be a list... in the case of ELF/COFF (and this could use DSPSUFFIX?) SYSLINKSUFFIX_omap3 = "x64P" SYSLINKSUFFIX_omapl137 = "x674" SYSLINKSUFFIX_omapl138 = "x674" SYSLINKSUFFIX_ti816x = "xe674" SYSLINKSUFFIX_ti814x = "xe674" SYSLINKSUFFIX ?= "" SYSLINKLOADER_omap3 = "COFF" SYSLINKLOADER_omapl137 = "COFF" SYSLINKLOADER_omapl138 = "COFF" SYSLINKLOADER_ti816x = "ELF" SYSLINKLOADER_ti814x = "ELF" SYSLINKLOADER ?= "" # Do we really need to configure this? - configured already in config.bld XDCTARGETS_omap3 = "ti.targets.C64P" XDCTARGETS_omapl137 = "ti.targets.C674" XDCTARGETS_omapl138 = "ti.targets.C674" # for ti816x and ti814x, we should later also build for ti.targets.arm.elf.M3 XDCTARGETS_ti816x = "ti.targets.elf.C674 ti.targets.arm.elf.M3" XDCTARGETS_ti814x = "ti.targets.elf.C674 ti.targets.arm.elf.M3" XDCTARGETS ?= "" export XDCTARGETS # Exported Variable needed by build export SYSLINK_ROOT = "${S}/packages/" export XDCPATH = "${IPC_INSTALL_DIR}/packages;${SYSBIOS_INSTALL_DIR}/packages" do_configure() { sed -i -e s:@VERSION@:${PV}:g ${WORKDIR}/syslink.pc cp ${WORKDIR}/syslink.pc ${S} } do_prepsources () { # Prepare the tree for rebuiling - clean and generate interfaces cd ${SYSLINK_ROOT}/ti/syslink ${XDC_INSTALL_DIR}/xdc --jobs=${BB_NUMBER_THREADS} .make -PR . ${XDC_INSTALL_DIR}/xdc --jobs=${BB_NUMBER_THREADS} clean -PR . ${XDC_INSTALL_DIR}/xdc --jobs=${BB_NUMBER_THREADS} .interfaces -PR . } addtask prepsources after do_configure before do_compile do_compile() { # TODO :: KERNEL_CC, should use for kernel module build? # TODO :: Check the 'unset's unset CFLAGS CPPFLAGS CXXFLAGS LDFLAGS do_make_scripts # Build the gpp (hlos) kernel space cd ${SYSLINK_ROOT}/ti/syslink/utils/hlos/knl/Linux && make \ ARCH="${TARGET_ARCH}" \ CROSS_COMPILE="${TARGET_PREFIX}" \ SYSLINK_PLATFORM="${SYSLINKPLATFORM}" \ SYSLINK_VARIANT="${SYSLINKVARIANT}" \ SYSLINK_LOADER="${SYSLINKLOADER}" \ SYSLINK_PKGPATH="${IPC_INSTALL_DIR}/packages" \ KDIR="${STAGING_KERNEL_DIR}" # # Build the gpp (hlos) kernel space samples. # for sample in ${SYSLINKHLOSSAMPLES}; do # cd ${SYSLINK_ROOT}/ti/syslink/samples/hlos/$sample/knl/Linux && make \ # ARCH="${TARGET_ARCH}" \ # CROSS_COMPILE="${TARGET_PREFIX}" \ # SYSLINK_PLATFORM="${SYSLINKPLATFORM}" \ # SYSLINK_VARIANT="${SYSLINKVARIANT}" \ # SYSLINK_LOADER="${SYSLINKLOADER}" \ # SYSLINK_PKGPATH="${IPC_INSTALL_DIR}/packages" \ # SYSLINK_SDK=EZSDK \ # KDIR="${STAGING_KERNEL_DIR}" # done # Build the gpp (hlos) user space cd ${SYSLINK_ROOT}/ti/syslink/utils/hlos/usr/Linux && make \ ARCH="${TARGET_ARCH}" \ CROSS_COMPILE="${TARGET_PREFIX}" \ TOOLCHAIN_PREFIX="${TOOLCHAIN_PATH}/${TARGET_PREFIX}" \ SYSLINK_PLATFORM="${SYSLINKPLATFORM}" \ SYSLINK_VARIANT="${SYSLINKVARIANT}" \ SYSLINK_LOADER="${SYSLINKLOADER}" \ SYSLINK_PKGPATH="${IPC_INSTALL_DIR}/packages" # Build the gpp (hlos) user space samples # First build the common lib for samples. cd ${SYSLINK_ROOT}/ti/syslink/samples/hlos/common/usr/Linux && make \ ARCH="${TARGET_ARCH}" \ CROSS_COMPILE="${TARGET_PREFIX}" \ TOOLCHAIN_PREFIX="${TOOLCHAIN_PATH}/${TARGET_PREFIX}" \ SYSLINK_PLATFORM="${SYSLINKPLATFORM}" \ SYSLINK_VARIANT="${SYSLINKVARIANT}" \ SYSLINK_LOADER="${SYSLINKLOADER}" \ SYSLINK_SDK=EZSDK \ SYSLINK_PKGPATH="${IPC_INSTALL_DIR}/packages" for sample in ${SYSLINKHLOSSAMPLES}; do cd ${SYSLINK_ROOT}/ti/syslink/samples/hlos/$sample/usr/Linux && make \ ARCH="${TARGET_ARCH}" \ CROSS_COMPILE="${TARGET_PREFIX}" \ TOOLCHAIN_PREFIX="${TOOLCHAIN_PATH}/${TARGET_PREFIX}" \ SYSLINK_PLATFORM="${SYSLINKPLATFORM}" \ SYSLINK_VARIANT="${SYSLINKVARIANT}" \ SYSLINK_LOADER="${SYSLINKLOADER}" \ SYSLINK_SDK=EZSDK \ SYSLINK_PKGPATH="${IPC_INSTALL_DIR}/packages" done # Build the dsp/arm (rtos) code (system and samples) # cd ${SYSLINK_ROOT}/ti/syslink && \ # ${XDC_INSTALL_DIR}/xdc --jobs=${BB_NUMBER_THREADS} -PR . export XDCOPTIONS=v cd ${SYSLINK_ROOT}/ti/syslink && \ ${XDC_INSTALL_DIR}/xdc -P \ `${XDC_INSTALL_DIR}/bin/xdcpkg ${SYSLINK_ROOT}/ti/syslink | grep -v samples` export XDCARGS="profile=debug" cd ${SYSLINK_ROOT}/ti/syslink && \ ${XDC_INSTALL_DIR}/xdc --jobs=${BB_NUMBER_THREADS} -P \ `${XDC_INSTALL_DIR}/bin/xdcpkg ${SYSLINK_ROOT}/ti/syslink | grep samples` } KERNEL_VERSION = "${@base_read_file('${STAGING_KERNEL_DIR}/kernel-abiversion')}" do_install () { # Install the hlos kernel module install -d ${D}/lib/modules/${KERNEL_VERSION}/kernel/drivers/dsp install -m 0755 ${SYSLINK_ROOT}/ti/syslink/bin/${SYSLINKVARIANT}/syslink.ko ${D}/lib/modules/${KERNEL_VERSION}/kernel/drivers/dsp/ # Install the hlos example kernel modules and apps install -d ${D}/${installdir}/ti-syslink-examples install -m 0755 ${SYSLINK_ROOT}/ti/syslink/bin/${SYSLINKVARIANT}/samples/* ${D}/${installdir}/ti-syslink-examples/ # Install the rtos example apps install -d ${D}/${installdir}/ti-syslink-examples/dsp cd ${SYSLINK_ROOT}/ti/syslink/samples/rtos for i in $(find . -name "*.${SYSLINKSUFFIX}" | grep ${SOC_FAMILY}); do install ${i} ${D}/${installdir}/ti-syslink-examples/dsp/ done # TODO :: Fixup - library/headers installation - this shouldn't go into the examples directory.... # Needs proper staging # Install the library in the filesystem # install -d ${D}/${installdir}/ti-syslink-examples # install -m 0755 ${SYSLINK_ROOT}/ti/syslink/lib/syslink.a ${D}/${installdir}/ti-syslink-examples/ # Install/Stage the Source Tree install -d ${D}${SYSLINK_INSTALL_DIR_RECIPE} cp -pPrf ${S}/* ${D}${SYSLINK_INSTALL_DIR_RECIPE} install -d ${D}/${libdir}/pkgconfig install ${S}/syslink.pc ${D}/${libdir}/pkgconfig/ } PACKAGES =+ "ti-syslink-module" FILES_ti-syslink-module = "/lib/modules/${KERNEL_VERSION}/kernel/drivers/dsp/syslink.ko" RDEPENDS_ti-syslink-module += "update-modules" pkg_postinst_ti-syslink-module () { #!/bin/sh if [ -n "$D" ]; then exit 1 fi depmod -a update-modules || true } pkg_postrm_ti-syslink-module () { #!/bin/sh update-modules || true } PACKAGES =+ "ti-syslink-examples" RRECOMMENDS_ti-syslink-examples_append = " ti-syslink-module" FILES_ti-syslink-examples = "${installdir}/ti-syslink-examples/*" INSANE_SKIP_ti-syslink-examples = True FILES_ti-syslink-dev = "${libdir}/*"