index c4c88ec5c1ecc55d79060434fe5f79d9bb375d53..9c3e5ff3c6f4f5c1e0570cccb6886ef85cad97e1 100644 (file)
--- a/README
+++ b/README
-This layer depends on:
+This layer hard depends on:
URI: git://git.openembedded.org/openembedded-core
branch: master
revision: HEAD
URI: git://git.openembedded.org/openembedded-core
branch: master
revision: HEAD
-URI: git://git.angstrom-distribution.org/meta-angstrom
+URI: git://git.openembedded.org/meta-openembedded
branch: master
revision: HEAD
branch: master
revision: HEAD
-URI: git://git.openembedded.org/meta-openembedded
+And optionally depends on:
+
+URI: git://git.angstrom-distribution.org/meta-angstrom
branch: master
revision: HEAD
branch: master
revision: HEAD
-It is recommended to follow the instructions at http://www.angstrom-distribution.org/building-angstrom
+Currently meta-ti only works with the Angstrom distribution and hence
+requires the meta-angstrom layer. There are known issues when using
+gcc-4.6 based toolchain from OpenEmbedded-Core, thus gcc-4.5 toolchain,
+provided by meta-openembedded, is needed. It is planned to fix these
+shortcomings in the near future and allow building the base BSP part
+of meta-ti with different distributions and layer stacks, such as:
+distro-less (only with OE-Core), with Yocto/Poky, with Angstrom or
+Arago.
+
+Due to the above, it is now recommended to follow the instructions at
+http://www.angstrom-distribution.org/building-angstrom
-This will set it up for the OpenEmbedded-core layout instead of the old
-OpenEmbedded-dev layout. You can optionally tweak sources/layers.txt and conf/bblayers.conf to (de)select BSP layers.
+This will set it up for the OpenEmbedded-core ('yocto') layout instead
+of the old "Classic" OpenEmbedded-dev layout. You can optionally tweak
+sources/layers.txt and conf/bblayers.conf to (de)select BSP layers.
Send pull requests to meta-ti@yoctoproject.org
Send pull requests to meta-ti@yoctoproject.org