diff --git a/recipes-graphics/libgles/libgles-omap3-4.09.00.01/rc_dri.pvr b/recipes-graphics/libgles/libgles-omap3-4.09.00.01/rc_dri.pvr
--- /dev/null
@@ -0,0 +1,136 @@
+#!/bin/sh
+PATH=$PATH:/usr/sbin
+
+# Check if an fb device is available. If not then just go ahead and
+# exit because we have no display.
+fbset > /dev/null 2>&1
+if [ "$?" == "1" ]
+then
+ # looks like there is no display, so let's exit
+ exit 0
+fi
+
+BITSPERPIXEL="$(fbset | grep geom | awk '{print $6}')"
+YRES="$(fbset | grep geom | awk '{print $3}')"
+
+CPUTYPE="$(cputype)"
+
+if [ "$1" = "" ]; then
+ echo PVR-INIT: Please use start, stop, or restart.
+ exit 1
+fi
+
+if [ "$1" = "stop" -o "$1" = "restart" ]; then
+ echo Stopping PVR
+
+ # Stop the X Server.
+ #
+ [ -f /tmp/.X0-lock ] && read XPID < /tmp/.X0-lock && [ -n "$XPID" ] && kill $XPID && while [ -e /proc/$XPID ] ; do sleep 1; done
+
+ rmmod bufferclass_ti
+ rmmod pvrsrvkm 2>/dev/null
+ rmmod drm 2>/dev/null
+fi
+
+if [ "$1" = "stop" ]; then
+ exit 0
+fi
+
+# Set RGBA ordering to something the drivers like
+if [ "$BITSPERPIXEL" = "32" ] ; then
+ fbset -rgba 8/16,8/8,8/0,8/24
+fi
+
+# Try to enable triple buffering when there's enough VRAM
+fbset -vyres $(expr $YRES \* 3)
+
+sgxprepare () {
+ echo Starting PVR
+
+ # Start the X Server.
+ # The X Server will load the PVR Services module.
+ #
+ /usr/local/XSGX/bin/X -verbose -config /usr/local/XSGX/etc/xorg.conf &
+
+ modprobe drm
+
+ insmod $(busybox find /lib/modules/$(uname -r) -name "pvrsrvkm.ko")
+
+ if [ "$?" != "0" ]
+ then
+ echo "Could not find pvrsrvkm driver"
+ exit 1
+ fi
+
+ modprobe bufferclass_ti
+
+ pvr_maj=`grep "pvrsrvkm$" /proc/devices | cut -b1,2,3`
+ bc_maj=`grep "bc" /proc/devices | cut -b1,2,3`
+
+ if [ -e /dev/pvrsrvkm ] ; then
+ rm -f /dev/pvrsrvkm
+ fi
+
+ mknod /dev/pvrsrvkm c $pvr_maj 0
+ chmod 666 /dev/pvrsrvkm
+
+ touch /etc/powervr-esrev
+
+ SAVED_ESREVISION="$(cat /etc/powervr-esrev)"
+}
+
+sgxfinish () {
+ # Fix up a bug in opkg
+ if [ $(readlink /usr/lib/libsrv_um.so) != $(readlink /usr/lib/libsrv_um.so.1) ] ; then
+ cd /usr/lib
+ ln -sf $(readlink /usr/lib/libsrv_um.so.1) libsrv_um.so
+ fi
+
+ if [ "${ES_REVISION}" != "${SAVED_ESREVISION}" ] ; then
+ echo -n "Starting SGX fixup for"
+ echo " ES${ES_REVISION}.x"
+ cp -a /usr/lib/ES${ES_REVISION}.0/* /usr/lib
+ cp -a /usr/bin/ES${ES_REVISION}.0/* /usr/bin
+ echo "${ES_REVISION}" > /etc/powervr-esrev
+ fi
+
+ if ! /usr/bin/pvrsrvctl --start --no-module; then return; fi
+}
+
+case $CPUTYPE in
+"OMAP3530")
+ sgxprepare
+
+ devmem2 0x48004B48 w 0x2 > /dev/null
+ devmem2 0x48004B10 w 0x1 > /dev/null
+ devmem2 0x48004B00 w 0x2 > /dev/null
+
+ ES_REVISION="$(devmem2 0x50000014 | sed -e s:0x00010205:5: -e s:0x00010201:3: -e s:0x00010003:2: | tail -n1 | awk -F': ' '{print $2}')"
+
+ sgxfinish
+ ;;
+"TI33XX")
+ sgxprepare
+
+ devmem2 0x44e01104 w 0x0 > /dev/null
+ devmem2 0x44e00904 w 0x2 > /dev/null
+
+ ES_REVISION="$(devmem2 0x56000014 | sed -e s:0x00010205:8: | tail -n1 | awk -F': ' '{print $2}')"
+
+ sgxfinish
+ ;;
+"TI816x")
+ sgxprepare
+
+ devmem2 0x48180F04 w 0x0 > /dev/null
+ devmem2 0x48180900 w 0x2 > /dev/null
+ devmem2 0x48180920 w 0x2 > /dev/null
+
+ ES_REVISION="$(devmem2 0x56000014 | sed -e s:0x00010205:6: -e s:0x00010201:3: -e s:0x00010003:2: | tail -n1 | awk -F': ' '{print $2}')"
+
+ sgxfinish
+ ;;
+*)
+ echo No SGX hardware, not starting PVR
+ ;;
+esac