linux-ti-staging: update to ti2013.04.02 release
[glsdk/meta-ti-glsdk.git] / recipes-kernel / linux / linux-ti-staging_3.8.bb
index 21202f42e585f823dbb1d43e79e31a5826db66ba..29ffebc2a465287d18697d3eb9e515994be15da9 100644 (file)
@@ -6,33 +6,19 @@ KERNEL_IMAGETYPE = "uImage"
 
 inherit kernel
 
 
 inherit kernel
 
-# This function must be here BEFORE the require of linux-dtb.inc below.
-# There is a "bug" in the base kernel.bbclass that after it's do_deploy
-# step it does not return back to the ${S} directory but stays in the
-# DEPLOY_DIR.  However, the do_deploy_append defined in linux-dtb.inc
-# assumes that it is being run in the ${S} directory.  A patch is
-# being submitted to fix this issue by either changing the do_deploy
-# in the kernel.bbclass to do "cd -" as the last step or to add
-# "cd ${S}" as the first line of do_deploy in linux-dtb.inc and this
-# function can be removed once that change is available.
-# If the function is not placed BEFORE the require then the change
-# directory is not appended before the linux-dtb.inc changes.
-do_deploy_append() {
-    cd ${S}
-}
-
 require recipes-kernel/linux/linux-dtb.inc
 require recipes-kernel/linux/setup-defconfig.inc
 
 require recipes-kernel/linux/linux-dtb.inc
 require recipes-kernel/linux/setup-defconfig.inc
 
-# Stage the power management firmware before building the kernel
-# for ti33x SOC_FAMILY devices
-DEPENDS_ti33x += "am33x-cm3"
+# Add a run-time dependency for the PM firmware to be installed
+# on the target file system.
+RDEPENDS_kernel-base_ti33x += "am33x-cm3 am33x-cm3-initscript"
 
 # Default is to package all dts files for ti33x devices unless building
 # for the specific beaglebone machine.
 KERNEL_DEVICETREE_ti33x = "arch/arm/boot/dts/am335x-evm.dts arch/arm/boot/dts/am335x-evmsk.dts arch/arm/boot/dts/am335x-bone.dts"
 KERNEL_DEVICETREE_beaglebone = "arch/arm/boot/dts/am335x-bone.dts"
 KERNEL_DEVICETREE_omap5-evm = "arch/arm/boot/dts/omap5-sevm.dts arch/arm/boot/dts/omap5-uevm.dts"
 
 # Default is to package all dts files for ti33x devices unless building
 # for the specific beaglebone machine.
 KERNEL_DEVICETREE_ti33x = "arch/arm/boot/dts/am335x-evm.dts arch/arm/boot/dts/am335x-evmsk.dts arch/arm/boot/dts/am335x-bone.dts"
 KERNEL_DEVICETREE_beaglebone = "arch/arm/boot/dts/am335x-bone.dts"
 KERNEL_DEVICETREE_omap5-evm = "arch/arm/boot/dts/omap5-sevm.dts arch/arm/boot/dts/omap5-uevm.dts"
+KERNEL_DEVICETREE_dra7xx-evm = "arch/arm/boot/dts/dra7-evm.dts"
 
 COMPATIBLE_MACHINE = "ti33x|omap-a15"
 
 
 COMPATIBLE_MACHINE = "ti33x|omap-a15"
 
@@ -40,20 +26,13 @@ S = "${WORKDIR}/git"
 
 BRANCH = "ti-linux-3.8.y"
 
 
 BRANCH = "ti-linux-3.8.y"
 
-SRCREV = "f6ce51c2d6e5489262beb6f42cc39ac19e49bc9e"
-PV = "3.8.5"
+# This commit corresponds to ti2013.04.02 release tag
+SRCREV = "f3cb62a800ae37f17a3382b10d155ee02dbc83fc"
+PV = "3.8.13"
 
 # Append to the MACHINE_KERNEL_PR so that a new SRCREV will cause a rebuild
 
 # Append to the MACHINE_KERNEL_PR so that a new SRCREV will cause a rebuild
-MACHINE_KERNEL_PR_append = "c+gitr${SRCPV}"
+MACHINE_KERNEL_PR_append = "f+gitr${SRCPV}"
 
 SRC_URI = "git://git.ti.com/ti-linux-kernel/ti-linux-kernel.git;protocol=git;branch=${BRANCH} \
            file://defconfig \
           "
 
 SRC_URI = "git://git.ti.com/ti-linux-kernel/ti-linux-kernel.git;protocol=git;branch=${BRANCH} \
            file://defconfig \
           "
-
-# Copy the am33x-cm3 firmware if it is available for ti33x SOC_FAMILY devices
-do_compile_prepend_ti33x() {
-    if [ -e "${STAGING_DIR_HOST}/${base_libdir}/firmware/am335x-pm-firmware.bin" ]
-    then
-        cp "${STAGING_DIR_HOST}/${base_libdir}/firmware/am335x-pm-firmware.bin" "${S}/firmware"
-    fi
-}