linux-omap_2.6.39: remove patch that prevented board from resuming from suspend.
authorTasslehoff Kjappfot <tasskjapp@gmail.com>
Thu, 1 Sep 2011 01:41:19 +0000 (01:41 +0000)
committerKoen Kooi <koen@dominion.thruhere.net>
Thu, 1 Sep 2011 07:56:15 +0000 (09:56 +0200)
commit5c670d945ef54b820a142287bdf4a55c868f3b93
tree15582c9a4d3828c9c7167a1069add25b4b98f2c2
parent30d7de63ec4284164cfc9ac80db16d9c6b98be33
linux-omap_2.6.39: remove patch that prevented board from resuming from suspend.

Running on a board similar to Beagleboard C3 (but without NAND) I could not resume from suspend with the patch.
The console output when suspending was as expected, but neither console input nor a timer would wake the board.
Without the patch, everything works as it should.

Signed-off-by: Tasslehoff Kjappfot <tasskjapp@gmail.com>
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
recipes-kernel/linux/linux-omap_2.6.39.bb