linux.inc: If the kernel has CONFIG_KERNEL_LZO=y, it may well attempt to use the...
authorChristopher Larson <chris_larson@mentor.com>
Sat, 17 Dec 2011 15:36:07 +0000 (16:36 +0100)
committerKoen Kooi <koen@dominion.thruhere.net>
Mon, 19 Dec 2011 20:11:50 +0000 (21:11 +0100)
commitb72cb13fcf83b9d342808ea30379bfb6a1321b54
tree7ccea20e2e927a43042b453954eaab9e62ed0480
parent018824ece4a04245b4277d5c8afcccfd6ca75df0
linux.inc: If the kernel has CONFIG_KERNEL_LZO=y, it may well attempt to use the 'lzop' utility to do the lzo compression, but we should not be relying on that utility being installed on the build machine.

This currently affects the linux-omap4 build for omap4430-panda.

Signed-off-by: Christopher Larson <chris_larson@mentor.com>
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
recipes-kernel/linux/linux.inc