]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/meta-ti-glsdk.git/commitdiff
linux-ti33x-psp 3.2: merge in 6 musb patches from PSP
authorKoen Kooi <koen@dominion.thruhere.net>
Tue, 22 May 2012 06:06:26 +0000 (08:06 +0200)
committerDenys Dmytriyenko <denys@ti.com>
Tue, 29 May 2012 19:49:27 +0000 (15:49 -0400)
Updating the SRCREV would require redoing all boardfile patches due to the
EVM-SK changes. So cherry-pick the 6 patches we need.

Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
recipes-kernel/linux/linux-ti33x-psp-3.2/usb/0001-usb-musb-cppi41-revisit-the-teardown-path-to-fix-iso.patch [new file with mode: 0644]
recipes-kernel/linux/linux-ti33x-psp-3.2/usb/0002-usb-musb-fix-bug-in-data-toggle-sw-workaround.patch [new file with mode: 0644]
recipes-kernel/linux/linux-ti33x-psp-3.2/usb/0003-usb-gadget-udc-core-stop-UDC-on-device-initiated-dis.patch [new file with mode: 0644]
recipes-kernel/linux/linux-ti33x-psp-3.2/usb/0004-usb-gadget-udc-core-fix-asymmetric-calls-in-remove_d.patch [new file with mode: 0644]
recipes-kernel/linux/linux-ti33x-psp-3.2/usb/0005-usb-gadget-udc-core-fix-wrong-call-order.patch [new file with mode: 0644]
recipes-kernel/linux/linux-ti33x-psp-3.2/usb/0006-usb-gadget-udc-core-fix-incompatibility-with-dummy-h.patch [new file with mode: 0644]
recipes-kernel/linux/linux-ti33x-psp_3.2.bb

diff --git a/recipes-kernel/linux/linux-ti33x-psp-3.2/usb/0001-usb-musb-cppi41-revisit-the-teardown-path-to-fix-iso.patch b/recipes-kernel/linux/linux-ti33x-psp-3.2/usb/0001-usb-musb-cppi41-revisit-the-teardown-path-to-fix-iso.patch
new file mode 100644 (file)
index 0000000..dd2e19a
--- /dev/null
@@ -0,0 +1,103 @@
+From c2746810dc7bcaaae2dec493c501eb7213d14858 Mon Sep 17 00:00:00 2001
+From: Ajay Kumar Gupta <ajay.gupta@ti.com>
+Date: Tue, 8 May 2012 12:05:47 +0530
+Subject: [PATCH 1/6] usb: musb: cppi41: revisit the teardown path to fix isoc
+ issue
+
+Fixes the camera streaming issue when application is stopped and restarted multiple times.
+Changes:
+       - Disable DMAReq of TX/RX endpoints before teardown
+       - FIFO flush only when RxPktRdy is set
+       - Clear ReqPkt if in host mode.
+---
+ drivers/usb/musb/cppi41_dma.c |   42 ++++++++++++++++++++++++----------------
+ drivers/usb/musb/musb_host.c  |    2 +-
+ 2 files changed, 26 insertions(+), 18 deletions(-)
+
+diff --git a/drivers/usb/musb/cppi41_dma.c b/drivers/usb/musb/cppi41_dma.c
+index e4d3173..4761acd 100644
+--- a/drivers/usb/musb/cppi41_dma.c
++++ b/drivers/usb/musb/cppi41_dma.c
+@@ -1206,6 +1206,11 @@ static int cppi41_channel_abort(struct dma_channel *channel)
+       if (cppi_ch->transmit) {
+               dprintk("Tx channel teardown, cppi_ch = %p\n", cppi_ch);
++              /* disable the DMAreq before teardown */
++              csr  = musb_readw(epio, MUSB_TXCSR);
++              csr &= ~MUSB_TXCSR_DMAENAB;
++              musb_writew(epio, MUSB_TXCSR, csr);
++
+               /* Tear down Tx DMA channel */
+               usb_tx_ch_teardown(cppi_ch);
+@@ -1223,11 +1228,30 @@ static int cppi41_channel_abort(struct dma_channel *channel)
+       } else { /* Rx */
+               dprintk("Rx channel teardown, cppi_ch = %p\n", cppi_ch);
++              /* disable the DMAreq and remove reqpkt */
++              csr  = musb_readw(epio, MUSB_RXCSR);
++              dev_dbg(musb->controller,
++                      "before rx-teardown: rxcsr %x rxcount %x\n", csr,
++                      musb_readw(epio, MUSB_RXCOUNT));
++
++              /* For host, clear (just) ReqPkt at end of current packet(s) */
++              if (is_host_active(cppi->musb))
++                      csr &= ~MUSB_RXCSR_H_REQPKT;
++
++              csr &= ~MUSB_RXCSR_DMAENAB;
++              musb_writew(epio, MUSB_RXCSR, csr);
++
++
+               /* Flush FIFO of the endpoint */
+               csr  = musb_readw(epio, MUSB_RXCSR);
+-              csr |= MUSB_RXCSR_FLUSHFIFO | MUSB_RXCSR_H_WZC_BITS;
++
++              if (csr & MUSB_RXCSR_RXPKTRDY)
++                      csr |= MUSB_RXCSR_FLUSHFIFO;
++
++              csr |= MUSB_RXCSR_H_WZC_BITS;
+               musb_writew(epio, MUSB_RXCSR, csr);
+               musb_writew(epio, MUSB_RXCSR, csr);
++              csr  = musb_readw(epio, MUSB_RXCSR);
+               /* Issue CPPI FIFO teardown for Rx channel */
+               td_reg  = musb_readl(reg_base, cppi->teardown_reg_offs);
+@@ -1246,22 +1270,6 @@ static int cppi41_channel_abort(struct dma_channel *channel)
+               /* For host, ensure ReqPkt is never set again */
+               cppi41_autoreq_update(cppi_ch, USB_NO_AUTOREQ);
+-
+-              /* For host, clear (just) ReqPkt at end of current packet(s) */
+-              if (is_host_active(cppi->musb))
+-                      csr &= ~MUSB_RXCSR_H_REQPKT;
+-              csr |= MUSB_RXCSR_H_WZC_BITS;
+-
+-              /* Clear DMA enable */
+-              csr &= ~MUSB_RXCSR_DMAENAB;
+-              musb_writew(epio, MUSB_RXCSR, csr);
+-
+-              /* Flush the FIFO of endpoint once again */
+-              csr  = musb_readw(epio, MUSB_RXCSR);
+-              csr |= MUSB_RXCSR_FLUSHFIFO | MUSB_RXCSR_H_WZC_BITS;
+-              musb_writew(epio, MUSB_RXCSR, csr);
+-
+-              udelay(50);
+       }
+       /*
+diff --git a/drivers/usb/musb/musb_host.c b/drivers/usb/musb/musb_host.c
+index d805d1b..2195633 100644
+--- a/drivers/usb/musb/musb_host.c
++++ b/drivers/usb/musb/musb_host.c
+@@ -2224,7 +2224,7 @@ static int musb_cleanup_urb(struct urb *urb, struct musb_qh *qh)
+       }
+       /* turn off DMA requests, discard state, stop polling ... */
+-      if (is_in) {
++      if (is_in && ep->epnum) {
+               /* giveback saves bulk toggle */
+               csr = musb_h_flush_rxfifo(ep, 0);
+-- 
+1.7.7.6
+
diff --git a/recipes-kernel/linux/linux-ti33x-psp-3.2/usb/0002-usb-musb-fix-bug-in-data-toggle-sw-workaround.patch b/recipes-kernel/linux/linux-ti33x-psp-3.2/usb/0002-usb-musb-fix-bug-in-data-toggle-sw-workaround.patch
new file mode 100644 (file)
index 0000000..dab230c
--- /dev/null
@@ -0,0 +1,31 @@
+From a9e9e758646ee41289c0030645bbdd43c711e9c1 Mon Sep 17 00:00:00 2001
+From: Ajay Kumar Gupta <ajay.gupta@ti.com>
+Date: Fri, 18 May 2012 14:51:15 +0530
+Subject: [PATCH 2/6] usb: musb: fix bug in data toggle sw workaround
+
+Data toggle software workaround for extra IN issue introduced a bug for PIO mode
+as data toggle is getting updated even for PIO mode which should not be done.
+
+Merge to:
+usb: musb: cppi41: correct data toggle mismatch to fix extra IN token issue
+---
+ drivers/usb/musb/musb_host.c |    3 ++-
+ 1 files changed, 2 insertions(+), 1 deletions(-)
+
+diff --git a/drivers/usb/musb/musb_host.c b/drivers/usb/musb/musb_host.c
+index 2195633..80d83bd 100644
+--- a/drivers/usb/musb/musb_host.c
++++ b/drivers/usb/musb/musb_host.c
+@@ -359,7 +359,8 @@ static inline void musb_save_toggle(struct musb_qh *qh, int is_in,
+               curr_toggle = csr ? 1 : 0;
+               /* check if data toggle has gone out of sync */
+-              if (curr_toggle == qh->hw_ep->prev_toggle) {
++              if (is_dma_capable() && qh->hw_ep->rx_channel &&
++                              curr_toggle == qh->hw_ep->prev_toggle) {
+                       dev_dbg(musb->controller,
+                               "Data toggle same as previous (=%d) on ep%d\n",
+                                       curr_toggle, qh->hw_ep->epnum);
+-- 
+1.7.7.6
+
diff --git a/recipes-kernel/linux/linux-ti33x-psp-3.2/usb/0003-usb-gadget-udc-core-stop-UDC-on-device-initiated-dis.patch b/recipes-kernel/linux/linux-ti33x-psp-3.2/usb/0003-usb-gadget-udc-core-stop-UDC-on-device-initiated-dis.patch
new file mode 100644 (file)
index 0000000..88a1fb9
--- /dev/null
@@ -0,0 +1,41 @@
+From 2eac6057134bcb77edcdc462b810465850caec23 Mon Sep 17 00:00:00 2001
+From: Felipe Balbi <balbi@ti.com>
+Date: Thu, 15 Mar 2012 16:37:18 +0200
+Subject: [PATCH 3/6] usb: gadget: udc-core: stop UDC on device-initiated
+ disconnect
+
+When we want to do device-initiated disconnect,
+let's make sure we stop the UDC in order to
+e.g. allow lower power states to be achieved by
+turning off unnecessary clocks and/or stoping
+PHYs.
+
+When reconnecting, call ->udc_start() again to
+make sure UDC is reinitialized.
+
+Cc: stable@vger.kernel.org
+Signed-off-by: Felipe Balbi <balbi@ti.com>
+---
+ drivers/usb/gadget/udc-core.c |    4 ++++
+ 1 files changed, 4 insertions(+), 0 deletions(-)
+
+diff --git a/drivers/usb/gadget/udc-core.c b/drivers/usb/gadget/udc-core.c
+index 0b0d12c..475c997 100644
+--- a/drivers/usb/gadget/udc-core.c
++++ b/drivers/usb/gadget/udc-core.c
+@@ -359,8 +359,12 @@ static ssize_t usb_udc_softconn_store(struct device *dev,
+       struct usb_udc          *udc = container_of(dev, struct usb_udc, dev);
+       if (sysfs_streq(buf, "connect")) {
++              if (udc_is_newstyle(udc))
++                      usb_gadget_udc_start(udc->gadget, udc->driver);
+               usb_gadget_connect(udc->gadget);
+       } else if (sysfs_streq(buf, "disconnect")) {
++              if (udc_is_newstyle(udc))
++                      usb_gadget_udc_stop(udc->gadget, udc->driver);
+               usb_gadget_disconnect(udc->gadget);
+       } else {
+               dev_err(dev, "unsupported command '%s'\n", buf);
+-- 
+1.7.7.6
+
diff --git a/recipes-kernel/linux/linux-ti33x-psp-3.2/usb/0004-usb-gadget-udc-core-fix-asymmetric-calls-in-remove_d.patch b/recipes-kernel/linux/linux-ti33x-psp-3.2/usb/0004-usb-gadget-udc-core-fix-asymmetric-calls-in-remove_d.patch
new file mode 100644 (file)
index 0000000..eae1c70
--- /dev/null
@@ -0,0 +1,43 @@
+From fefa8fade565b137ae3d01801196840b6ccfc98f Mon Sep 17 00:00:00 2001
+From: Kishon Vijay Abraham I <kishon@ti.com>
+Date: Wed, 21 Mar 2012 21:34:30 +0530
+Subject: [PATCH 4/6] usb: gadget: udc-core: fix asymmetric calls in
+ remove_driver
+
+During modprobe of gadget driver, pullup is called after
+udc_start. In order to make the exit path symmetric when
+removing a gadget driver, call pullup before ->udc_stop.
+
+This is needed to avoid issues with PM where udc_stop
+disables the module completely (put IP in reset state,
+cut functional and interface clocks, and so on), which
+prevents us from accessing the IP's address space,
+thus creating the possibility of an abort exception
+when we try to access IP's address space after clocks
+are off.
+
+Cc: stable@vger.kernel.org
+Signed-off-by: Partha Basak <p-basak2@ti.com>
+Signed-off-by: Kishon Vijay Abraham I <kishon@ti.com>
+Signed-off-by: Felipe Balbi <balbi@ti.com>
+---
+ drivers/usb/gadget/udc-core.c |    2 +-
+ 1 files changed, 1 insertions(+), 1 deletions(-)
+
+diff --git a/drivers/usb/gadget/udc-core.c b/drivers/usb/gadget/udc-core.c
+index 475c997..ec02ed0 100644
+--- a/drivers/usb/gadget/udc-core.c
++++ b/drivers/usb/gadget/udc-core.c
+@@ -212,8 +212,8 @@ static void usb_gadget_remove_driver(struct usb_udc *udc)
+       if (udc_is_newstyle(udc)) {
+               udc->driver->disconnect(udc->gadget);
+               udc->driver->unbind(udc->gadget);
+-              usb_gadget_udc_stop(udc->gadget, udc->driver);
+               usb_gadget_disconnect(udc->gadget);
++              usb_gadget_udc_stop(udc->gadget, udc->driver);
+       } else {
+               usb_gadget_stop(udc->gadget, udc->driver);
+       }
+-- 
+1.7.7.6
+
diff --git a/recipes-kernel/linux/linux-ti33x-psp-3.2/usb/0005-usb-gadget-udc-core-fix-wrong-call-order.patch b/recipes-kernel/linux/linux-ti33x-psp-3.2/usb/0005-usb-gadget-udc-core-fix-wrong-call-order.patch
new file mode 100644 (file)
index 0000000..ae705cf
--- /dev/null
@@ -0,0 +1,33 @@
+From 7a0dcaac06bfffd4df4bf7a006c601b31acc7cb7 Mon Sep 17 00:00:00 2001
+From: Felipe Balbi <balbi@ti.com>
+Date: Fri, 27 Apr 2012 11:02:15 +0300
+Subject: [PATCH 5/6] usb: gadget: udc-core: fix wrong call order
+
+commit 6d258a4 (usb: gadget: udc-core: stop UDC on device-initiated
+disconnect) introduced another case of asymmetric calls when issuing
+a device-initiated disconnect. Fix it.
+
+Reported-by: Ben Hutchings <ben@decadent.org.uk>
+Signed-off-by: Felipe Balbi <balbi@ti.com>
+---
+ drivers/usb/gadget/udc-core.c |    2 +-
+ 1 files changed, 1 insertions(+), 1 deletions(-)
+
+diff --git a/drivers/usb/gadget/udc-core.c b/drivers/usb/gadget/udc-core.c
+index ec02ed0..3ea783d 100644
+--- a/drivers/usb/gadget/udc-core.c
++++ b/drivers/usb/gadget/udc-core.c
+@@ -363,9 +363,9 @@ static ssize_t usb_udc_softconn_store(struct device *dev,
+                       usb_gadget_udc_start(udc->gadget, udc->driver);
+               usb_gadget_connect(udc->gadget);
+       } else if (sysfs_streq(buf, "disconnect")) {
++              usb_gadget_disconnect(udc->gadget);
+               if (udc_is_newstyle(udc))
+                       usb_gadget_udc_stop(udc->gadget, udc->driver);
+-              usb_gadget_disconnect(udc->gadget);
+       } else {
+               dev_err(dev, "unsupported command '%s'\n", buf);
+               return -EINVAL;
+-- 
+1.7.7.6
+
diff --git a/recipes-kernel/linux/linux-ti33x-psp-3.2/usb/0006-usb-gadget-udc-core-fix-incompatibility-with-dummy-h.patch b/recipes-kernel/linux/linux-ti33x-psp-3.2/usb/0006-usb-gadget-udc-core-fix-incompatibility-with-dummy-h.patch
new file mode 100644 (file)
index 0000000..70f9398
--- /dev/null
@@ -0,0 +1,46 @@
+From 91cdc6fbc271e01e231dcf0e9403448aa19433fb Mon Sep 17 00:00:00 2001
+From: Alan Stern <stern@rowland.harvard.edu>
+Date: Thu, 26 Apr 2012 11:31:57 -0400
+Subject: [PATCH 6/6] usb: gadget: udc-core: fix incompatibility with
+ dummy-hcd
+
+This patch (as1548) fixes a recently-introduced incompatibility
+between the UDC core and the dummy-hcd driver.  Commit
+8ae8090c82eb407267001f75b3d256b3bd4ae691 (usb: gadget: udc-core: fix
+asymmetric calls in remove_driver) moved the usb_gadget_udc_stop()
+call in usb_gadget_remove_driver() below the usb_gadget_disconnect()
+call.
+
+As a result, usb_gadget_disconnect() gets called at a time when the
+gadget driver believes it has been unbound but dummy-hcd believes
+it has not.  A nasty error ensues when dummy-hcd calls the gadget
+driver's disconnect method a second time.
+
+To fix the problem, this patch moves the gadget driver's unbind
+notification after the usb_gadget_disconnect() call.  Now nothing
+happens between the two unbind notifications, so nothing goes wrong.
+
+Signed-off-by: Alan Stern <stern@rowland.harvard.edu>
+Tested-by: Alexander Shishkin <alexander.shishkin@linux.intel.com>
+Signed-off-by: Felipe Balbi <balbi@ti.com>
+---
+ drivers/usb/gadget/udc-core.c |    2 +-
+ 1 files changed, 1 insertions(+), 1 deletions(-)
+
+diff --git a/drivers/usb/gadget/udc-core.c b/drivers/usb/gadget/udc-core.c
+index 3ea783d..4e2e13e 100644
+--- a/drivers/usb/gadget/udc-core.c
++++ b/drivers/usb/gadget/udc-core.c
+@@ -211,8 +211,8 @@ static void usb_gadget_remove_driver(struct usb_udc *udc)
+       if (udc_is_newstyle(udc)) {
+               udc->driver->disconnect(udc->gadget);
+-              udc->driver->unbind(udc->gadget);
+               usb_gadget_disconnect(udc->gadget);
++              udc->driver->unbind(udc->gadget);
+               usb_gadget_udc_stop(udc->gadget, udc->driver);
+       } else {
+               usb_gadget_stop(udc->gadget, udc->driver);
+-- 
+1.7.7.6
+
index 888c7a3ddd0a8554b2e22ff376bd0fc4baab6bbf..82fa5ebebf96ae3da2473a67ee1779b5b00b11ac 100644 (file)
@@ -12,7 +12,7 @@ MULTI_CONFIG_BASE_SUFFIX = ""
 
 BRANCH = "v3.2-staging"
 SRCREV = "720e07b4c1f687b61b147b31c698cb6816d72f01"
-MACHINE_KERNEL_PR_append = "m+gitr${SRCREV}"
+MACHINE_KERNEL_PR_append = "n+gitr${SRCREV}"
 
 COMPATIBLE_MACHINE = "(ti33x)"
 
@@ -29,6 +29,12 @@ do_compile_prepend() {
 }
 
 PATCHES_OVER_PSP = " \
+       file://usb/0001-usb-musb-cppi41-revisit-the-teardown-path-to-fix-iso.patch \
+       file://usb/0002-usb-musb-fix-bug-in-data-toggle-sw-workaround.patch \
+       file://usb/0003-usb-gadget-udc-core-stop-UDC-on-device-initiated-dis.patch \
+       file://usb/0004-usb-gadget-udc-core-fix-asymmetric-calls-in-remove_d.patch \
+       file://usb/0005-usb-gadget-udc-core-fix-wrong-call-order.patch \
+       file://usb/0006-usb-gadget-udc-core-fix-incompatibility-with-dummy-h.patch \
        file://3.2.1/0001-MAINTAINERS-stable-Update-address.patch \
        file://3.2.1/0002-Documentation-Update-stable-address.patch \
        file://3.2.1/0003-firmware-Fix-an-oops-on-reading-fw_priv-fw-in-sysfs-.patch \