summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 35be5df)
raw | patch | inline | side by side (parent: 35be5df)
author | Denys Dmytriyenko <denys@ti.com> | |
Fri, 26 Apr 2013 19:55:47 +0000 (15:55 -0400) | ||
committer | Denys Dmytriyenko <denys@ti.com> | |
Fri, 26 Apr 2013 19:55:47 +0000 (15:55 -0400) |
Also, remove do_deploy_append() fix, as it's in oe-core now.
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
recipes-kernel/linux/linux-ti-staging_3.8.bb | patch | blob | history |
diff --git a/recipes-kernel/linux/linux-ti-staging_3.8.bb b/recipes-kernel/linux/linux-ti-staging_3.8.bb
index 622fa3e901f0f102b863e8417fc10afaf33b9f60..6fe52e292bf856dadcef46ae1e8b67b24608ab38 100644 (file)
inherit kernel
inherit kernel
-# This function must be here BEFORE the require of linux-dtb.inc below.
-# There is a "bug" in the base kernel.bbclass that after it's do_deploy
-# step it does not return back to the ${S} directory but stays in the
-# DEPLOY_DIR. However, the do_deploy_append defined in linux-dtb.inc
-# assumes that it is being run in the ${S} directory. A patch is
-# being submitted to fix this issue by either changing the do_deploy
-# in the kernel.bbclass to do "cd -" as the last step or to add
-# "cd ${S}" as the first line of do_deploy in linux-dtb.inc and this
-# function can be removed once that change is available.
-# If the function is not placed BEFORE the require then the change
-# directory is not appended before the linux-dtb.inc changes.
-do_deploy_append() {
- cd ${S}
-}
-
require recipes-kernel/linux/linux-dtb.inc
require recipes-kernel/linux/setup-defconfig.inc
require recipes-kernel/linux/linux-dtb.inc
require recipes-kernel/linux/setup-defconfig.inc
BRANCH = "ti-linux-3.8.y"
BRANCH = "ti-linux-3.8.y"
-SRCREV = "1de3616c36710b6949844738f9c63b96e307c49f"
+# This commit corresponds to ti2013.04.00 release tag
+SRCREV = "23e7f725a6af4ca44660c06bc3569f6ce705d1d0"
PV = "3.8.8"
# Append to the MACHINE_KERNEL_PR so that a new SRCREV will cause a rebuild
PV = "3.8.8"
# Append to the MACHINE_KERNEL_PR so that a new SRCREV will cause a rebuild
-MACHINE_KERNEL_PR_append = "a+gitr${SRCPV}"
+MACHINE_KERNEL_PR_append = "b+gitr${SRCPV}"
SRC_URI = "git://git.ti.com/ti-linux-kernel/ti-linux-kernel.git;protocol=git;branch=${BRANCH} \
file://defconfig \
SRC_URI = "git://git.ti.com/ti-linux-kernel/ti-linux-kernel.git;protocol=git;branch=${BRANCH} \
file://defconfig \