summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 37e525b)
raw | patch | inline | side by side (parent: 37e525b)
author | Franklin S. Cooper Jr <fcooper@ti.com> | |
Fri, 16 Nov 2012 19:19:41 +0000 (13:19 -0600) | ||
committer | Denys Dmytriyenko <denys@ti.com> | |
Fri, 16 Nov 2012 20:02:39 +0000 (15:02 -0500) |
* Non X11 base distros are unable to build this Graphics SDK.
* This patch tweaks the libgles-omap3 include file to always build the
Graphics SDK in Raw mode and also build in X11 mode only if X11 is
a part of the DISTRO_FEATURE. Components are built, installed and packaged
based on which mode the Graphics SDK is built in.
* Create a new variable PVR_INIT that is by default set to pvrsrvinit. This is
needed for newer version of the Graphics SDK that replaced this file.
Signed-off-by: Franklin S. Cooper Jr <fcooper@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
* This patch tweaks the libgles-omap3 include file to always build the
Graphics SDK in Raw mode and also build in X11 mode only if X11 is
a part of the DISTRO_FEATURE. Components are built, installed and packaged
based on which mode the Graphics SDK is built in.
* Create a new variable PVR_INIT that is by default set to pvrsrvinit. This is
needed for newer version of the Graphics SDK that replaced this file.
Signed-off-by: Franklin S. Cooper Jr <fcooper@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
recipes-graphics/libgles/libgles-omap3.inc | patch | blob | history |
diff --git a/recipes-graphics/libgles/libgles-omap3.inc b/recipes-graphics/libgles/libgles-omap3.inc
index db0d1cb1ce63526b4ae17b111b7eaacee18ef3a6..599070d4d0003850df2cf499e030092f025f079d 100644 (file)
# 'TSPA.txt' might not be the best file to md5sum
LIC_FILES_CHKSUM = "file://TSPA.txt;md5=c0d5d9c1e38b41677144c4e24d6ddee1"
-PR = "r33"
+PR = "r34"
COMPATIBLE_MACHINE = "(omap3|ti814x|ti816x|ti33x)"
-DEPENDS = "virtual/libx11 libxau libxdmcp libdrm"
+X11DEPENDS = "virtual/libx11 libxau libxdmcp libdrm"
+DEPENDS = "${@base_contains('DISTRO_FEATURES', 'x11', '${X11DEPENDS}', '', d)}"
+
+export SUPPORT_XORG ?= "${@base_contains('DISTRO_FEATURES', 'x11', '1', '0', d)}"
+PVR_INIT ?= "pvrsrvinit"
PROVIDES += "virtual/egl virtual/libgles1 virtual/libgles2"
export ES6LOCATION ?= "${S}/gfx_rel_es6.x"
export ES8LOCATION ?= "${S}/gfx_rel_es8.x"
+LIBGLESWINDOWSYSTEM ?= "libpvrPVR2D_FRONTWSEGL.so.1"
+
do_configure() {
# Attempt to fix up the worst offenders for file permissions
for i in $(find ${S} -name "*.h") $(find ${S} -name "*.c") $(find ${S} -name "Make*") ; do
chmod 0644 $i
- done
+ done
# Attempt to create proper library softlinks
for sofile in $(find ${S} -name "lib*Open*.so") $(find ${S} -name "lib*srv*.so") $(find ${S} -name "lib*gl*.so") $(find ${S} -name "libpvr*.so") $(find ${S} -name "lib*GL*.so"); do
PLATFORM ?= "LinuxOMAP3"
do_compile() {
- export X11ROOT="${STAGING_DIR_HOST}/usr"
export TOOLCHAIN="${TOOLCHAIN_PATH}"
-
export PLAT_CC="${CC}"
export PLAT_CPP="${CXX}"
export PLAR_AR="${AR}"
+ if [ ${SUPPORT_XORG} -eq 1 ] ; then
+ export X11ROOT="${STAGING_DIR_HOST}/usr"
+ mkdir -p ${S}/demos/x11
+ mkdir -p ${S}/trainingcourses/x11
+ fi
+
mkdir -p ${S}/demos/raw
- mkdir -p ${S}/demos/x11
+ mkdir -p ${S}/trainingcourses/raw
- # Rebuild demos for both Raw and X11
+ # Rebuild demos
for X11BUILD in 0 1 ; do
+ # Don't rebuild demos with X11 support for a non X11 distro
+ if [ ${SUPPORT_XORG} -eq 0 -a $X11BUILD -eq 1 ] ; then
+ continue
+ fi
+
for demo in ${S}/GFX_Linux_SDK/OGLES/SDKPackage/Demos/* ; do
cd $demo/OGLES/Build/LinuxGeneric
oe_runmake Common=1 PLATFORM=${PLATFORM} X11BUILD=$X11BUILD
rm $demo/OGLES/Build/${PLATFORM}/Release*/*.o
- install -m 0755 $demo/OGLES/Build/${PLATFORM}/ReleaseX11/* ${S}/demos/x11 || true
- sed -e s:NAME:$(basename $demo): \
- -e s:EXEC:${bindir}/SGX/demos/X11/$(basename $demo/OGLES/Build/${PLATFORM}/ReleaseX11/*): \
- ${WORKDIR}/sample.desktop > ${WORKDIR}/$(basename $demo).desktop
- install -m 0755 $demo/OGLES/Build/${PLATFORM}/ReleaseRaw/* ${S}/demos/raw || true
+
+ if [ $X11BUILD -eq 1 ] ; then
+ install -m 0755 $demo/OGLES/Build/${PLATFORM}/ReleaseX11/* ${S}/demos/x11 || true
+ sed -e s:NAME:$(basename $demo): \
+ -e s:EXEC:${bindir}/SGX/demos/X11/$(basename $demo/OGLES/Build/${PLATFORM}/ReleaseX11/*): \
+ ${WORKDIR}/sample.desktop > ${WORKDIR}/$(basename $demo).desktop
+ else
+ install -m 0755 $demo/OGLES/Build/${PLATFORM}/ReleaseRaw/* ${S}/demos/raw || true
+ fi
done
+
for demo in ${S}/GFX_Linux_SDK/OGLES2/SDKPackage/Demos/* ; do
cd $demo/OGLES2/Build/LinuxGeneric
oe_runmake Common=1 PLATFORM=${PLATFORM} X11BUILD=$X11BUILD
rm -f $demo/OGLES2/Build/${PLATFORM}/Release*/*.o
- install -m 0755 $demo/OGLES2/Build/${PLATFORM}/ReleaseX11/* ${S}/demos/x11 || true
- sed -e s:NAME:$(basename $demo): \
- -e s:EXEC:${bindir}/SGX/demos/X11/$(basename $demo/OGLES2/Build/${PLATFORM}/ReleaseX11/*): \
- ${WORKDIR}/sample.desktop > ${WORKDIR}/$(basename $demo).desktop
- install -m 0755 $demo/OGLES2/Build/${PLATFORM}/ReleaseRaw/* ${S}/demos/raw || true
+
+ if [ $X11BUILD -eq 1 ] ; then
+ install -m 0755 $demo/OGLES2/Build/${PLATFORM}/ReleaseX11/* ${S}/demos/x11 || true
+ sed -e s:NAME:$(basename $demo): \
+ -e s:EXEC:${bindir}/SGX/demos/X11/$(basename $demo/OGLES2/Build/${PLATFORM}/ReleaseX11/*): \
+ ${WORKDIR}/sample.desktop > ${WORKDIR}/$(basename $demo).desktop
+ else
+ install -m 0755 $demo/OGLES2/Build/${PLATFORM}/ReleaseRaw/* ${S}/demos/raw || true
+ fi
done
done
- mkdir -p ${S}/trainingcourses/raw
- mkdir -p ${S}/trainingcourses/x11
-
find ${S} -name "*_org" -delete
- # Build OGLES2 Trainingcourses for both Raw and X11
+ # Build OGLES2 Trainingcourses
for X11BUILD in 0 1 ; do
+ # Don't rebuild training courses with X11 support for a non X11 distro
+ if [ ${SUPPORT_XORG} -eq 0 -a $X11BUILD -eq 1 ] ; then
+ continue
+ fi
+
for training in ${S}/GFX_Linux_SDK/OGLES2/SDKPackage/TrainingCourse/* ; do
if [ -e $training/OGLES2/Build/LinuxGeneric/Makefile ] ; then
cd $training/OGLES2/Build/LinuxGeneric
if [ -e $training/OGLES2/Build/${PLATFORM}/Makefile ] ; then
cd $training/OGLES2/Build/${PLATFORM}
- fi
+ fi
oe_runmake Common=1 PLATFORM=${PLATFORM} X11BUILD=$X11BUILD
rm -f $training/OGLES2/Build/${PLATFORM}/Release*/*.o
- install -m 0755 $training/OGLES2/Build/${PLATFORM}/ReleaseX11/* ${S}/trainingcourses/x11 || true
- install -m 0755 $training/OGLES2/Build/${PLATFORM}/ReleaseRaw/* ${S}/trainingcourses/raw || true
+
+ if [ $X11BUILD -eq 1 ] ; then
+ install -m 0755 $training/OGLES2/Build/${PLATFORM}/ReleaseX11/* ${S}/trainingcourses/x11 || true
+ else
+ install -m 0755 $training/OGLES2/Build/${PLATFORM}/ReleaseRaw/* ${S}/trainingcourses/raw || true
+ fi
done
done
install -m 0755 ${BINLOCATION}/*_test ${D}${bindir}/
install -m 0755 ${BINLOCATION}/gl* ${D}${bindir}/
- install -m 0755 ${BINLOCATION}/pvrsrvinit ${D}${bindir}/
+ install -m 0755 ${BINLOCATION}/${PVR_INIT} ${D}${bindir}/
- install -m 0755 ${BINLOCATION}/xgles1test1 ${D}${bindir}/
-
- install -m 0755 ${BINLOCATION}/freedesktop/kdrive/usr/X11R6_SGX/bin/Xsgx ${D}${bindir}/|| true
- cp -pPR ${S}/GFX_Linux_SDK/OGLES2/SDKPackage/Builds/OGLES2/${PLATFORM}/lib/*X11WS* ${D}${libdir} || true
+ if [ ${SUPPORT_XORG} -eq 1 ] ; then
+ install -m 0755 ${BINLOCATION}/xgles1test1 ${D}${bindir}/
+ install -m 0755 ${BINLOCATION}/freedesktop/kdrive/usr/X11R6_SGX/bin/Xsgx ${D}${bindir}/|| true
+ cp -pPR ${S}/GFX_Linux_SDK/OGLES2/SDKPackage/Builds/OGLES2/${PLATFORM}/lib/*X11WS* ${D}${libdir} || true
+ fi
install -d ${D}${includedir}
cp -pPR ${S}/GFX_Linux_KM/include4 ${D}${includedir}/
install -d ${D}${sysconfdir}
echo "[default]" > ${D}${sysconfdir}/powervr.ini
- echo "WindowSystem=libpvrPVR2D_FRONTWSEGL.so.1" >> ${D}${sysconfdir}/powervr.ini
+ echo "WindowSystem=${LIBGLESWINDOWSYSTEM}" >> ${D}${sysconfdir}/powervr.ini
# The ES2.x, ES3.x, ES5.x and ES6.x CPUs have different SGX hardware, so we need to install multiple sets of userspace
install -d ${D}${bindir}/ES3.0
install -d ${D}${bindir}/ES2.0
+ shared_prog="eglinfo pvr2d_test ${PVR_INIT} services_test sgx_blit_test sgx_clipblit_test sgx_flip_test sgx_init_test sgx_render_flip_test"
+ raw_prog="gles1test1 gles2test1 ovg_unit_test"
+ x11_prog="eglinfo_x xgles1test1 xgles2test1 xmultiegltest xovg_unit_test"
+
for esrev in 2 3 5 6 8 ; do
ESLOCATION=$(eval echo $(echo \$\{ES${esrev}LOCATION\}))
if [ -e ${ESLOCATION} ] ; then
cp -pPR ${ESLOCATION}/lib*${IMGPV} ${ESLOCATION}/pvr_drv.so ${ESLOCATION}/*.a ${D}${libdir}/ES${esrev}.0/
- for esprog in eglinfo eglinfo_x gles1test1 gles2test1 ovg_unit_test pvr2d_test pvrsrvinit services_test sgx_blit_test sgx_clipblit_test sgx_flip_test sgx_init_test sgx_render_flip_test xgles1test1 xgles2test1 xmultiegltest xovg_unit_test ; do
+ for esprog in $shared_prog $raw_prog ${@base_contains('DISTRO_FEATURES', 'x11',"$x11_prog","",d)} ; do
install -m 0755 ${ESLOCATION}/$esprog ${D}${bindir}/ES${esrev}.0/ || true
done
fi
cp ${WORKDIR}/*.desktop ${D}${prefix}/share/applications
rm ${D}${prefix}/share/applications/sample.desktop
- install -d ${D}${bindir}/SGX/demos/X11/
+ if [ ${SUPPORT_XORG} -eq 1 ] ; then
+ install -d ${D}${bindir}/SGX/demos/X11/
+ install -m 0755 ${S}/demos/x11/* ${D}${bindir}/SGX/demos/X11/
+ install -d ${D}${bindir}/SGX/trainingcourses/X11
+ install -m 0755 ${S}/trainingcourses/x11/* ${D}${bindir}/SGX/trainingcourses/X11/
+ fi
+
install -d ${D}${bindir}/SGX/demos/Raw/
- install -m 0755 ${S}/demos/x11/* ${D}${bindir}/SGX/demos/X11/
install -m 0755 ${S}/demos/raw/* ${D}${bindir}/SGX/demos/Raw/
-
install -d ${D}${bindir}/SGX/trainingcourses/Raw
- install -d ${D}${bindir}/SGX/trainingcourses/X11
- install -m 0755 ${S}/trainingcourses/x11/* ${D}${bindir}/SGX/trainingcourses/X11/
install -m 0755 ${S}/trainingcourses/raw/* ${D}${bindir}/SGX/trainingcourses/Raw/
+
# Delete objects and linker scripts hidden between the headers
find ${D} -name "*.o" -delete
find ${D} -name "*.o.cmd" -delete
}
-PACKAGES =+ "${PN}-rawdemos \
- ${PN}-x11demos \
- ${PN}-rawtrainingcourses \
- ${PN}-x11trainingcourses \
-"
-
-PACKAGES += "xserver-kdrive-powervrsgx \
- ${PN}-tests "
-
+PACKAGES =+ "${@base_contains('DISTRO_FEATURES', 'x11',"${PN}-x11demos ${PN}-x11trainingcourses xserver-kdrive-powervrsgx" ,"", d)} \
+ ${PN}-rawdemos ${PN}-rawtrainingcourses ${PN}-tests"
# Package the base libraries per silicon revision
PACKAGES =+ "${PN}-es2 ${PN}-es3 ${PN}-es5 ${PN}-es6 ${PN}-es8"
RRECOMMENDS_${PN} += "${PN}-es2 ${PN}-es3 ${PN}-es5 ${PN}-es6 ${PN}-es8"
@@ -238,7 +269,9 @@ PRIVATE_LIBS_${PN}-es5 = "libGLESv2.so libIMGegl.so libsrv_um.so libOpenVG.so li
PRIVATE_LIBS_${PN}-es6 = "libGLESv2.so libIMGegl.so libsrv_um.so libOpenVG.so libpvr2d.so libsrv_init.so libEGL.so libsrv_um_dri.so libOpenVGU.so libglslcompiler.so libGLES_CM.so"
PRIVATE_LIBS_${PN}-es8 = "libGLESv2.so libIMGegl.so libsrv_um.so libOpenVG.so libpvr2d.so libsrv_init.so libEGL.so libsrv_um_dri.so libOpenVGU.so libglslcompiler.so libGLES_CM.so"
-PACKAGES =+ "${PN}-blitwsegl ${PN}-flipwsegl ${PN}-frontwsegl ${PN}-linuxfbwsegl ${PN}-x11wsegl ${PN}-driwsegl"
+
+PACKAGES =+ "${PN}-blitwsegl ${PN}-flipwsegl ${PN}-frontwsegl ${PN}-linuxfbwsegl"
+PACKAGES =+ "${@base_contains('DISTRO_FEATURES', 'x11',"${PN}-x11wsegl ${PN}-driwsegl" ,"", d)}"
FILES_${PN}-blitwsegl = "${libdir}/libpvrPVR2D_BLITWSEGL.so.*"
FILES_${PN}-flipwsegl = "${libdir}/libpvrPVR2D_FLIPWSEGL.so.*"
FILES_${PN}-frontwsegl = "${libdir}/libpvrPVR2D_FRONTWSEGL.so.*"
FILES_${PN}-x11wsegl = "${libdir}/libpvrPVR2D_X11WSEGL.so* ${bindir}/x* ${bindir}/*x"
FILES_${PN}-driwsegl = "${libdir}/libpvrPVR2D_DRIWSEGL.so* ${libdir}/libsrv_um_dri*"
-PACKAGES =+ "${PN}-blitwsegl-es2 ${PN}-blitwsegl-es3 ${PN}-blitwsegl-es5 ${PN}-blitwsegl-es6 ${PN}-blitwsegl-es8 ${PN}-flipwsegl-es2 ${PN}-flipwsegl-es3 ${PN}-flipwsegl-es5 ${PN}-flipwsegl-es6 ${PN}-flipwsegl-es8 ${PN}-frontwsegl-es2 ${PN}-frontwsegl-es3 ${PN}-frontwsegl-es5 ${PN}-frontwsegl-es6 ${PN}-frontwsegl-es8 ${PN}-linuxfbwsegl-es2 ${PN}-linuxfbwsegl-es3 ${PN}-linuxfbwsegl-es5 ${PN}-linuxfbwsegl-es6 ${PN}-linuxfbwsegl-es8 ${PN}-x11wsegl-es2 ${PN}-x11wsegl-es3 ${PN}-x11wsegl-es5 ${PN}-x11wsegl-es6 ${PN}-x11wsegl-es8 ${PN}-driwsegl-es2 ${PN}-driwsegl-es3 ${PN}-driwsegl-es5 ${PN}-driwsegl-es6 ${PN}-driwsegl-es8"
+PACKAGES =+ "${PN}-blitwsegl-es2 ${PN}-blitwsegl-es3 ${PN}-blitwsegl-es5 ${PN}-blitwsegl-es6 ${PN}-blitwsegl-es8 ${PN}-flipwsegl-es2 ${PN}-flipwsegl-es3 ${PN}-flipwsegl-es5 ${PN}-flipwsegl-es6 ${PN}-flipwsegl-es8 ${PN}-frontwsegl-es2 ${PN}-frontwsegl-es3 ${PN}-frontwsegl-es5 ${PN}-frontwsegl-es6 ${PN}-frontwsegl-es8 ${PN}-linuxfbwsegl-es2 ${PN}-linuxfbwsegl-es3 ${PN}-linuxfbwsegl-es5 ${PN}-linuxfbwsegl-es6 ${PN}-linuxfbwsegl-es8"
+
+X11_SEGL = " ${PN}-x11wsegl-es2 ${PN}-x11wsegl-es3 ${PN}-x11wsegl-es5 ${PN}-x11wsegl-es6 ${PN}-x11wsegl-es8 ${PN}-driwsegl-es2 ${PN}-driwsegl-es3 ${PN}-driwsegl-es5 ${PN}-driwsegl-es6 ${PN}-driwsegl-es8 "
+PACKAGES =+ "${@base_contains('DISTRO_FEATURES', 'x11',"${X11_SEGL}" ,"", d)}"
FILES_${PN}-blitwsegl-es2 = "${libdir}/ES2*/libpvrPVR2D_BLITWSEGL.so.*"
FILES_${PN}-blitwsegl-es3 = "${libdir}/ES3*/libpvrPVR2D_BLITWSEGL.so.*"
FILES_${PN}-blitwsegl-es5 = "${libdir}/ES5*/libpvrPVR2D_BLITWSEGL.so.*"
@@ -291,7 +327,7 @@ RRECOMMENDS_${PN}-driwsegl = " ${PN}-driwsegl-es2 ${PN}-driwsegl-es3 ${PN}-driws
CONFFILES_${PN} = "${sysconfdir}/powervr.ini"
-FILES_${PN} = "${sysconfdir} ${libdir}/*.so* ${bindir}/pvrsrvinit ${bindir}/cputype ${bindir}/*"
+FILES_${PN} = "${sysconfdir} ${libdir}/*.so* ${bindir}/${PVR_INIT} ${bindir}/cputype ${bindir}/*"
FILES_xserver-kdrive-powervrsgx = "${bindir}/Xsgx"
FILES_${PN}-tests = "${bindir}/*test*"
pkg_postinst_${PN}_append() {
rm -f $D${sysconfdir}/powervr-esrev
-ln -sf /usr/lib/libXdmcp.so.6.0.0 /usr/lib/libXdmcp.so.0
-ln -sf /usr/lib/libXau.so.6.0.0 /usr/lib/libXau.so.0
+if [ ${SUPPORT_XORG} -eq 1 ] ; then
+ ln -sf /usr/lib/libXdmcp.so.6.0.0 /usr/lib/libXdmcp.so.0
+ ln -sf /usr/lib/libXau.so.6.0.0 /usr/lib/libXau.so.0
+fi
+
}
pkg_postinst_${PN}-blitwsegl() {