u-boot 2011.10rc: update SRCREV and rediff patches
authorKoen Kooi <koen@dominion.thruhere.net>
Tue, 1 Nov 2011 11:40:44 +0000 (12:40 +0100)
committerKoen Kooi <koen@dominion.thruhere.net>
Tue, 1 Nov 2011 11:40:44 +0000 (12:40 +0100)
Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
recipes-bsp/u-boot/u-boot/2011.09git/0001-am335x_evm-only-do-in-kernel-dhcp-when-using-NFS-use.patch [new file with mode: 0644]
recipes-bsp/u-boot/u-boot/2011.09git/0001-mach-types-Add-new-beaglebone-machine-type.patch [deleted file]
recipes-bsp/u-boot/u-boot/2011.09git/0002-am335x_evm-boot-kernel-from-boot-in-ext2-3-filesyste.patch [moved from recipes-bsp/u-boot/u-boot/2011.09git/0001-am335x_evm-boot-kernel-from-ext2-3-filesystem.patch with 74% similarity]
recipes-bsp/u-boot/u-boot/2011.09git/0002-evm-If-beaglebone-is-detected-pass-the-MACH_TYPE_BEA.patch [deleted file]
recipes-bsp/u-boot/u-boot/2011.09git/0003-am335x_evm-set-bootdelay-to-1.patch [moved from recipes-bsp/u-boot/u-boot/2011.09git/0002-am335x_evm-set-bootdelay-to-0.patch with 75% similarity]
recipes-bsp/u-boot/u-boot/2011.09git/0003-am335x_evm-single-byte-address-EEPROM-for-board-iden.patch [deleted file]
recipes-bsp/u-boot/u-boot/2011.09git/0004-am335x-evm-fall-back-to-bone-if-header.config-is-emp.patch [deleted file]
recipes-bsp/u-boot/u-boot/2011.09git/0004-am335x-evm-make-MMC-rootfs-RO-on-boot-so-fsck-works.patch [moved from recipes-bsp/u-boot/u-boot/2011.09git/0003-am335x-evm-make-rootfs-RO-on-boot.patch with 74% similarity]
recipes-bsp/u-boot/u-boot/2011.09git/0005-am335x-evm-Read-name-field-in-EEPROM-header-for-Beag.patch [deleted file]
recipes-bsp/u-boot/u-boot_2011.10rc.bb

diff --git a/recipes-bsp/u-boot/u-boot/2011.09git/0001-am335x_evm-only-do-in-kernel-dhcp-when-using-NFS-use.patch b/recipes-bsp/u-boot/u-boot/2011.09git/0001-am335x_evm-only-do-in-kernel-dhcp-when-using-NFS-use.patch
new file mode 100644 (file)
index 0000000..1ccfe19
--- /dev/null
@@ -0,0 +1,35 @@
+From 557a773eb245f3f2508e40d6d8a6c593738fd46f Mon Sep 17 00:00:00 2001
+From: Koen Kooi <koen@dominion.thruhere.net>
+Date: Tue, 1 Nov 2011 12:19:54 +0100
+Subject: [PATCH 1/4] am335x_evm: only do in-kernel dhcp when using NFS, userspace will do dhcp otherwise
+
+Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
+---
+ include/configs/am335x_evm.h |    4 ++--
+ 1 files changed, 2 insertions(+), 2 deletions(-)
+
+diff --git a/include/configs/am335x_evm.h b/include/configs/am335x_evm.h
+index 41a3316..93b3161 100755
+--- a/include/configs/am335x_evm.h
++++ b/include/configs/am335x_evm.h
+@@ -69,7 +69,7 @@
+       "nfsopts=nolock\0" \
+       "static_ip=${ipaddr}:${serverip}:${gatewayip}:${netmask}:${hostname}" \
+                       "::off\0" \
+-      "ip_method=dhcp\0" \
++      "ip_method=none\0" \
+       "bootenv=uEnv.txt\0" \
+       "loadbootenv=fatload mmc ${mmc_dev} ${loadaddr} ${bootenv}\0" \
+       "importbootenv=echo Importing environment from mmc ...; " \
+@@ -99,7 +99,7 @@
+               "setenv bootargs ${bootargs} " \
+               "root=/dev/nfs " \
+               "nfsroot=${serverip}:${rootpath},${nfsopts} rw " \
+-              "ip=${ip_method}\0" \
++              "ip=dhcp\0" \
+       "mmc_boot=run mmc_args; " \
+               "run mmc_load_uimage; " \
+               "bootm ${loadaddr}\0" \
+-- 
+1.7.2.5
+
diff --git a/recipes-bsp/u-boot/u-boot/2011.09git/0001-mach-types-Add-new-beaglebone-machine-type.patch b/recipes-bsp/u-boot/u-boot/2011.09git/0001-mach-types-Add-new-beaglebone-machine-type.patch
deleted file mode 100644 (file)
index 6f12d6c..0000000
+++ /dev/null
@@ -1,47 +0,0 @@
-From ec41c3f94a9a498d1f7061abd98e41a66c0ab13e Mon Sep 17 00:00:00 2001
-From: Steve Kipisz <s-kipisz2@ti.com>
-Date: Thu, 13 Oct 2011 14:42:35 -0500
-Subject: [PATCH 1/4] mach-types: Add new beaglebone machine type.
-
-* New machine type is 3808
-
-Signed-off-by: Steve Kipisz <s-kipisz2@ti.com>
-Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
----
- arch/arm/include/asm/mach-types.h |   13 +++++++++++++
- 1 files changed, 13 insertions(+), 0 deletions(-)
-
-diff --git a/arch/arm/include/asm/mach-types.h b/arch/arm/include/asm/mach-types.h
-index c6ea523..68ac2ba 100644
---- a/arch/arm/include/asm/mach-types.h
-+++ b/arch/arm/include/asm/mach-types.h
-@@ -3314,6 +3314,7 @@ extern unsigned int __machine_arch_type;
- #define MACH_TYPE_GOFLEXHOME           3338
- #define MACH_TYPE_TIAM335EVM           3589
- #define MACH_TYPE_TIAM335IAEVM         3684
-+#define MACH_TYPE_BEAGLEBONE           3808
- #ifdef CONFIG_ARCH_EBSA110
- # ifdef machine_arch_type
-@@ -42927,6 +42928,18 @@ extern unsigned int __machine_arch_type;
- # define machine_is_tiam335evm() (0)
- #endif
-+#ifdef CONFIG_MACH_BEAGLEBONE
-+# ifdef machine_arch_type
-+#  undef machine_arch_type
-+#  define machine_arch_type     __machine_arch_type
-+# else
-+#  define machine_arch_type     MACH_TYPE_BEAGLEBONE
-+# endif
-+# define machine_is_beaglebone() (machine_arch_type == MACH_TYPE_BEAGLEBONE)
-+#else
-+# define machine_is_beaglebone() (0)
-+#endif
-+
- /*
-  * These have not yet been registered
-  */
--- 
-1.6.6.1
-
similarity index 74%
rename from recipes-bsp/u-boot/u-boot/2011.09git/0001-am335x_evm-boot-kernel-from-ext2-3-filesystem.patch
rename to recipes-bsp/u-boot/u-boot/2011.09git/0002-am335x_evm-boot-kernel-from-boot-in-ext2-3-filesyste.patch
index 1ed68ea89b4704f86529253ed0bb206306b0340e..612ac981f5177275537486b217baf4ba9d979943 100644 (file)
@@ -1,7 +1,7 @@
-From 30c5198d37863d4f1598f7fe2b8f690b6cf6ae53 Mon Sep 17 00:00:00 2001
+From 206baf5d1d8eb19312c0c8216e6722a63548573d Mon Sep 17 00:00:00 2001
 From: Koen Kooi <koen@dominion.thruhere.net>
-Date: Thu, 13 Oct 2011 12:15:25 +0200
-Subject: [PATCH 1/2] am335x_evm: boot kernel from ext2/3 filesystem
+Date: Tue, 1 Nov 2011 12:21:07 +0100
+Subject: [PATCH 2/4] am335x_evm: boot kernel from /boot in ext2/3 filesystem
 
 Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
 ---
@@ -9,7 +9,7 @@ Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
  1 files changed, 2 insertions(+), 1 deletions(-)
 
 diff --git a/include/configs/am335x_evm.h b/include/configs/am335x_evm.h
-index f1cc2b2..9ce360d 100755
+index 93b3161..9bbfe3b 100755
 --- a/include/configs/am335x_evm.h
 +++ b/include/configs/am335x_evm.h
 @@ -74,7 +74,8 @@
@@ -19,9 +19,9 @@ index f1cc2b2..9ce360d 100755
 -      "mmc_load_uimage=fatload mmc ${mmc_dev} ${loadaddr} ${bootfile}\0" \
 +      "mmc_load_uimage_fat=fatload mmc ${mmc_dev} ${loadaddr} ${bootfile}\0" \
 +      "mmc_load_uimage=ext2load mmc 0:2 ${loadaddr} /boot/${bootfile}\0" \
+       "optargs=\0" \
        "bootargs_defaults=setenv bootargs " \
-               "console=${console}\0" \
-       "mmc_args=run bootargs_defaults;" \
+               "console=${console} " \
 -- 
-1.6.6.1
+1.7.2.5
 
diff --git a/recipes-bsp/u-boot/u-boot/2011.09git/0002-evm-If-beaglebone-is-detected-pass-the-MACH_TYPE_BEA.patch b/recipes-bsp/u-boot/u-boot/2011.09git/0002-evm-If-beaglebone-is-detected-pass-the-MACH_TYPE_BEA.patch
deleted file mode 100644 (file)
index 7b8e52b..0000000
+++ /dev/null
@@ -1,29 +0,0 @@
-From 17c0530b1539fb8813efc11c60dd87fd9a3a074b Mon Sep 17 00:00:00 2001
-From: Steve Kipisz <s-kipisz2@ti.com>
-Date: Thu, 13 Oct 2011 16:31:26 -0500
-Subject: [PATCH 2/4] evm: If beaglebone is detected, pass the MACH_TYPE_BEAGLEBONE to Linux
-
-Signed-off-by: Steve Kipisz <s-kipisz2@ti.com>
-Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
----
- board/ti/am335x/evm.c |    4 +++-
- 1 files changed, 3 insertions(+), 1 deletions(-)
-
-diff --git a/board/ti/am335x/evm.c b/board/ti/am335x/evm.c
-index 95e790b..af34bfd 100755
---- a/board/ti/am335x/evm.c
-+++ b/board/ti/am335x/evm.c
-@@ -447,7 +447,9 @@ static void detect_daughter_board_profile(void)
- int board_evm_init(void)
- {
-       /* mach type passed to kernel */
--      if (board_id == IA_BOARD)
-+      if (board_id == BONE_BOARD)
-+              gd->bd->bi_arch_number = MACH_TYPE_BEAGLEBONE;
-+      else if (board_id == IA_BOARD)
-               gd->bd->bi_arch_number = MACH_TYPE_TIAM335IAEVM;
-       else
-               gd->bd->bi_arch_number = MACH_TYPE_TIAM335EVM;
--- 
-1.6.6.1
-
similarity index 75%
rename from recipes-bsp/u-boot/u-boot/2011.09git/0002-am335x_evm-set-bootdelay-to-0.patch
rename to recipes-bsp/u-boot/u-boot/2011.09git/0003-am335x_evm-set-bootdelay-to-1.patch
index 99b7cadc5b0169cc525643708ce91a87d803453c..3265540014da5b2a0393c1a82fa9504b09b833e2 100644 (file)
@@ -1,7 +1,7 @@
-From 481457db4fe870fcbab47fe29cb768daf235fd1f Mon Sep 17 00:00:00 2001
+From bf513a05bc37f6d32e14c1e46d090773d1664c99 Mon Sep 17 00:00:00 2001
 From: Koen Kooi <koen@dominion.thruhere.net>
-Date: Thu, 13 Oct 2011 12:17:27 +0200
-Subject: [PATCH 2/2] am335x_evm: set bootdelay to 1
+Date: Tue, 1 Nov 2011 12:21:38 +0100
+Subject: [PATCH 3/4] am335x_evm: set bootdelay to 1
 
 Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
 ---
@@ -9,7 +9,7 @@ Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
  1 files changed, 1 insertions(+), 1 deletions(-)
 
 diff --git a/include/configs/am335x_evm.h b/include/configs/am335x_evm.h
-index 9ce360d..78c823b 100755
+index 9bbfe3b..6143dc3 100755
 --- a/include/configs/am335x_evm.h
 +++ b/include/configs/am335x_evm.h
 @@ -38,7 +38,7 @@
@@ -22,5 +22,5 @@ index 9ce360d..78c823b 100755
  #define CONFIG_MMC
  #define CONFIG_NAND
 -- 
-1.6.6.1
+1.7.2.5
 
diff --git a/recipes-bsp/u-boot/u-boot/2011.09git/0003-am335x_evm-single-byte-address-EEPROM-for-board-iden.patch b/recipes-bsp/u-boot/u-boot/2011.09git/0003-am335x_evm-single-byte-address-EEPROM-for-board-iden.patch
deleted file mode 100644 (file)
index d4ea607..0000000
+++ /dev/null
@@ -1,46 +0,0 @@
-From 52165b34c2fbcfe93f4cfabb616c2feb3ea7344f Mon Sep 17 00:00:00 2001
-From: Jason Kridner <jdk@ti.com>
-Date: Thu, 13 Oct 2011 23:50:35 -0400
-Subject: [PATCH 3/4] am335x_evm: single-byte address EEPROM for board identifier
-
-The BeagleBone has an EEPROM that uses a single byte address instead of a
-2-byte address used by the EVM versions.  This simply adds a quick attempt
-at reading the board identifier header with a 1-byte address if the header
-signature isn't correct using a 2-byte address.
-
-This is only build tested.  Having a script to program the expected EEPROM
-contents would help me reduce my time to test this.
-
-Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
----
- board/ti/am335x/evm.c |   14 ++++++++++++--
- 1 files changed, 12 insertions(+), 2 deletions(-)
-
-diff --git a/board/ti/am335x/evm.c b/board/ti/am335x/evm.c
-index af34bfd..f484a3c 100755
---- a/board/ti/am335x/evm.c
-+++ b/board/ti/am335x/evm.c
-@@ -496,8 +496,18 @@ int board_init(void)
-       }
-       if (header.magic != 0xEE3355AA) {
--              printf("Incorrect magic number in EEPROM\n");
--              goto err_out;
-+              /* read the eeprom using i2c again, but use only a 1 byte address */
-+              if (i2c_read(I2C_BASE_BOARD_ADDR, 0, 1, (uchar *)&header,
-+                                                              sizeof(header))) {
-+                      printf("Could not read the EEPROM; something fundamentally"
-+                              " wrong on the I2C bus.\n");
-+                      goto err_out;
-+              }
-+
-+              if (header.magic != 0xEE3355AA) {
-+                      printf("Incorrect magic number in EEPROM\n");
-+                      goto err_out;
-+              }
-       }
-       detect_daughter_board();
--- 
-1.6.6.1
-
diff --git a/recipes-bsp/u-boot/u-boot/2011.09git/0004-am335x-evm-fall-back-to-bone-if-header.config-is-emp.patch b/recipes-bsp/u-boot/u-boot/2011.09git/0004-am335x-evm-fall-back-to-bone-if-header.config-is-emp.patch
deleted file mode 100644 (file)
index db3ae69..0000000
+++ /dev/null
@@ -1,40 +0,0 @@
-From 3e3ac90cdd7fade62e898453f529364e4d9c7589 Mon Sep 17 00:00:00 2001
-From: Koen Kooi <koen@dominion.thruhere.net>
-Date: Tue, 18 Oct 2011 19:18:56 +0200
-Subject: [PATCH 4/4] am335x-evm: fall back to bone if header.config is empty
-
-Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
----
- board/ti/am335x/evm.c |    8 ++++----
- 1 files changed, 4 insertions(+), 4 deletions(-)
-
-diff --git a/board/ti/am335x/evm.c b/board/ti/am335x/evm.c
-index f484a3c..1c3ba2c 100755
---- a/board/ti/am335x/evm.c
-+++ b/board/ti/am335x/evm.c
-@@ -495,6 +495,7 @@ int board_init(void)
-               goto err_out;
-       }
-+      printf("EEPROM ID:\n magic: %#08x\n name: %8s\n version: %4s\n serial: %12s\n config: %32s\n mac_addr: %s\n", header.magic, header.name, header.version, header.serial, header.config, header.mac_addr);
-       if (header.magic != 0xEE3355AA) {
-               /* read the eeprom using i2c again, but use only a 1 byte address */
-               if (i2c_read(I2C_BASE_BOARD_ADDR, 0, 1, (uchar *)&header,
-@@ -522,11 +523,10 @@ int board_init(void)
-               board_id = IPP_BOARD;
-       } else {
-               printf("Did not find a recognized configuration, "
--                      "assuming General purpose EVM in Profile 0 with "
--                      "Daughter board\n");
--              board_id = GP_BOARD;
-+                      "assuming BeagleBone\n");
-+              board_id = BONE_BOARD;
-               profile = 1;    /* profile 0 is internally considered as 1 */
--              daughter_board_connected = 1;
-+              daughter_board_connected = 0;
-       }
-       configure_evm_pin_mux(board_id, profile, daughter_board_connected);
--- 
-1.6.6.1
-
similarity index 74%
rename from recipes-bsp/u-boot/u-boot/2011.09git/0003-am335x-evm-make-rootfs-RO-on-boot.patch
rename to recipes-bsp/u-boot/u-boot/2011.09git/0004-am335x-evm-make-MMC-rootfs-RO-on-boot-so-fsck-works.patch
index 4dc053e03a5fafaaf1d14aba9b1b21bf5dd71600..721955475404f0301b9eccf836fb014f14dd9f8f 100644 (file)
@@ -1,7 +1,7 @@
-From 9f8585887a08e6a9c7ca24c2a9c0e9a8c66a2a54 Mon Sep 17 00:00:00 2001
+From 63e5b3b4271917e0a3c5a4903a76fdfb30118d3c Mon Sep 17 00:00:00 2001
 From: Koen Kooi <koen@dominion.thruhere.net>
-Date: Sun, 16 Oct 2011 09:57:06 +0200
-Subject: [PATCH 3/3] am335x-evm: make rootfs RO on boot
+Date: Tue, 1 Nov 2011 12:22:30 +0100
+Subject: [PATCH 4/4] am335x-evm: make MMC rootfs RO on boot so fsck works
 
 Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
 ---
@@ -9,7 +9,7 @@ Signed-off-by: Koen Kooi <koen@dominion.thruhere.net>
  1 files changed, 1 insertions(+), 1 deletions(-)
 
 diff --git a/include/configs/am335x_evm.h b/include/configs/am335x_evm.h
-index cb45037..5db3d9f 100755
+index 6143dc3..56e36da 100755
 --- a/include/configs/am335x_evm.h
 +++ b/include/configs/am335x_evm.h
 @@ -50,7 +50,7 @@
@@ -22,5 +22,5 @@ index cb45037..5db3d9f 100755
        "spi_root=/dev/mtdblock4 rw\0" \
        "nor_root=/dev/mtdblock3 rw\0" \
 -- 
-1.6.6.1
+1.7.2.5
 
diff --git a/recipes-bsp/u-boot/u-boot/2011.09git/0005-am335x-evm-Read-name-field-in-EEPROM-header-for-Beag.patch b/recipes-bsp/u-boot/u-boot/2011.09git/0005-am335x-evm-Read-name-field-in-EEPROM-header-for-Beag.patch
deleted file mode 100644 (file)
index ef901a9..0000000
+++ /dev/null
@@ -1,28 +0,0 @@
-From 186250ee6abca3f080b5321504a1c5881ffbf7c6 Mon Sep 17 00:00:00 2001
-From: Joel A Fernandes <joelagnel@ti.com>
-Date: Thu, 20 Oct 2011 19:46:53 -0500
-Subject: [PATCH] am335x-evm: Read name field in EEPROM header for BeagleBoard bone detection
-
-Signed-off-by: Joel A Fernandes <joelagnel@ti.com>
----
- board/ti/am335x/evm.c |    4 ++++
- 1 files changed, 4 insertions(+), 0 deletions(-)
-
-diff --git a/board/ti/am335x/evm.c b/board/ti/am335x/evm.c
-index 37e348f..b63dcbe 100755
---- a/board/ti/am335x/evm.c
-+++ b/board/ti/am335x/evm.c
-@@ -501,6 +501,10 @@ int board_init(void)
-               detect_daughter_board_profile();
-       } else if (!strncmp("SKU#03", header.config, 6)) {
-               board_id = IPP_BOARD;
-+      } else if (!strncmp("A335BONE", header.name, 8)) {
-+              board_id = BONE_BOARD;
-+              profile = 1;    /* profile 0 is internally considered as 1 */
-+              daughter_board_connected = 0;
-       } else {
-               printf("Did not find a recognized configuration, "
-                       "assuming BeagleBone\n");
--- 
-1.7.1
-
index ca7b670abd0fba97a51de6959561b7523ce042af..e4552b864461686a3c481ad165a9a6afef4f7bf0 100644 (file)
@@ -4,7 +4,7 @@ require u-boot.inc
 COMPATIBLE_MACHINE = "(ti33x)"
 DEFAULT_PREFERENCE_ti33x = "99"
 PV = "2011.09+git"
-PR = "r15"
+PR = "r16"
 
 # SPL build
 UBOOT_BINARY = "u-boot.img"
@@ -12,16 +12,13 @@ UBOOT_IMAGE = "u-boot-${MACHINE}-${PV}-${PR}.img"
 UBOOT_SYMLINK = "u-boot-${MACHINE}.img"
 
 SRC_URI = "git://arago-project.org/git/projects/u-boot-am33x.git;protocol=git;branch=int_am335xpsp_04.06.00.01-v2011.09-for-sdk-05.03.00.00 \
-           file://2011.09git/0001-am335x_evm-boot-kernel-from-ext2-3-filesystem.patch \
-           file://2011.09git/0002-am335x_evm-set-bootdelay-to-0.patch \
-           file://2011.09git/0003-am335x-evm-make-rootfs-RO-on-boot.patch \
-           file://2011.09git/0001-mach-types-Add-new-beaglebone-machine-type.patch \
-           file://2011.09git/0003-am335x_evm-single-byte-address-EEPROM-for-board-iden.patch \
-           file://2011.09git/0004-am335x-evm-fall-back-to-bone-if-header.config-is-emp.patch \
-           file://2011.09git/0005-am335x-evm-Read-name-field-in-EEPROM-header-for-Beag.patch \
+           file://2011.09git/0001-am335x_evm-only-do-in-kernel-dhcp-when-using-NFS-use.patch \
+           file://2011.09git/0002-am335x_evm-boot-kernel-from-boot-in-ext2-3-filesyste.patch \
+           file://2011.09git/0003-am335x_evm-set-bootdelay-to-1.patch \
+           file://2011.09git/0004-am335x-evm-make-MMC-rootfs-RO-on-boot-so-fsck-works.patch \
           "
 
-SRCREV = "9158d7f37d596b867039345cb2e3f8f18f54fe46"
+SRCREV = "f63b270e47f62f4d1a05b2001357e215966c6f5a"
 
 LIC_FILES_CHKSUM = "file://COPYING;md5=1707d6db1d42237583f50183a5651ecb"