summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 757c0e5)
raw | patch | inline | side by side (parent: 757c0e5)
author | Franklin S. Cooper Jr <fcooper@ti.com> | |
Tue, 12 Feb 2013 01:04:38 +0000 (19:04 -0600) | ||
committer | Denys Dmytriyenko <denys@ti.com> | |
Tue, 12 Feb 2013 23:13:47 +0000 (18:13 -0500) |
* Add latest patches to linux-omapl138 that were added since this recipe was
added to meta-ti.
* Update to latest am180x-evm defconfig
* Mimic the following commits from arago:
linux-davinci: update to add mmc patches
* Optimizations to reduce overhead on weak platforms
linux: disable DMA for MUSB
* For the am3517, am180x, and am335x devices the CPPI 4.1 DMA
should NOT be used for the MUSB controller. Using this DMA
can cause the controller to lockup.
* Updated the defconfigs to set the use of PIO mode
* Added a patch to updated the PIO mode description to make it
easier to determine when it can be used.
Signed-off-by: Franklin S. Cooper Jr <fcooper@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
added to meta-ti.
* Update to latest am180x-evm defconfig
* Mimic the following commits from arago:
linux-davinci: update to add mmc patches
* Optimizations to reduce overhead on weak platforms
linux: disable DMA for MUSB
* For the am3517, am180x, and am335x devices the CPPI 4.1 DMA
should NOT be used for the MUSB controller. Using this DMA
can cause the controller to lockup.
* Updated the defconfigs to set the use of PIO mode
* Added a patch to updated the PIO mode description to make it
easier to determine when it can be used.
Signed-off-by: Franklin S. Cooper Jr <fcooper@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
index 80198449dd6820cb4980b9a2a6a4acdaceea152f..71eca709ce343166574ce8e4a03a8fcc29e95f68 100644 (file)
require conf/machine/include/tune-arm926ejs.inc
# Increase this everytime you change something in the kernel
-MACHINE_KERNEL_PR = "r51"
+MACHINE_KERNEL_PR = "r52"
KERNEL_IMAGETYPE = "uImage"
diff --git a/recipes-kernel/linux/linux-omapl138-psp-2.6.37/0001-musb-update-PIO-mode-help-information-in-Kconfig.patch b/recipes-kernel/linux/linux-omapl138-psp-2.6.37/0001-musb-update-PIO-mode-help-information-in-Kconfig.patch
--- /dev/null
@@ -0,0 +1,44 @@
+From 10fbd32a96aedd644b6bf38888a2af64cc13a35f Mon Sep 17 00:00:00 2001
+From: Matt Porter <mporter@ti.com>
+Date: Mon, 5 Dec 2011 15:29:35 -0600
+Subject: [PATCH] musb: update PIO mode help information in Kconfig
+
+* Updated the Kconfig help information for the PIO mode for MUSB
+ to make it more clear to the customer when to select this option
+ and which devices currently have issues with this option.
+* This is in accordance with the findings for CPPI4.1 DMA usage
+ for MUSB
+
+Upstream-Status: Submitted
+ * Submitted to the PSP team using the lpr list
+
+Signed-off-by: Matt Porter <mporter@ti.com>
+Signed-off-by: Chase Maupin <Chase.Maupin@ti.com>
+---
+ drivers/usb/musb/Kconfig | 11 +++++++----
+ 1 files changed, 7 insertions(+), 4 deletions(-)
+
+diff --git a/drivers/usb/musb/Kconfig b/drivers/usb/musb/Kconfig
+index ee75cbc..d56f23d 100644
+--- a/drivers/usb/musb/Kconfig
++++ b/drivers/usb/musb/Kconfig
+@@ -107,10 +107,13 @@ config MUSB_PIO_ONLY
+ All data is copied between memory and FIFO by the CPU.
+ DMA controllers are ignored.
+
+- Do not select 'n' here unless DMA support for your SOC or board
+- is unavailable (or unstable). When DMA is enabled at compile time,
+- you can still disable it at run time using the "use_dma=n" module
+- parameter.
++ Select 'y' here if DMA support for your SOC or board
++ is unavailable (or unstable). On CPPI 4.1 DMA based
++ systems (AM335x, AM35x, and AM180x) DMA support is
++ considered unstable and this option should be enabled
++ in production. When DMA is enabled at compile time,
++ you can still disable it at run time using the "use_dma=n"
++ module parameter.
+
+ config USB_UX500_DMA_HW
+ select USB_UX500_DMA
+--
+1.7.0.4
diff --git a/recipes-kernel/linux/linux-omapl138-psp-2.6.37/0007-mmc-davinci-Eliminate-spurious-interrupts.patch b/recipes-kernel/linux/linux-omapl138-psp-2.6.37/0007-mmc-davinci-Eliminate-spurious-interrupts.patch
--- /dev/null
+++ b/recipes-kernel/linux/linux-omapl138-psp-2.6.37/0007-mmc-davinci-Eliminate-spurious-interrupts.patch
@@ -0,0 +1,64 @@
+From 568c76b4c8483ca912eb55f2d69398d1a162aabf Mon Sep 17 00:00:00 2001
+From: Ido Yariv <ido@wizery.com>
+Date: Wed, 21 Dec 2011 02:13:17 +0200
+Subject: [PATCH] mmc: davinci: Eliminate spurious interrupts *EXPERIMENTAL*
+
+The davinci mmc interrupt handler fills the fifo in a loop, as long as
+the DXRDY or DRRDY bits are set in the status register.
+
+If interrupts fire during this loop, they will be handled by the
+handler, but the PIC will still buffer these. As a result, the handler
+will be called again to serve these needlessly. In order to avoid these
+spurious interrupts, keep interrupts masked during the loop.
+---
+ drivers/mmc/host/davinci_mmc.c | 35 +++++++++++++++++++++++++++++------
+ 1 files changed, 29 insertions(+), 6 deletions(-)
+
+diff --git a/drivers/mmc/host/davinci_mmc.c b/drivers/mmc/host/davinci_mmc.c
+index 64a8325..8e3212e 100644
+--- a/drivers/mmc/host/davinci_mmc.c
++++ b/drivers/mmc/host/davinci_mmc.c
+@@ -1009,12 +1009,35 @@ static irqreturn_t mmc_davinci_irq(int irq, void *dev_id)
+ * by read. So, it is not unbouned loop even in the case of
+ * non-dma.
+ */
+- while (host->bytes_left && (status & (MMCST0_DXRDY | MMCST0_DRRDY))) {
+- davinci_fifo_data_trans(host, rw_threshold);
+- status = readl(host->base + DAVINCI_MMCST0);
+- if (!status)
+- break;
+- qstatus |= status;
++ if (host->bytes_left && (status & (MMCST0_DXRDY | MMCST0_DRRDY))) {
++ unsigned long im_val;
++
++ /*
++ * If interrupts fire during the following loop, they will be
++ * handled by the handler, but the PIC will still buffer these.
++ * As a result, the handler will be called again to serve these
++ * needlessly. In order to avoid these spurious interrupts,
++ * keep interrupts masked during the loop.
++ */
++ im_val = readl(host->base + DAVINCI_MMCIM);
++ writel(0, host->base + DAVINCI_MMCIM);
++
++ do {
++ davinci_fifo_data_trans(host, rw_threshold);
++ status = readl(host->base + DAVINCI_MMCST0);
++ if (!status)
++ break;
++ qstatus |= status;
++ } while (host->bytes_left &&
++ (status & (MMCST0_DXRDY | MMCST0_DRRDY)));
++
++ /*
++ * Assumption: if an interrupt is already pending, it will fire
++ * when it is unmasked. This is also assumed when the MMCIM is
++ * first set. Otherwise, writing to MMCIM after reading the
++ * status is race-prone.
++ */
++ writel(im_val, host->base + DAVINCI_MMCIM);
+ }
+
+ if (qstatus & MMCST0_DATDNE) {
+--
+1.7.7.4
diff --git a/recipes-kernel/linux/linux-omapl138-psp-2.6.37/0008-mmc-davinci-Poll-for-small-size-transfers.patch b/recipes-kernel/linux/linux-omapl138-psp-2.6.37/0008-mmc-davinci-Poll-for-small-size-transfers.patch
--- /dev/null
+++ b/recipes-kernel/linux/linux-omapl138-psp-2.6.37/0008-mmc-davinci-Poll-for-small-size-transfers.patch
@@ -0,0 +1,96 @@
+From 2323173abf87fa542d8434fa187dd67ed6048da2 Mon Sep 17 00:00:00 2001
+From: Ido Yariv <ido@wizery.com>
+Date: Sat, 24 Dec 2011 14:02:45 +0200
+Subject: [PATCH] mmc: davinci: Poll for small size transfers
+
+When initiating small size sdio transactions, it might be worth while to
+poll instead of waiting for an interrupt.
+
+While this optimization wastes CPU cycles, tests have shown that the
+interrupts handling and context switches' overhead is actually larger.
+
+Signed-off-by: Ido Yariv <ido@wizery.com>
+---
+ drivers/mmc/host/davinci_mmc.c | 25 ++++++++++++++++++++++---
+ 1 files changed, 22 insertions(+), 3 deletions(-)
+
+diff --git a/drivers/mmc/host/davinci_mmc.c b/drivers/mmc/host/davinci_mmc.c
+index c5b540b..39be44a 100644
+--- a/drivers/mmc/host/davinci_mmc.c
++++ b/drivers/mmc/host/davinci_mmc.c
+@@ -152,6 +152,11 @@ module_param(rw_threshold, uint, S_IRUGO);
+ MODULE_PARM_DESC(rw_threshold,
+ "Read/Write threshold. Default = 32");
+
++static unsigned poll_threshold = 128;
++module_param(poll_threshold, uint, S_IRUGO);
++MODULE_PARM_DESC(poll_threshold,
++ "Polling transaction size threshold. Default = 128");
++
+ static unsigned __initdata use_dma = 1;
+ module_param(use_dma, uint, 0);
+ MODULE_PARM_DESC(use_dma, "Whether to use DMA or not. Default = 1");
+@@ -184,6 +189,7 @@ struct mmc_davinci_host {
+ u32 rxdma, txdma;
+ bool use_dma;
+ bool do_dma;
++ bool active_request;
+
+ /* Scatterlist DMA uses one or more parameter RAM entries:
+ * the main one (associated with rxdma or txdma) plus zero or
+@@ -212,6 +218,7 @@ struct mmc_davinci_host {
+ unsigned char power_mode;
+ };
+
++static irqreturn_t mmc_davinci_irq(int irq, void *dev_id);
+
+ /* PIO only */
+ static void mmc_davinci_sg_to_buf(struct mmc_davinci_host *host)
+@@ -369,7 +376,16 @@ static void mmc_davinci_start_command(struct mmc_davinci_host *host,
+
+ writel(cmd->arg, host->base + DAVINCI_MMCARGHL);
+ writel(cmd_reg, host->base + DAVINCI_MMCCMD);
+- writel(im_val, host->base + DAVINCI_MMCIM);
++
++ host->active_request = true;
++ if (!host->do_dma && host->bytes_left <= poll_threshold) {
++ while (host->active_request) {
++ mmc_davinci_irq(0, host);
++ cpu_relax();
++ }
++ } else {
++ writel(im_val, host->base + DAVINCI_MMCIM);
++ }
+ }
+
+ /*----------------------------------------------------------------------*/
+@@ -684,8 +700,9 @@ mmc_davinci_prepare_data(struct mmc_davinci_host *host, struct mmc_request *req)
+ * While we *could* change that, unusual block sizes are rarely
+ * used. The occasional fallback to PIO should't hurt.
+ */
+- if (host->use_dma && (host->bytes_left & (rw_threshold - 1)) == 0
+- && mmc_davinci_start_dma_transfer(host, data) == 0) {
++ if (host->use_dma && (host->bytes_left & (rw_threshold - 1)) == 0 &&
++ host->bytes_left > poll_threshold &&
++ mmc_davinci_start_dma_transfer(host, data) == 0) {
+ /* zero this to ensure we take no PIO paths */
+ host->bytes_left = 0;
+ } else {
+@@ -898,6 +915,7 @@ mmc_davinci_xfer_done(struct mmc_davinci_host *host, struct mmc_data *data)
+ if (!data->stop || (host->cmd && host->cmd->error)) {
+ mmc_request_done(host->mmc, data->mrq);
+ writel(0, host->base + DAVINCI_MMCIM);
++ host->active_request = false;
+ } else
+ mmc_davinci_start_command(host, data->stop);
+ }
+@@ -925,6 +943,7 @@ static void mmc_davinci_cmd_done(struct mmc_davinci_host *host,
+ cmd->mrq->cmd->retries = 0;
+ mmc_request_done(host->mmc, cmd->mrq);
+ writel(0, host->base + DAVINCI_MMCIM);
++ host->active_request = false;
+ }
+ }
+
+--
+1.7.7.4
diff --git a/recipes-kernel/linux/linux-omapl138-psp-2.6.37/am180x-evm/defconfig b/recipes-kernel/linux/linux-omapl138-psp-2.6.37/am180x-evm/defconfig
index 3528214ca0b3f38e67bcca035d5a4e4c2a712ad6..e1d64770f556ca29deb75e7b0641c158f90dbd81 100644 (file)
#
# Automatically generated make config: don't edit
# Linux/arm 2.6.37 Kernel Configuration
-# Thu Apr 7 20:15:42 2011
+# Wed Mar 14 15:15:30 2012
#
CONFIG_ARM=y
CONFIG_SYS_SUPPORTS_APM_EMULATION=y
# CONFIG_SLAB is not set
CONFIG_SLUB=y
# CONFIG_SLOB is not set
-# CONFIG_PROFILING is not set
+CONFIG_PROFILING=y
+CONFIG_OPROFILE=y
CONFIG_HAVE_OPROFILE=y
# CONFIG_KPROBES is not set
CONFIG_HAVE_KPROBES=y
# CONFIG_MODULE_SRCVERSION_ALL is not set
CONFIG_BLOCK=y
CONFIG_LBDAF=y
-# CONFIG_BLK_DEV_BSG is not set
+CONFIG_BLK_DEV_BSG=y
# CONFIG_BLK_DEV_INTEGRITY is not set
#
#
CONFIG_ZBOOT_ROM_TEXT=0x0
CONFIG_ZBOOT_ROM_BSS=0x0
-CONFIG_CMDLINE=""
+CONFIG_CMDLINE=" debug "
+# CONFIG_CMDLINE_FORCE is not set
# CONFIG_XIP_KERNEL is not set
# CONFIG_KEXEC is not set
# CONFIG_AUTO_ZRELADDR is not set
# CONFIG_IPV6_TUNNEL is not set
# CONFIG_IPV6_MULTIPLE_TABLES is not set
# CONFIG_IPV6_MROUTE is not set
+# CONFIG_NETLABEL is not set
# CONFIG_NETWORK_SECMARK is not set
# CONFIG_NETWORK_PHY_TIMESTAMPING is not set
CONFIG_NETFILTER=y
# CONFIG_NETFILTER_NETLINK_QUEUE is not set
# CONFIG_NETFILTER_NETLINK_LOG is not set
CONFIG_NF_CONNTRACK=y
-CONFIG_NF_CONNTRACK_IPV4=y
-CONFIG_NF_CONNTRACK_PROC_COMPAT=y
+# CONFIG_NF_CONNTRACK_MARK is not set
+# CONFIG_NF_CONNTRACK_EVENTS is not set
+# CONFIG_NF_CT_PROTO_DCCP is not set
+# CONFIG_NF_CT_PROTO_SCTP is not set
+# CONFIG_NF_CT_PROTO_UDPLITE is not set
+# CONFIG_NF_CONNTRACK_AMANDA is not set
+# CONFIG_NF_CONNTRACK_FTP is not set
+# CONFIG_NF_CONNTRACK_H323 is not set
+# CONFIG_NF_CONNTRACK_IRC is not set
+# CONFIG_NF_CONNTRACK_NETBIOS_NS is not set
+# CONFIG_NF_CONNTRACK_PPTP is not set
+# CONFIG_NF_CONNTRACK_SANE is not set
+# CONFIG_NF_CONNTRACK_SIP is not set
+# CONFIG_NF_CONNTRACK_TFTP is not set
+# CONFIG_NF_CT_NETLINK is not set
CONFIG_NETFILTER_XTABLES=y
+
+#
+# Xtables combined modules
+#
+# CONFIG_NETFILTER_XT_MARK is not set
+# CONFIG_NETFILTER_XT_CONNMARK is not set
+
+#
+# Xtables targets
+#
+# CONFIG_NETFILTER_XT_TARGET_CLASSIFY is not set
+# CONFIG_NETFILTER_XT_TARGET_CONNMARK is not set
+# CONFIG_NETFILTER_XT_TARGET_IDLETIMER is not set
+# CONFIG_NETFILTER_XT_TARGET_MARK is not set
+# CONFIG_NETFILTER_XT_TARGET_NFLOG is not set
+# CONFIG_NETFILTER_XT_TARGET_NFQUEUE is not set
+# CONFIG_NETFILTER_XT_TARGET_RATEEST is not set
+# CONFIG_NETFILTER_XT_TARGET_TEE is not set
+# CONFIG_NETFILTER_XT_TARGET_TCPMSS is not set
+
+#
+# Xtables matches
+#
+# CONFIG_NETFILTER_XT_MATCH_CLUSTER is not set
+# CONFIG_NETFILTER_XT_MATCH_COMMENT is not set
+# CONFIG_NETFILTER_XT_MATCH_CONNBYTES is not set
+# CONFIG_NETFILTER_XT_MATCH_CONNLIMIT is not set
+# CONFIG_NETFILTER_XT_MATCH_CONNMARK is not set
+# CONFIG_NETFILTER_XT_MATCH_CONNTRACK is not set
+# CONFIG_NETFILTER_XT_MATCH_CPU is not set
+# CONFIG_NETFILTER_XT_MATCH_DCCP is not set
+# CONFIG_NETFILTER_XT_MATCH_DSCP is not set
+# CONFIG_NETFILTER_XT_MATCH_ESP is not set
+# CONFIG_NETFILTER_XT_MATCH_HASHLIMIT is not set
+# CONFIG_NETFILTER_XT_MATCH_HELPER is not set
+# CONFIG_NETFILTER_XT_MATCH_HL is not set
+# CONFIG_NETFILTER_XT_MATCH_IPRANGE is not set
+# CONFIG_NETFILTER_XT_MATCH_LENGTH is not set
+# CONFIG_NETFILTER_XT_MATCH_LIMIT is not set
+# CONFIG_NETFILTER_XT_MATCH_MAC is not set
+# CONFIG_NETFILTER_XT_MATCH_MARK is not set
+# CONFIG_NETFILTER_XT_MATCH_MULTIPORT is not set
+# CONFIG_NETFILTER_XT_MATCH_OWNER is not set
+# CONFIG_NETFILTER_XT_MATCH_POLICY is not set
+# CONFIG_NETFILTER_XT_MATCH_PKTTYPE is not set
+# CONFIG_NETFILTER_XT_MATCH_QUOTA is not set
+# CONFIG_NETFILTER_XT_MATCH_RATEEST is not set
+# CONFIG_NETFILTER_XT_MATCH_REALM is not set
+# CONFIG_NETFILTER_XT_MATCH_RECENT is not set
+# CONFIG_NETFILTER_XT_MATCH_SCTP is not set
+# CONFIG_NETFILTER_XT_MATCH_STATE is not set
+# CONFIG_NETFILTER_XT_MATCH_STATISTIC is not set
+# CONFIG_NETFILTER_XT_MATCH_STRING is not set
+# CONFIG_NETFILTER_XT_MATCH_TCPMSS is not set
+# CONFIG_NETFILTER_XT_MATCH_TIME is not set
+# CONFIG_NETFILTER_XT_MATCH_U32 is not set
# CONFIG_IP_VS is not set
#
# IP: Netfilter Configuration
#
CONFIG_NF_DEFRAG_IPV4=y
+CONFIG_NF_CONNTRACK_IPV4=y
+CONFIG_NF_CONNTRACK_PROC_COMPAT=y
# CONFIG_IP_NF_QUEUE is not set
+CONFIG_IP_NF_IPTABLES=y
+# CONFIG_IP_NF_MATCH_ADDRTYPE is not set
+# CONFIG_IP_NF_MATCH_AH is not set
+# CONFIG_IP_NF_MATCH_ECN is not set
+# CONFIG_IP_NF_MATCH_TTL is not set
CONFIG_IP_NF_FILTER=y
+# CONFIG_IP_NF_TARGET_REJECT is not set
CONFIG_IP_NF_TARGET_LOG=y
+# CONFIG_IP_NF_TARGET_ULOG is not set
CONFIG_NF_NAT=y
CONFIG_NF_NAT_NEEDED=y
-CONFIG_IP_NF_TARGET_MASQUERADE=y
-CONFIG_IP_NF_IPTABLES=y
+CONFIG_IP_NF_TARGET_MASQUERADE=y
+# CONFIG_IP_NF_TARGET_NETMAP is not set
+# CONFIG_IP_NF_TARGET_REDIRECT is not set
+# CONFIG_NF_NAT_SNMP_BASIC is not set
+# CONFIG_NF_NAT_FTP is not set
+# CONFIG_NF_NAT_IRC is not set
+# CONFIG_NF_NAT_TFTP is not set
+# CONFIG_NF_NAT_AMANDA is not set
+# CONFIG_NF_NAT_PPTP is not set
+# CONFIG_NF_NAT_H323 is not set
+# CONFIG_NF_NAT_SIP is not set
+# CONFIG_IP_NF_MANGLE is not set
+# CONFIG_IP_NF_RAW is not set
+# CONFIG_IP_NF_SECURITY is not set
# CONFIG_IP_NF_ARPTABLES is not set
#
# IPv6: Netfilter Configuration
#
# CONFIG_NF_DEFRAG_IPV6 is not set
+# CONFIG_NF_CONNTRACK_IPV6 is not set
# CONFIG_IP6_NF_QUEUE is not set
# CONFIG_IP6_NF_IPTABLES is not set
# CONFIG_IP_DCCP is not set
# CONFIG_IEEE802154 is not set
# CONFIG_NET_SCHED is not set
# CONFIG_DCB is not set
+# CONFIG_DNS_RESOLVER is not set
#
# Network testing
# CONFIG_HAMRADIO is not set
# CONFIG_CAN is not set
# CONFIG_IRDA is not set
-CONFIG_BT=y
-CONFIG_BT_L2CAP=y
-CONFIG_BT_SCO=y
-CONFIG_BT_RFCOMM=y
-CONFIG_BT_RFCOMM_TTY=y
-CONFIG_BT_BNEP=y
-CONFIG_BT_BNEP_MC_FILTER=y
-CONFIG_BT_BNEP_PROTO_FILTER=y
-CONFIG_BT_HIDP=y
-
-#
-# Bluetooth device drivers
-#
-CONFIG_BT_HCIUART=y
-CONFIG_BT_HCIUART_H4=y
-CONFIG_BT_HCIUART_LL=y
-
+# CONFIG_BT is not set
# CONFIG_AF_RXRPC is not set
CONFIG_WIRELESS=y
CONFIG_WIRELESS_EXT=y
CONFIG_WEXT_CORE=y
CONFIG_WEXT_PROC=y
-CONFIG_WEXT_SPY=y
-CONFIG_WEXT_PRIV=y
# CONFIG_CFG80211 is not set
+CONFIG_WIRELESS_EXT_SYSFS=y
# CONFIG_LIB80211 is not set
#
#
# CONFIG_WIMAX is not set
CONFIG_RFKILL=y
+# CONFIG_RFKILL_INPUT is not set
# CONFIG_NET_9P is not set
# CONFIG_CAIF is not set
# CONFIG_CEPH_LIB is not set
#
# Generic Driver Options
#
-CONFIG_UEVENT_HELPER_PATH="/sbin/hotplug"
-# CONFIG_DEVTMPFS is not set
+CONFIG_UEVENT_HELPER_PATH=""
+CONFIG_DEVTMPFS=y
+CONFIG_DEVTMPFS_MOUNT=y
CONFIG_STANDALONE=y
CONFIG_PREVENT_FIRMWARE_BUILD=y
CONFIG_FW_LOADER=y
#
# Texas Instruments shared transport line discipline
#
+# CONFIG_TI_ST is not set
CONFIG_HAVE_IDE=y
# CONFIG_IDE is not set
# CONFIG_NETDEV_1000 is not set
# CONFIG_NETDEV_10000 is not set
CONFIG_WLAN=y
+# CONFIG_USB_ZD1201 is not set
# CONFIG_HOSTAP is not set
-# CONFIG_HOSTAP_FIRMWARE is not set
CONFIG_WL12XX_PLATFORM_DATA=y
#
# CONFIG_USB_PEGASUS is not set
# CONFIG_USB_RTL8150 is not set
# CONFIG_USB_USBNET is not set
+# CONFIG_USB_HSO is not set
# CONFIG_USB_IPHETH is not set
# CONFIG_WAN is not set
#
# Userland interfaces
#
-# CONFIG_INPUT_MOUSEDEV is not set
+CONFIG_INPUT_MOUSEDEV=y
+CONFIG_INPUT_MOUSEDEV_PSAUX=y
+CONFIG_INPUT_MOUSEDEV_SCREEN_X=1024
+CONFIG_INPUT_MOUSEDEV_SCREEN_Y=768
# CONFIG_INPUT_JOYDEV is not set
CONFIG_INPUT_EVDEV=y
# CONFIG_INPUT_EVBUG is not set
# CONFIG_KEYBOARD_STOWAWAY is not set
# CONFIG_KEYBOARD_SUNKBD is not set
CONFIG_KEYBOARD_XTKBD=m
-# CONFIG_INPUT_MOUSE is not set
+CONFIG_INPUT_MOUSE=y
+CONFIG_MOUSE_PS2=y
+CONFIG_MOUSE_PS2_ALPS=y
+CONFIG_MOUSE_PS2_LOGIPS2PP=y
+CONFIG_MOUSE_PS2_SYNAPTICS=y
+CONFIG_MOUSE_PS2_TRACKPOINT=y
+# CONFIG_MOUSE_PS2_ELANTECH is not set
+# CONFIG_MOUSE_PS2_SENTELIC is not set
+# CONFIG_MOUSE_PS2_TOUCHKIT is not set
+# CONFIG_MOUSE_SERIAL is not set
+# CONFIG_MOUSE_APPLETOUCH is not set
+# CONFIG_MOUSE_BCM5974 is not set
+# CONFIG_MOUSE_VSXXXAA is not set
+# CONFIG_MOUSE_GPIO is not set
+# CONFIG_MOUSE_SYNAPTICS_I2C is not set
# CONFIG_INPUT_JOYSTICK is not set
# CONFIG_INPUT_TABLET is not set
CONFIG_INPUT_TOUCHSCREEN=y
# CONFIG_TOUCHSCREEN_TSC2004 is not set
# CONFIG_TOUCHSCREEN_W90X900 is not set
CONFIG_TOUCHSCREEN_TPS6507X=y
-# CONFIG_INPUT_MISC is not set
+CONFIG_INPUT_MISC=y
+# CONFIG_INPUT_AD714X is not set
+# CONFIG_INPUT_ATI_REMOTE is not set
+# CONFIG_INPUT_ATI_REMOTE2 is not set
+# CONFIG_INPUT_KEYSPAN_REMOTE is not set
+# CONFIG_INPUT_POWERMATE is not set
+# CONFIG_INPUT_YEALINK is not set
+# CONFIG_INPUT_CM109 is not set
+CONFIG_INPUT_UINPUT=y
+# CONFIG_INPUT_PCF8574 is not set
+# CONFIG_INPUT_GPIO_ROTARY_ENCODER is not set
+# CONFIG_INPUT_ADXL34X is not set
#
# Hardware I/O ports
# CONFIG_FONTS is not set
CONFIG_FONT_8x8=y
CONFIG_FONT_8x16=y
-CONFIG_LOGO=y
-CONFIG_LOGO_LINUX_MONO=y
-CONFIG_LOGO_LINUX_VGA16=y
-CONFIG_LOGO_LINUX_CLUT224=y
+# CONFIG_LOGO is not set
CONFIG_SOUND=y
# CONFIG_SOUND_OSS_CORE is not set
CONFIG_SND=y
CONFIG_SND_ARM=y
CONFIG_SND_SPI=y
CONFIG_SND_USB=y
-# CONFIG_SND_USB_AUDIO is not set
+CONFIG_SND_USB_AUDIO=y
# CONFIG_SND_USB_UA101 is not set
# CONFIG_SND_USB_CAIAQ is not set
CONFIG_SND_SOC=y
# CONFIG_USB_DEVICEFS is not set
CONFIG_USB_DEVICE_CLASS=y
# CONFIG_USB_DYNAMIC_MINORS is not set
+# CONFIG_USB_SUSPEND is not set
# CONFIG_USB_OTG_WHITELIST is not set
# CONFIG_USB_OTG_BLACKLIST_HUB is not set
# CONFIG_USB_MON is not set
# CONFIG_USB_MUSB_UX500 is not set
CONFIG_USB_MUSB_HOST=y
CONFIG_USB_MUSB_HDRC_HCD=y
-# CONFIG_MUSB_PIO_ONLY is not set
-# CONFIG_USB_INVENTRA_DMA_HW is not set
-# CONFIG_USB_TI_CPPI_DMA_HW is not set
-CONFIG_USB_TI_CPPI41_DMA_HW=y
+CONFIG_MUSB_PIO_ONLY=y
# CONFIG_USB_INVENTRA_DMA is not set
# CONFIG_USB_TI_CPPI_DMA is not set
-CONFIG_USB_TI_CPPI41_DMA=y
+# CONFIG_USB_TI_CPPI41_DMA is not set
# CONFIG_USB_TUSB_OMAP_DMA is not set
CONFIG_USB_MUSB_DEBUG=y
CONFIG_UIO=y
# CONFIG_UIO_PDRV is not set
# CONFIG_UIO_PDRV_GENIRQ is not set
-# CONFIG_UIO_SMX is not set
-# CONFIG_UIO_SERCOS3 is not set
CONFIG_UIO_PRUSS=m
# CONFIG_STAGING is not set
CONFIG_FS_MBCACHE=y
# CONFIG_REISERFS_FS is not set
# CONFIG_JFS_FS is not set
-# CONFIG_FS_POSIX_ACL is not set
+CONFIG_FS_POSIX_ACL=y
# CONFIG_XFS_FS is not set
# CONFIG_GFS2_FS is not set
# CONFIG_OCFS2_FS is not set
# CONFIG_QUOTACTL is not set
CONFIG_AUTOFS4_FS=m
# CONFIG_FUSE_FS is not set
+CONFIG_GENERIC_ACL=y
#
# Caches
CONFIG_PROC_PAGE_MONITOR=y
CONFIG_SYSFS=y
CONFIG_TMPFS=y
-# CONFIG_TMPFS_POSIX_ACL is not set
+CONFIG_TMPFS_POSIX_ACL=y
# CONFIG_HUGETLB_PAGE is not set
# CONFIG_CONFIGFS_FS is not set
CONFIG_MISC_FILESYSTEMS=y
# CONFIG_ADFS_FS is not set
# CONFIG_AFFS_FS is not set
+# CONFIG_ECRYPT_FS is not set
# CONFIG_HFS_FS is not set
# CONFIG_HFSPLUS_FS is not set
# CONFIG_BEFS_FS is not set
CONFIG_HAVE_FUNCTION_TRACER=y
CONFIG_HAVE_DYNAMIC_FTRACE=y
CONFIG_HAVE_FTRACE_MCOUNT_RECORD=y
+CONFIG_RING_BUFFER=y
+CONFIG_RING_BUFFER_ALLOW_SWAP=y
CONFIG_TRACING_SUPPORT=y
# CONFIG_FTRACE is not set
# CONFIG_DYNAMIC_DEBUG is not set
# Security options
#
CONFIG_KEYS=y
+# CONFIG_KEYS_DEBUG_PROC_KEYS is not set
# CONFIG_SECURITY_DMESG_RESTRICT is not set
CONFIG_SECURITY=y
# CONFIG_SECURITYFS is not set
+# CONFIG_SECURITY_NETWORK is not set
+# CONFIG_SECURITY_PATH is not set
+# CONFIG_SECURITY_TOMOYO is not set
+# CONFIG_SECURITY_APPARMOR is not set
+# CONFIG_IMA is not set
CONFIG_DEFAULT_SECURITY_DAC=y
CONFIG_DEFAULT_SECURITY=""
CONFIG_CRYPTO=y
#
# Crypto core or helper
#
-# CONFIG_CRYPTO_MANAGER is not set
-# CONFIG_CRYPTO_MANAGER2 is not set
+CONFIG_CRYPTO_ALGAPI=y
+CONFIG_CRYPTO_ALGAPI2=y
+CONFIG_CRYPTO_AEAD2=y
+CONFIG_CRYPTO_BLKCIPHER=y
+CONFIG_CRYPTO_BLKCIPHER2=y
+CONFIG_CRYPTO_HASH=y
+CONFIG_CRYPTO_HASH2=y
+CONFIG_CRYPTO_RNG2=y
+CONFIG_CRYPTO_PCOMP2=y
+CONFIG_CRYPTO_MANAGER=y
+CONFIG_CRYPTO_MANAGER2=y
+CONFIG_CRYPTO_MANAGER_DISABLE_TESTS=y
# CONFIG_CRYPTO_GF128MUL is not set
# CONFIG_CRYPTO_NULL is not set
+CONFIG_CRYPTO_WORKQUEUE=y
# CONFIG_CRYPTO_CRYPTD is not set
# CONFIG_CRYPTO_AUTHENC is not set
# CONFIG_CRYPTO_TEST is not set
CONFIG_BITREVERSE=y
CONFIG_GENERIC_FIND_LAST_BIT=y
CONFIG_CRC_CCITT=m
-# CONFIG_CRC16 is not set
+CONFIG_CRC16=y
CONFIG_CRC_T10DIF=m
# CONFIG_CRC_ITU_T is not set
CONFIG_CRC32=y
diff --git a/recipes-kernel/linux/linux-omapl138-psp_2.6.37.bb b/recipes-kernel/linux/linux-omapl138-psp_2.6.37.bb
index ec472d7cd8754f76c060f4161c81e2844dd131f8..d569a8f5cddc10efd42704c3c8eee8e3032b4683 100644 (file)
file://0005-Davinci-da850-Add-Mistral-WL12XX-config-support-to.patch \
file://0006-Add-wlan-and-BT-config-switches.patch \
file://uio_pruss.patch \
-"
+ file://0007-mmc-davinci-Eliminate-spurious-interrupts.patch \
+ file://0008-mmc-davinci-Poll-for-small-size-transfers.patch \
+ "
+
+# Updated PIO mode for MUSB help description
+PATCHES_OVER_PSP += "file://0001-musb-update-PIO-mode-help-information-in-Kconfig.patch"