summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 54d48a8)
raw | patch | inline | side by side (parent: 54d48a8)
author | Chase Maupin <Chase.Maupin@ti.com> | |
Mon, 11 Mar 2013 20:03:35 +0000 (15:03 -0500) | ||
committer | Denys Dmytriyenko <denys@ti.com> | |
Mon, 11 Mar 2013 21:17:40 +0000 (17:17 -0400) |
* Until the permanent fix can be picked up in oe-core fix the
do_deploy function to properly package the dtb files built
as part of the kernel build.
Signed-off-by: Chase Maupin <Chase.Maupin@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
do_deploy function to properly package the dtb files built
as part of the kernel build.
Signed-off-by: Chase Maupin <Chase.Maupin@ti.com>
Signed-off-by: Denys Dmytriyenko <denys@ti.com>
recipes-kernel/linux/linux-ti-staging_git.bb | patch | blob | history |
diff --git a/recipes-kernel/linux/linux-ti-staging_git.bb b/recipes-kernel/linux/linux-ti-staging_git.bb
index f6fa6d211dab6b091038b21258d1eefb602b13d6..9ce507bbfdef94abc23fb513adf14105828770d8 100644 (file)
KERNEL_IMAGETYPE = "uImage"
inherit kernel
+
+# This function must be here BEFORE the require of linux-dtb.inc below.
+# There is a "bug" in the base kernel.bbclass that after it's do_deploy
+# step it does not return back to the ${S} directory but stays in the
+# DEPLOY_DIR. However, the do_deploy_append defined in linux-dtb.inc
+# assumes that it is being run in the ${S} directory. A patch is
+# being submitted to fix this issue by either changing the do_deploy
+# in the kernel.bbclass to do "cd -" as the last step or to add
+# "cd ${S}" as the first line of do_deploy in linux-dtb.inc and this
+# function can be removed once that change is available.
+# If the function is not placed BEFORE the require then the change
+# directory is not appended before the linux-dtb.inc changes.
+do_deploy_append() {
+ cd ${S}
+}
+
require recipes-kernel/linux/linux-dtb.inc
require recipes-kernel/linux/setup-defconfig.inc
PV = "3.8.2"
# Append to the MACHINE_KERNEL_PR so that a new SRCREV will cause a rebuild
-MACHINE_KERNEL_PR_append = "c+gitr${SRCPV}"
+MACHINE_KERNEL_PR_append = "d+gitr${SRCPV}"
SRC_URI = "git://gitorious.ti.com/ti-linux-kernel/ti-linux-kernel.git;protocol=git;branch=${BRANCH} \
file://defconfig \